Functions | |
| void | AONEventMcuWakeUpSet (uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified MCU wakeup programmable event. More... | |
| uint32_t | AONEventMcuWakeUpGet (uint32_t ui32MCUWUEvent) |
| Get event source for the specified MCU wakeup programmable event. More... | |
| void | AONEventAuxWakeUpSet (uint32_t ui32AUXWUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified AUX wakeup programmable event. More... | |
| uint32_t | AONEventAuxWakeUpGet (uint32_t ui32AUXWUEvent) |
| Get event source for the specified AUX wakeup programmable event. More... | |
| void | AONEventMcuSet (uint32_t ui32MCUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified programmable event forwarded to the MCU event fabric. More... | |
| uint32_t | AONEventMcuGet (uint32_t ui32MCUEvent) |
| Get source for the specified programmable event forwarded to the MCU event fabric. More... | |
| __STATIC_INLINE void | AONEventRtcSet (uint32_t ui32EventSrc) |
| Select event source forwarded to AON Real Time Clock (RTC). More... | |
| __STATIC_INLINE uint32_t | AONEventRtcGet (void) |
| Get event source forwarded to AON Real Time Clock (RTC). More... | |
| uint32_t AONEventAuxWakeUpGet | ( | uint32_t | ui32AUXWUEvent | ) |
Get event source for the specified AUX wakeup programmable event.
The AON event fabric has a total of three programmable events that can wake-up the AUX domain. The events are forwarded to the wakeup controller (WUC).
| ui32AUXWUEvent | is one of three programmable AUX wakeup event sources. |
Definition at line 200 of file aon_event.c.
| void AONEventAuxWakeUpSet | ( | uint32_t | ui32AUXWUEvent, |
| uint32_t | ui32EventSrc | ||
| ) |
Select event source for the specified AUX wakeup programmable event.
The AON event fabric has a total of three programmable events that can wake-up the AUX domain. The events are forwarded to the wakeup controller (WUC).
| ui32AUXWUEvent | is one of three programmable AUX wakeup event sources. |
| ui32EventSrc | is an event sources for the event AON fabric.
|
Definition at line 161 of file aon_event.c.
| uint32_t AONEventMcuGet | ( | uint32_t | ui32MCUEvent | ) |
Get source for the specified programmable event forwarded to the MCU event fabric.
The AON event fabric has a total of three programmable events that can be forwarded to the MCU event fabric.
| ui32MCUEvent | is one of three programmable events forwarded to the MCU event fabric. |
Get source for the specified programmable event forwarded to the MCU event fabric.
Definition at line 283 of file aon_event.c.
| void AONEventMcuSet | ( | uint32_t | ui32MCUEvent, |
| uint32_t | ui32EventSrc | ||
| ) |
Select event source for the specified programmable event forwarded to the MCU event fabric.
The AON event fabric has a total of three programmable events that can be forwarded to the MCU event fabric.
| ui32MCUEvent | is one of three programmable events forwarded to the MCU event fabric. |
| ui32EventSrc | is event sources for the event AON fabric.
|
Select event source for the specified programmable event forwarded to the MCU event fabric
Definition at line 243 of file aon_event.c.
| uint32_t AONEventMcuWakeUpGet | ( | uint32_t | ui32MCUWUEvent | ) |
Get event source for the specified MCU wakeup programmable event.
The AON event fabric has a total of four programmable events that can wake-up the MCU. The events are forwarded to the wakeup controller (WUC).
| ui32MCUWUEvent | is one of four programmable MCU wakeup event sources. |
Definition at line 113 of file aon_event.c.
| void AONEventMcuWakeUpSet | ( | uint32_t | ui32MCUWUEvent, |
| uint32_t | ui32EventSrc | ||
| ) |
Select event source for the specified MCU wakeup programmable event.
The AON event fabric has a total of four programmable events that can wake-up the MCU. The events are forwarded to the wakeup controller (WUC).
| ui32MCUWUEvent | is one of four programmable MCU wakeup event sources. |
| ui32EventSrc | is an event source for the event AON fabric.
|
Definition at line 68 of file aon_event.c.
| __STATIC_INLINE uint32_t AONEventRtcGet | ( | void | ) |
Get event source forwarded to AON Real Time Clock (RTC).
A programmable event can be forwarded to the AON real time clock for triggering a capture event on RTC channel 1.
Definition at line 414 of file aon_event.h.
| __STATIC_INLINE void AONEventRtcSet | ( | uint32_t | ui32EventSrc | ) |
Select event source forwarded to AON Real Time Clock (RTC).
A programmable event can be forwarded to the AON real time clock for triggering a capture event on RTC channel 1.
| ui32EventSrc | is the event sources for the event AON fabric.
|
Definition at line 381 of file aon_event.h.
| #define AON_EVENT_AUX0 44 |
Definition at line 142 of file aon_event.h.
| #define AON_EVENT_AUX1 45 |
Definition at line 144 of file aon_event.h.
| #define AON_EVENT_AUX2 46 |
Definition at line 146 of file aon_event.h.
| #define AON_EVENT_AUX_ADC_DONE 49 |
Definition at line 150 of file aon_event.h.
| #define AON_EVENT_AUX_CMPA 47 |
Definition at line 148 of file aon_event.h.
| #define AON_EVENT_AUX_CMPB 48 |
Definition at line 149 of file aon_event.h.
| #define AON_EVENT_AUX_TDC_DONE 50 |
Definition at line 151 of file aon_event.h.
| #define AON_EVENT_AUX_TIMER0 51 |
Definition at line 152 of file aon_event.h.
| #define AON_EVENT_AUX_TIMER1 52 |
Definition at line 153 of file aon_event.h.
| #define AON_EVENT_AUX_WU0 0 |
Definition at line 176 of file aon_event.h.
Referenced by AONEventAuxWakeUpGet(), and AONEventAuxWakeUpSet().
| #define AON_EVENT_AUX_WU1 1 |
Definition at line 177 of file aon_event.h.
Referenced by AONEventAuxWakeUpGet(), and AONEventAuxWakeUpSet().
| #define AON_EVENT_AUX_WU2 2 |
Definition at line 178 of file aon_event.h.
Referenced by AONEventAuxWakeUpGet(), and AONEventAuxWakeUpSet().
| #define AON_EVENT_BATMON_TEMP 53 |
Definition at line 155 of file aon_event.h.
| #define AON_EVENT_BATMON_VOLT 54 |
Definition at line 156 of file aon_event.h.
| #define AON_EVENT_IO 32 |
Definition at line 130 of file aon_event.h.
| #define AON_EVENT_IO0 AON_EVENT_DIO_0 |
Definition at line 98 of file aon_event.h.
| #define AON_EVENT_IO1 AON_EVENT_DIO_1 |
Definition at line 99 of file aon_event.h.
| #define AON_EVENT_IO10 AON_EVENT_DIO_10 |
Definition at line 108 of file aon_event.h.
| #define AON_EVENT_IO11 AON_EVENT_DIO_11 |
Definition at line 109 of file aon_event.h.
| #define AON_EVENT_IO12 AON_EVENT_DIO_12 |
Definition at line 110 of file aon_event.h.
| #define AON_EVENT_IO13 AON_EVENT_DIO_13 |
Definition at line 111 of file aon_event.h.
| #define AON_EVENT_IO14 AON_EVENT_DIO_14 |
Definition at line 112 of file aon_event.h.
| #define AON_EVENT_IO15 AON_EVENT_DIO_15 |
Definition at line 113 of file aon_event.h.
| #define AON_EVENT_IO16 AON_EVENT_DIO_16 |
Definition at line 114 of file aon_event.h.
| #define AON_EVENT_IO17 AON_EVENT_DIO_17 |
Definition at line 115 of file aon_event.h.
| #define AON_EVENT_IO18 AON_EVENT_DIO_18 |
Definition at line 116 of file aon_event.h.
| #define AON_EVENT_IO19 AON_EVENT_DIO_19 |
Definition at line 117 of file aon_event.h.
| #define AON_EVENT_IO2 AON_EVENT_DIO_2 |
Definition at line 100 of file aon_event.h.
| #define AON_EVENT_IO20 AON_EVENT_DIO_20 |
Definition at line 118 of file aon_event.h.
| #define AON_EVENT_IO21 AON_EVENT_DIO_21 |
Definition at line 119 of file aon_event.h.
| #define AON_EVENT_IO22 AON_EVENT_DIO_22 |
Definition at line 120 of file aon_event.h.
| #define AON_EVENT_IO23 AON_EVENT_DIO_23 |
Definition at line 121 of file aon_event.h.
| #define AON_EVENT_IO24 AON_EVENT_DIO_24 |
Definition at line 122 of file aon_event.h.
| #define AON_EVENT_IO25 AON_EVENT_DIO_25 |
Definition at line 123 of file aon_event.h.
| #define AON_EVENT_IO26 AON_EVENT_DIO_26 |
Definition at line 124 of file aon_event.h.
| #define AON_EVENT_IO27 AON_EVENT_DIO_27 |
Definition at line 125 of file aon_event.h.
| #define AON_EVENT_IO28 AON_EVENT_DIO_28 |
Definition at line 126 of file aon_event.h.
| #define AON_EVENT_IO29 AON_EVENT_DIO_29 |
Definition at line 127 of file aon_event.h.
| #define AON_EVENT_IO3 AON_EVENT_DIO_3 |
Definition at line 101 of file aon_event.h.
| #define AON_EVENT_IO30 AON_EVENT_DIO_30 |
Definition at line 128 of file aon_event.h.
| #define AON_EVENT_IO31 AON_EVENT_DIO_31 |
Definition at line 129 of file aon_event.h.
| #define AON_EVENT_IO4 AON_EVENT_DIO_4 |
Definition at line 102 of file aon_event.h.
| #define AON_EVENT_IO5 AON_EVENT_DIO_5 |
Definition at line 103 of file aon_event.h.
| #define AON_EVENT_IO6 AON_EVENT_DIO_6 |
Definition at line 104 of file aon_event.h.
| #define AON_EVENT_IO7 AON_EVENT_DIO_7 |
Definition at line 105 of file aon_event.h.
| #define AON_EVENT_IO8 AON_EVENT_DIO_8 |
Definition at line 106 of file aon_event.h.
| #define AON_EVENT_IO9 AON_EVENT_DIO_9 |
Definition at line 107 of file aon_event.h.
| #define AON_EVENT_JTAG 43 |
Definition at line 141 of file aon_event.h.
| #define AON_EVENT_MCU_EVENT0 0 |
Definition at line 185 of file aon_event.h.
Referenced by AONEventMcuGet(), and AONEventMcuSet().
| #define AON_EVENT_MCU_EVENT1 1 |
Definition at line 187 of file aon_event.h.
Referenced by AONEventMcuGet(), and AONEventMcuSet().
| #define AON_EVENT_MCU_EVENT2 2 |
Definition at line 189 of file aon_event.h.
Referenced by AONEventMcuGet(), and AONEventMcuSet().
| #define AON_EVENT_MCU_WU0 0 |
Definition at line 166 of file aon_event.h.
Referenced by AONEventMcuWakeUpGet(), and AONEventMcuWakeUpSet().
| #define AON_EVENT_MCU_WU1 1 |
Definition at line 167 of file aon_event.h.
Referenced by AONEventMcuWakeUpGet(), and AONEventMcuWakeUpSet().
| #define AON_EVENT_MCU_WU2 2 |
Definition at line 168 of file aon_event.h.
Referenced by AONEventMcuWakeUpGet(), and AONEventMcuWakeUpSet().
| #define AON_EVENT_MCU_WU3 3 |
Definition at line 169 of file aon_event.h.
Referenced by AONEventMcuWakeUpGet(), and AONEventMcuWakeUpSet().
| #define AON_EVENT_NULL 63 |
Definition at line 158 of file aon_event.h.
Referenced by AONEventAuxWakeUpSet(), AONEventMcuSet(), AONEventMcuWakeUpSet(), and AONEventRtcSet().
| #define AON_EVENT_RTC0 35 |
Definition at line 133 of file aon_event.h.
| #define AON_EVENT_RTC0DLY 38 |
Definition at line 136 of file aon_event.h.
| #define AON_EVENT_RTC1 36 |
Definition at line 134 of file aon_event.h.
| #define AON_EVENT_RTC1DLY 39 |
Definition at line 137 of file aon_event.h.
| #define AON_EVENT_RTC2 37 |
Definition at line 135 of file aon_event.h.
| #define AON_EVENT_RTC2DLY 40 |
Definition at line 138 of file aon_event.h.
| #define AON_EVENT_RTCDLYC 41 |
Definition at line 139 of file aon_event.h.
| #define AON_EVENT_SPISCS 34 |
Definition at line 132 of file aon_event.h.
| #define AON_EVENT_SPISRTX 33 |
Definition at line 131 of file aon_event.h.