Functions | |
| void | AONIOCDriveStrengthSet (uint32_t ui32LowDrvStr, uint32_t ui32MedDrvStr, uint32_t ui32MaxDrvStr) |
| Setup the drive strength for all IOs on the chip. More... | |
| uint32_t | AONIOCDriveStrengthGet (uint32_t ui32DriveLevel) |
| Get a specific drive level setting for all IOs. More... | |
| __STATIC_INLINE void | AONIOCFreezeEnable (void) |
| Freeze the IOs. More... | |
| __STATIC_INLINE void | AONIOCFreezeDisable (void) |
| Un-freeze the IOs. More... | |
| __STATIC_INLINE void | AONIOC32kHzOutputDisable (void) |
| Disable the 32kHz clock output. More... | |
| __STATIC_INLINE void | AONIOC32kHzOutputEnable (void) |
| Enable the 32kHz clock output. More... | |
| __STATIC_INLINE void AONIOC32kHzOutputDisable | ( | void | ) |
Disable the 32kHz clock output.
When outputting a 32 kHz clock on an IO, the output enable/disable functionality in the IOC is bypassed. Therefore, the programmer needs to call this function to disable the clock output.
| __STATIC_INLINE void AONIOC32kHzOutputEnable | ( | void | ) |
Enable the 32kHz clock output.
When outputting a 32 kHz clock on an IO, the output enable/disable functionality in the IOC is bypassed. Therefore, the programmer needs to call this function to enable the clock output.
| uint32_t AONIOCDriveStrengthGet | ( | uint32_t | ui32DriveLevel | ) |
Get a specific drive level setting for all IOs.
Use this function to retreive the driver strengt setting for a specific IO drive level.
| ui32DriveLevel | is the specific drive level to get the setting for. |
| void AONIOCDriveStrengthSet | ( | uint32_t | ui32LowDrvStr, |
| uint32_t | ui32MedDrvStr, | ||
| uint32_t | ui32MaxDrvStr | ||
| ) |
Setup the drive strength for all IOs on the chip.
Use this function to define the general drive strength settings for all IOs on the device. The drive strength of the individual IOs is set using the IOC driver.
| ui32LowDrvStr | is the minimum drive strength for all IOs |
| ui32MedDrvStr | is the medium drive strength for all IOs |
| ui32MaxDrvStr | is the maximum drive strength for all IOs |
| __STATIC_INLINE void AONIOCFreezeDisable | ( | void | ) |
Un-freeze the IOs.
When rebooting the chip after it has entered powerdown/shutdown mode, the software can regain control of the IOs by setting the IO latches as transparent. The IOs should not be unfrozen before software has restored the functionality of the IO.
Definition at line 223 of file aon_ioc.h.
Referenced by PowerCtrlIOFreezeDisable().
| __STATIC_INLINE void AONIOCFreezeEnable | ( | void | ) |
Freeze the IOs.
To retain the values of the output IOs during a powerdown/shutdown of the device all IO latches in the AON domain should be frozen in their current state. This ensures that software can regain control of the IOs after a reboot without the IOs first falling back to the default values (i.e. input and no pull).
Definition at line 200 of file aon_ioc.h.
Referenced by PowerCtrlIOFreezeEnable(), and PowerCtrlStateSet().
| #define AONIOC_DRV_STR10_20_40 0x00000002 |
Definition at line 95 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR14_28_56 0x00000006 |
Definition at line 96 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR20_40_80 0x00000007 |
Definition at line 97 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR28_56_112 0x00000005 |
Definition at line 98 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR40_80_112 0x00000004 |
Definition at line 99 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR5_10_20 0x00000001 |
Definition at line 93 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR5_7_14 0x00000000 |
Definition at line 92 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_DRV_STR7_14_28 0x00000003 |
Definition at line 94 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthSet().
| #define AONIOC_MAX_DRIVE AONIOC_DRV_STR40_80_112 |
Definition at line 101 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthGet().
| #define AONIOC_MED_DRIVE AONIOC_DRV_STR14_28_56 |
Definition at line 102 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthGet().
| #define AONIOC_MIN_DRIVE AONIOC_DRV_STR5_7_14 |
Definition at line 103 of file aon_ioc.h.
Referenced by AONIOCDriveStrengthGet().