Functions | |
| void | AUXADCDisable (void) |
| Disables the ADC. More... | |
| void | AUXADCEnableAsync (uint32_t refSource, uint32_t trigger) |
| Enables the ADC for asynchronous operation. More... | |
| void | AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger) |
| Enables the ADC for synchronous operation. More... | |
| void | AUXADCFlushFifo (void) |
| Flushes the ADC FIFO. More... | |
| __STATIC_INLINE void | AUXADCGenManualTrigger (void) |
| Generates a single manual ADC trigger. More... | |
| __STATIC_INLINE uint32_t | AUXADCGetFifoStatus (void) |
| Returns flags indicating the status of the ADC FIFO. More... | |
| uint32_t | AUXADCReadFifo (void) |
| Waits for and returns the first sample in the ADC FIFO. More... | |
| __STATIC_INLINE void | AUXADCSelectInput (uint32_t input) |
| Selects internal or external input for the ADC. More... | |
| void AUXADCEnableAsync | ( | uint32_t | refSource, |
| uint32_t | trigger | ||
| ) |
Enables the ADC for asynchronous operation.
In asynchronous operation, the ADC samples continuously between conversions.
The ADC trigger starts the conversion. Note that the first conversion may be invalid if the sampling period is too short.
| refSource | ADC reference source:
|
| trigger | ADC conversion trigger: |
| void AUXADCEnableSync | ( | uint32_t | refSource, |
| uint32_t | sampleTime, | ||
| uint32_t | trigger | ||
| ) |
Enables the ADC for synchronous operation.
In synchronous operation, the ADC is idle between a conversion and subsequent samplings.
The ADC trigger starts sampling with specified duration, followed by the conversion. Note that the first conversion may be invalid if the sampling period is too short.
| refSource | ADC reference source:
|
| sampleTime | ADC sampling time:
|
| trigger | ADC conversion trigger: |
| void AUXADCFlushFifo | ( | void | ) |
| __STATIC_INLINE void AUXADCGenManualTrigger | ( | void | ) |
| __STATIC_INLINE uint32_t AUXADCGetFifoStatus | ( | void | ) |
Returns flags indicating the status of the ADC FIFO.
The flags indicate FIFO empty, full and almost full, and whether overflow/underflow has occurred.
| uint32_t AUXADCReadFifo | ( | void | ) |
Waits for and returns the first sample in the ADC FIFO.
This function waits until there is at least one sample in the ADC FIFO. It then pops and returns the first sample from the FIFO.
Note that this procedure will deadlock if called without setting up ADC trigger generation in advance. The trigger can either be manual or periodical (using a GPT).
| __STATIC_INLINE void AUXADCSelectInput | ( | uint32_t | input | ) |
Selects internal or external input for the ADC.
Note that calling this function also selects the same input for AUX_COMPB.
| input | Internal/external input selection: |
| #define AUXADC_FIFO_ALMOST_FULL_M AUX_ANAIF_ADCFIFOSTAT_ALMOST_FULL_M |
| #define AUXADC_FIFO_EMPTY_M AUX_ANAIF_ADCFIFOSTAT_EMPTY_M |
| #define AUXADC_FIFO_FULL_M AUX_ANAIF_ADCFIFOSTAT_FULL_M |
| #define AUXADC_FIFO_OVERFLOW_M AUX_ANAIF_ADCFIFOSTAT_OVERFLOW_M |
| #define AUXADC_FIFO_UNDERFLOW_M AUX_ANAIF_ADCFIFOSTAT_UNDERFLOW_M |
| #define AUXADC_REF_FIXED (0 << ADI_4_AUX_ADCREF0_SRC_S) |
| #define AUXADC_REF_VDDA_REL (1 << ADI_4_AUX_ADCREF0_SRC_S) |
| #define AUXADC_SAMPLE_TIME_10P6_US (5 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_10P9_MS (15 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_170_US (9 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_1P37_MS (12 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_21P3_US (6 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_2P73_MS (13 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_2P7_US (3 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_341_US (10 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_42P6_US (7 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_5P3_US (4 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_5P46_MS (14 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_682_US (11 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_SAMPLE_TIME_85P3_US (8 << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S) |
| #define AUXADC_TRIGGER_GPT0A EVENT_AUXSEL0_EV_GPT0A |
| #define AUXADC_TRIGGER_GPT0B EVENT_AUXSEL0_EV_GPT0B |
| #define AUXADC_TRIGGER_GPT1A EVENT_AUXSEL0_EV_GPT1A |
| #define AUXADC_TRIGGER_GPT1B EVENT_AUXSEL0_EV_GPT1B |
| #define AUXADC_TRIGGER_GPT2A EVENT_AUXSEL0_EV_GPT2A |
| #define AUXADC_TRIGGER_GPT2B EVENT_AUXSEL0_EV_GPT2B |
| #define AUXADC_TRIGGER_GPT3A EVENT_AUXSEL0_EV_GPT3A |
| #define AUXADC_TRIGGER_GPT3B EVENT_AUXSEL0_EV_GPT3B |
| #define AUXADC_TRIGGER_MANUAL EVENT_AUXSEL0_EV_NONE |
Definition at line 95 of file aux_adc.h.
Referenced by AUXADCEnableAsync(), and AUXADCEnableSync().