Functions | |
| __STATIC_INLINE void | EventRegister (uint32_t ui32ProgOut, uint32_t ui32EventId) |
| Register a dynamic Event in the event fabric and connect a subscriber. More... | |
| __STATIC_INLINE void EventRegister | ( | uint32_t | ui32ProgOut, |
| uint32_t | ui32EventId | ||
| ) |
Register a dynamic Event in the event fabric and connect a subscriber.
Not all events can be routed to all programmable output lines. The following lists the available events for each programmable line (TBD).
TBD - Should we add logic to make sure the subscriber is disabled when switching the source.
| ui32ProgOut | is the programmable output line to the subcriber which too connect to the event. |
| ui32EventId | is the specific event that must be acted upon. |
| #define EVENT_ADC 23 |
Definition at line 95 of file event.h.
Referenced by EventRegister().
| #define EVENT_ALWAYS_0 0 |
Definition at line 72 of file event.h.
Referenced by EventRegister().
| #define EVENT_ALWAYS_1 121 |
Definition at line 193 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_AUX0 10 |
Definition at line 82 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_EDGE_DETECT 4 |
Definition at line 76 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_PROG_0 1 |
Definition at line 73 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_PROG_1 2 |
Definition at line 74 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_PROG_2 3 |
Definition at line 75 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_RTC_UPD 119 |
Definition at line 191 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_RTCCOMDLY 7 |
Definition at line 79 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_CS 6 |
Definition at line 78 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_RTX 5 |
Definition at line 77 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_RX_BURST 57 |
Definition at line 129 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_RX_SINGLE 58 |
Definition at line 130 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_TX_BURST 59 |
Definition at line 131 of file event.h.
Referenced by EventRegister().
| #define EVENT_AON_SPIS_TX_SINGLE 60 |
Definition at line 132 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX0 105 |
Definition at line 177 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX1 106 |
Definition at line 178 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX10 115 |
Definition at line 187 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX2 107 |
Definition at line 179 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX3 108 |
Definition at line 180 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX4 109 |
Definition at line 181 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX5 110 |
Definition at line 182 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX6 111 |
Definition at line 183 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX7 112 |
Definition at line 184 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX8 113 |
Definition at line 185 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX9 114 |
Definition at line 186 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_ADC 33 |
Definition at line 105 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_CMP 29 |
Definition at line 101 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_DMA_BURST 118 |
Definition at line 190 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_DMA_SINGLE 117 |
Definition at line 189 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_DMA_SW 116 |
Definition at line 188 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_ERR 32 |
Definition at line 104 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_PROG EVENT_O_GPT0ACAPTSEL |
Definition at line 225 of file event.h.
Referenced by EventRegister().
| #define EVENT_AUX_SM 8 |
Definition at line 80 of file event.h.
Referenced by EventRegister().
| #define EVENT_CM3_PROG EVENT_O_CPUIRQSEL30 |
Definition at line 201 of file event.h.
Referenced by EventRegister().
| #define EVENT_CRYPTO_DMA_DONE 94 |
Definition at line 166 of file event.h.
Referenced by EventRegister().
| #define EVENT_CRYPTO_RES_RDY 93 |
Definition at line 165 of file event.h.
Referenced by EventRegister().
| #define EVENT_DMA_DONE 39 |
Definition at line 111 of file event.h.
Referenced by EventRegister().
| #define EVENT_DMA_ERR 38 |
Definition at line 110 of file event.h.
Referenced by EventRegister().
| #define EVENT_FLASH 21 |
Definition at line 93 of file event.h.
Referenced by EventRegister().
| #define EVENT_FREEZE_PROG EVENT_O_FRZSEL0 |
Definition at line 229 of file event.h.
Referenced by EventRegister().
| #define EVENT_HALTED 120 |
Definition at line 192 of file event.h.
Referenced by EventRegister().
| #define EVENT_I2C_INTERRUPT 9 |
Definition at line 81 of file event.h.
Referenced by EventRegister().
| #define EVENT_I2S_PROG EVENT_O_I2SSTMPSEL0 |
Definition at line 227 of file event.h.
Referenced by EventRegister().
| #define EVENT_NMI 99 |
Definition at line 171 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB0 85 |
Definition at line 157 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB1 86 |
Definition at line 158 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB2 87 |
Definition at line 159 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB3 88 |
Definition at line 160 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB4 89 |
Definition at line 161 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB5 90 |
Definition at line 162 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB6 91 |
Definition at line 163 of file event.h.
Referenced by EventRegister().
| #define EVENT_PAD_IN_TIMER_SUB7 92 |
Definition at line 164 of file event.h.
Referenced by EventRegister().
| #define EVENT_PRCM 31 |
Definition at line 103 of file event.h.
Referenced by EventRegister().
| #define EVENT_PRCM_BUSON 28 |
Definition at line 100 of file event.h.
Referenced by EventRegister().
| #define EVENT_PTIM_RTX 11 |
Definition at line 83 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_CMD_ACK 25 |
Definition at line 97 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_CPE0 27 |
Definition at line 99 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_CPE1 30 |
Definition at line 102 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_HW 26 |
Definition at line 98 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_INPUT_1 95 |
Definition at line 167 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_INPUT_2 96 |
Definition at line 168 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_INPUT_3 97 |
Definition at line 169 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_INPUT_4 98 |
Definition at line 170 of file event.h.
Referenced by EventRegister().
| #define EVENT_RFCORE_PROG EVENT_O_RFCSEL9 |
Definition at line 203 of file event.h.
Referenced by EventRegister().
| #define EVENT_SPIS 56 |
Definition at line 128 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI0 34 |
Definition at line 106 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI0_RX_BURST 40 |
Definition at line 112 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI0_RX_SINGLE 41 |
Definition at line 113 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI0_TX_BURST 42 |
Definition at line 114 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI0_TX_SINGLE 43 |
Definition at line 115 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI1 35 |
Definition at line 107 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI1_RX_BURST 44 |
Definition at line 116 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI1_RX_SINGLE 45 |
Definition at line 117 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI1_TX_BURST 46 |
Definition at line 118 of file event.h.
Referenced by EventRegister().
| #define EVENT_SSI1_TX_SINGLE 47 |
Definition at line 119 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW0 100 |
Definition at line 172 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW0_DONE 20 |
Definition at line 92 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW1 101 |
Definition at line 173 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW1_DMA_DONE 22 |
Definition at line 94 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW2 102 |
Definition at line 174 of file event.h.
Referenced by EventRegister().
| #define EVENT_SW3 103 |
Definition at line 175 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_A 16 |
Definition at line 88 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_A_COMP 61 |
Definition at line 133 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_A_PROG EVENT_O_GPT0ACAPTSEL |
Definition at line 205 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_A_REQ 77 |
Definition at line 149 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_A_SREQ_ 69 |
Definition at line 141 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_B 17 |
Definition at line 89 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_B_COMP 62 |
Definition at line 134 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_B_PROG EVENT_O_GPT0BCAPTSEL |
Definition at line 206 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_B_REQ 78 |
Definition at line 150 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER0_B_SREQ 70 |
Definition at line 142 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_A 18 |
Definition at line 90 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_A_COMP 63 |
Definition at line 135 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_A_PROG EVENT_O_GPT1ACAPTSEL |
Definition at line 207 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_A_REQ 79 |
Definition at line 151 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_A_SREQ 71 |
Definition at line 143 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_B 19 |
Definition at line 91 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_B_COMP 64 |
Definition at line 136 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_B_PROG EVENT_O_GPT1BCAPTSEL |
Definition at line 208 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_B_REQ 80 |
Definition at line 152 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER1_B_SREQ 72 |
Definition at line 144 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_A 12 |
Definition at line 84 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_A_COMP 65 |
Definition at line 137 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_A_PROG EVENT_O_GPT2ACAPTSEL |
Definition at line 209 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_A_REQ 81 |
Definition at line 153 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_A_SREQ 73 |
Definition at line 145 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_B 13 |
Definition at line 85 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_B_COMP 66 |
Definition at line 138 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_B_PROG EVENT_O_GPT2BCAPTSEL |
Definition at line 210 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_B_REQ 82 |
Definition at line 154 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER2_B_SREQ 74 |
Definition at line 146 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_A 14 |
Definition at line 86 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_A_COMP 67 |
Definition at line 139 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_A_PROG EVENT_O_GPT3ACAPTSEL |
Definition at line 211 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_A_REQ 83 |
Definition at line 155 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_A_SREQ 75 |
Definition at line 147 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_B 15 |
Definition at line 87 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_B_COMP 68 |
Definition at line 140 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_B_PROG EVENT_O_GPT3BCAPTSEL |
Definition at line 212 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_B_REQ 84 |
Definition at line 156 of file event.h.
Referenced by EventRegister().
| #define EVENT_TIMER3_B_SREQ 76 |
Definition at line 148 of file event.h.
Referenced by EventRegister().
| #define EVENT_TRNG 104 |
Definition at line 176 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART0 36 |
Definition at line 108 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART0_RX_BURST 48 |
Definition at line 120 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART0_RX_SINGLE 49 |
Definition at line 121 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART0_TX_BURST 50 |
Definition at line 122 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART0_TX_SINGLE 51 |
Definition at line 123 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART1 37 |
Definition at line 109 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART1_RX_BURST 52 |
Definition at line 124 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART1_RX_SINGLE 53 |
Definition at line 125 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART1_TX_BURST 54 |
Definition at line 126 of file event.h.
Referenced by EventRegister().
| #define EVENT_UART1_TX_SINGLE 55 |
Definition at line 127 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG0 EVENT_O_UDMACH9SSEL |
Definition at line 214 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG1 EVENT_O_UDMACH9BSEL |
Definition at line 215 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG2 EVENT_O_UDMACH10SSEL |
Definition at line 216 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG3 EVENT_O_UDMACH10BSEL |
Definition at line 217 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG4 EVENT_O_UDMACH11SSEL |
Definition at line 218 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG5 EVENT_O_UDMACH11BSEL |
Definition at line 219 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG6 EVENT_O_UDMACH12SSEL |
Definition at line 220 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG7 EVENT_O_UDMACH12BSEL |
Definition at line 221 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG8 EVENT_O_UDMACH14BSEL |
Definition at line 222 of file event.h.
Referenced by EventRegister().
| #define EVENT_UDMA_PROG9 EVENT_O_UDMACH14BSEL |
Definition at line 223 of file event.h.
Referenced by EventRegister().
| #define EVENT_WATCHDOG 24 |
Definition at line 96 of file event.h.
Referenced by EventRegister().