Functions | |
| void | I2CMasterInitExpClk (uint32_t ui32Base, uint32_t ui32I2CClk, bool bFast) |
| Initializes the I2C Master block. More... | |
| __STATIC_INLINE void | I2CMasterControl (uint32_t ui32Base, uint32_t ui32Cmd) |
| Controls the state of the I2C Master module. More... | |
| __STATIC_INLINE void | I2CMasterSlaveAddrSet (uint32_t ui32Base, uint8_t ui8SlaveAddr, bool bReceive) |
| Sets the address that the I2C Master will place on the bus. More... | |
| __STATIC_INLINE void | I2CMasterEnable (uint32_t ui32Base) |
| Enables the I2C Master block. More... | |
| __STATIC_INLINE void | I2CMasterDisable (uint32_t ui32Base) |
| Disables the I2C master block. More... | |
| __STATIC_INLINE bool | I2CMasterBusy (uint32_t ui32Base) |
| Indicates whether or not the I2C Master is busy. More... | |
| __STATIC_INLINE bool | I2CMasterBusBusy (uint32_t ui32Base) |
| Indicates whether or not the I2C bus is busy. More... | |
| __STATIC_INLINE uint32_t | I2CMasterDataGet (uint32_t ui32Base) |
| Receives a byte that has been sent to the I2C Master. More... | |
| __STATIC_INLINE void | I2CMasterDataPut (uint32_t ui32Base, uint8_t ui8Data) |
| Transmits a byte from the I2C Master. More... | |
| uint32_t | I2CMasterErr (uint32_t ui32Base) |
| Gets the error status of the I2C Master module. More... | |
| __STATIC_INLINE void | I2CMasterIntEnable (uint32_t ui32Base) |
| Enables the I2C Master interrupt. More... | |
| __STATIC_INLINE void | I2CMasterIntDisable (uint32_t ui32Base) |
| Disables the I2C Master interrupt. More... | |
| __STATIC_INLINE void | I2CMasterIntClear (uint32_t ui32Base) |
| Clears I2C Master interrupt sources. More... | |
| __STATIC_INLINE bool | I2CMasterIntStatus (uint32_t ui32Base, bool bMasked) |
| Gets the current I2C Master interrupt status. More... | |
| __STATIC_INLINE void | I2CSlaveEnable (uint32_t ui32Base) |
| Enables the I2C Slave block. More... | |
| __STATIC_INLINE void | I2CSlaveInit (uint32_t ui32Base, uint8_t ui8SlaveAddr) |
| Initializes the I2C Slave block. More... | |
| __STATIC_INLINE void | I2CSlaveAddressSet (uint32_t ui32Base, uint8_t ui8SlaveAddr) |
| Sets the I2C slave address. More... | |
| __STATIC_INLINE void | I2CSlaveDisable (uint32_t ui32Base) |
| Disables the I2C slave block. More... | |
| __STATIC_INLINE uint32_t | I2CSlaveStatus (uint32_t ui32Base) |
| Gets the I2C Slave module status. More... | |
| __STATIC_INLINE uint32_t | I2CSlaveDataGet (uint32_t ui32Base) |
| Receives a byte that has been sent to the I2C Slave. More... | |
| __STATIC_INLINE void | I2CSlaveDataPut (uint32_t ui32Base, uint8_t ui8Data) |
| Transmits a byte from the I2C Slave. More... | |
| __STATIC_INLINE void | I2CSlaveIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Enables individual I2C Slave interrupt sources. More... | |
| __STATIC_INLINE void | I2CSlaveIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Disables individual I2C Slave interrupt sources. More... | |
| __STATIC_INLINE void | I2CSlaveIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Clears I2C Slave interrupt sources. More... | |
| __STATIC_INLINE uint32_t | I2CSlaveIntStatus (uint32_t ui32Base, bool bMasked) |
| Gets the current I2C Slave interrupt status. More... | |
| void | I2CIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the I2C module. More... | |
| void | I2CIntUnregister (uint32_t ui32Base) |
| Unregisters an interrupt handler for the I2C module. More... | |
| void I2CIntRegister | ( | uint32_t | ui32Base, |
| void(*)(void) | pfnHandler | ||
| ) |
Registers an interrupt handler for the I2C module.
This sets the handler to be called when an I2C interrupt occurs. This will enable the global interrupt in the interrupt controller; specific I2C interrupts must be enabled via I2CMasterIntEnable() and I2CSlaveIntEnable(). If necessary, it is the interrupt handler's responsibility to clear the interrupt source via I2CMasterIntClear() and I2CSlaveIntClear().
| ui32Base | is the base address of the I2C Master module. |
| pfnHandler | is a pointer to the function to be called when the I2C interrupt occurs. |
| void I2CIntUnregister | ( | uint32_t | ui32Base | ) |
Unregisters an interrupt handler for the I2C module.
This function will clear the handler to be called when an I2C interrupt occurs. This will also mask off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
| ui32Base | is the base address of the I2C Master module. |
| __STATIC_INLINE bool I2CMasterBusBusy | ( | uint32_t | ui32Base | ) |
Indicates whether or not the I2C bus is busy.
This function returns an indication of whether or not the I2C bus is busy. This function can be used in a multi-master environment to determine if another master is currently using the bus.
| ui32Base | is the base address of the I2C module. |
true : I2C bus is busy.false : I2C bus is not busy. | __STATIC_INLINE bool I2CMasterBusy | ( | uint32_t | ui32Base | ) |
Indicates whether or not the I2C Master is busy.
This function returns an indication of whether or not the I2C Master is busy transmitting or receiving data.
| ui32Base | is the base address of the I2C module. |
true : I2C Master is busy.false : I2C Master is not busy. | __STATIC_INLINE void I2CMasterControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Cmd | ||
| ) |
Controls the state of the I2C Master module.
This function is used to control the state of the Master module send and receive operations.
| ui32Base | is the base address of the I2C module. |
| ui32Cmd | is the command to be issued by the I2C Master module The parameter can be one of the following values:
|
| __STATIC_INLINE uint32_t I2CMasterDataGet | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void I2CMasterDataPut | ( | uint32_t | ui32Base, |
| uint8_t | ui8Data | ||
| ) |
| __STATIC_INLINE void I2CMasterDisable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void I2CMasterEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Master block.
This will enable operation of the I2C Master block.
| ui32Base | is the base address of the I2C module. |
Definition at line 304 of file i2c.h.
Referenced by I2CMasterInitExpClk().
| uint32_t I2CMasterErr | ( | uint32_t | ui32Base | ) |
Gets the error status of the I2C Master module.
This function is used to obtain the error status of the Master module send and receive operations.
| ui32Base | is the base address of the I2C module. |
| void I2CMasterInitExpClk | ( | uint32_t | ui32Base, |
| uint32_t | ui32I2CClk, | ||
| bool | bFast | ||
| ) |
Initializes the I2C Master block.
This function initializes operation of the I2C Master block. Upon successful initialization of the I2C block, this function will have set the bus speed for the master, and will have enabled the I2C Master block.
If the parameter bFast is true, then the master block will be set up to transfer data at 400 kbps; otherwise, it will be set up to transfer data at 100 kbps.
The peripheral clock will be the same as the domain clock. This will be the value returned by the SysCtrlPeripheralClockGet() or it can be explicitly hard coded if it is constant and known (to save the code/execution overhead of a call to SysCtrlPeripheralClockGet() ).
| ui32Base | is the base address of the I2C module. |
| ui32I2CClk | is the rate of the clock supplied to the I2C module. |
| bFast | set up for fast data transfers. |
| __STATIC_INLINE void I2CMasterIntClear | ( | uint32_t | ui32Base | ) |
Clears I2C Master interrupt sources.
The I2C Master interrupt source is cleared, so that it no longer asserts. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| ui32Base | is the base address of the I2C module. |
| __STATIC_INLINE void I2CMasterIntDisable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void I2CMasterIntEnable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE bool I2CMasterIntStatus | ( | uint32_t | ui32Base, |
| bool | bMasked | ||
| ) |
Gets the current I2C Master interrupt status.
This returns the interrupt status for the I2C Master module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| ui32Base | is the base address of the I2C Master module. |
| bMasked | selects either raw or masked interrupt status.
|
true : Active.false : Not active. | __STATIC_INLINE void I2CMasterSlaveAddrSet | ( | uint32_t | ui32Base, |
| uint8_t | ui8SlaveAddr, | ||
| bool | bReceive | ||
| ) |
Sets the address that the I2C Master will place on the bus.
This function will set the address that the I2C Master will place on the bus when initiating a transaction. When the bReceive parameter is set to true, the address will indicate that the I2C Master is initiating a read from the slave; otherwise the address will indicate that the I2C Master is initiating a write to the slave.
| ui32Base | is the base address of the I2C module. |
| ui8SlaveAddr | is a 7-bit slave address |
| bReceive | flag indicates the type of communication with the slave.
|
| __STATIC_INLINE void I2CSlaveAddressSet | ( | uint32_t | ui32Base, |
| uint8_t | ui8SlaveAddr | ||
| ) |
| __STATIC_INLINE uint32_t I2CSlaveDataGet | ( | uint32_t | ui32Base | ) |
Receives a byte that has been sent to the I2C Slave.
This function reads a byte of data from the I2C Slave Data Register.
| ui32Base | is the base address of the I2C Slave module. |
| __STATIC_INLINE void I2CSlaveDataPut | ( | uint32_t | ui32Base, |
| uint8_t | ui8Data | ||
| ) |
| __STATIC_INLINE void I2CSlaveDisable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void I2CSlaveEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Slave block.
This will enable operation of the I2C Slave block.
| ui32Base | is the base address of the I2C Slave module. |
Definition at line 631 of file i2c.h.
Referenced by I2CSlaveInit().
| __STATIC_INLINE void I2CSlaveInit | ( | uint32_t | ui32Base, |
| uint8_t | ui8SlaveAddr | ||
| ) |
Initializes the I2C Slave block.
This function initializes operation of the I2C Slave block. Upon successful initialization of the I2C blocks, this function will have set the slave address and have enabled the I2C Slave block.
The parameter ui8SlaveAddr is the value that will be compared against the slave address sent by an I2C master.
| ui32Base | is the base address of the I2C Slave module. |
| ui8SlaveAddr | is the 7-bit slave address. |
| __STATIC_INLINE void I2CSlaveIntClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Clears I2C Slave interrupt sources.
The specified I2C Slave interrupt sources are cleared, so that they no longer assert. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| ui32Base | is the base address of the I2C module. |
| ui32IntFlags | is a bit mask of the interrupt sources to be cleared. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE void I2CSlaveIntDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Disables individual I2C Slave interrupt sources.
Disables the indicated I2C Slave interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32Base | is the base address of the I2C Slave module. |
| ui32IntFlags | is the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE void I2CSlaveIntEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Enables individual I2C Slave interrupt sources.
Enables the indicated I2C Slave interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32Base | is the base address of the I2C module. |
| ui32IntFlags | is the bit mask of the slave interrupt sources to be enabled. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE uint32_t I2CSlaveIntStatus | ( | uint32_t | ui32Base, |
| bool | bMasked | ||
| ) |
Gets the current I2C Slave interrupt status.
This returns the interrupt status for the I2C Slave module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| ui32Base | is the base address of the I2C Slave module. |
| bMasked | selects either raw or masked interrupt status.
|
| __STATIC_INLINE uint32_t I2CSlaveStatus | ( | uint32_t | ui32Base | ) |
Gets the I2C Slave module status.
This function will return the action requested from a master, if any.
| ui32Base | is the base address of the I2C Slave module. |
| #define I2C_MASTER_CMD_BURST_RECEIVE_CONT 0x00000009 |
Definition at line 112 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_RECEIVE_ERROR_STOP 0x00000004 |
Definition at line 116 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_RECEIVE_FINISH 0x00000005 |
Definition at line 114 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_RECEIVE_START 0x0000000b |
Definition at line 110 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_SEND_CONT 0x00000001 |
Definition at line 104 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_SEND_ERROR_STOP 0x00000004 |
Definition at line 108 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_SEND_FINISH 0x00000005 |
Definition at line 106 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_BURST_SEND_START 0x00000003 |
Definition at line 102 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_CMD_SINGLE_SEND 0x00000007 |
Definition at line 98 of file i2c.h.
Referenced by I2CMasterControl().
| #define I2C_MASTER_ERR_NONE 0 |
Definition at line 124 of file i2c.h.
Referenced by I2CMasterErr().
| #define I2C_SLAVE_INT_DATA 0x00000001 |
Definition at line 146 of file i2c.h.
Referenced by I2CSlaveIntDisable(), and I2CSlaveIntEnable().
| #define I2C_SLAVE_INT_START 0x00000002 |
Definition at line 145 of file i2c.h.
Referenced by I2CSlaveIntDisable(), and I2CSlaveIntEnable().
| #define I2C_SLAVE_INT_STOP 0x00000004 |
Definition at line 144 of file i2c.h.
Referenced by I2CSlaveIntDisable(), and I2CSlaveIntEnable().