Functions | |
| void | PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode) |
| Configure the infrastructure clock. More... | |
| uint32_t | PRCMInfClockConfigureGet (uint32_t ui32PowerMode) |
| Use this function to retreive the set infrastructure clock configuration. More... | |
| __STATIC_INLINE void | PRCMMcuPowerOff (void) |
| Request a power off of the MCU voltage domain. More... | |
| __STATIC_INLINE void | PRCMMcuPowerOffCancel (void) |
| Cancel a request for a power off of the MCU voltage domain. More... | |
| __STATIC_INLINE void | PRCMMcuUldoConfigure (uint32_t ui32Enable) |
| Assert or deassert a request for the uLDO. More... | |
| void | PRCMClockConfigureSet (uint32_t ui32Domains, uint32_t ui32ClkDiv) |
| Setup the clock division factor for a subsystem in the MCU voltage domain. More... | |
| uint32_t | PRCMClockConfigureGet (uint32_t ui32Domain) |
| Get the clock configuration for a specific sub system in the MCU Voltage Domain. More... | |
| __STATIC_INLINE void | PRCMAudioClockEnable (void) |
| Enable the audio clock generation. More... | |
| __STATIC_INLINE void | PRCMAudioClockDisable (void) |
| Disable the audio clock generation. More... | |
| void | PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate) |
| Configure the audio clock generation. More... | |
| void | PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv) |
| Configure the audio clock generation with manual setting of clock divider. More... | |
| __STATIC_INLINE void | PRCMLoadSet (void) |
| Use this function to synchronize the load settings. More... | |
| __STATIC_INLINE bool | PRCMLoadGet (void) |
| Check if any of the load sensitive register has been updated. More... | |
| __STATIC_INLINE void | PRCMDomainEnable (uint32_t ui32Domains) |
| Enable clock domains in the MCU voltage domain. More... | |
| __STATIC_INLINE void | PRCMDomainDisable (uint32_t ui32Domains) |
| Disable clock domains in the MCU voltage domain. More... | |
| void | PRCMPowerDomainOn (uint32_t ui32Domains) |
| Turn power on in power domains in the MCU domain. More... | |
| void | PRCMPowerDomainOff (uint32_t ui32Domains) |
| Turn off a specific power domain. More... | |
| __STATIC_INLINE void | PRCMRfPowerDownWhenIdle (void) |
| Configure RF core to power down when idle. More... | |
| void | PRCMPeripheralRunEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in Run mode. More... | |
| void | PRCMPeripheralRunDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in Run mode. More... | |
| void | PRCMPeripheralSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in deep-sleep mode. More... | |
| void | PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in deep-sleep mode. More... | |
| uint32_t | PRCMPowerDomainStatus (uint32_t ui32Domains) |
| Get the status for a specific power domain. More... | |
| __STATIC_INLINE bool | PRCMRfReady (void) |
| Return the access status of the RF Core. More... | |
| __STATIC_INLINE bool | PRCMWdtResetStatus (void) |
| Read reset status for WatchDog Timer. More... | |
| __STATIC_INLINE void | PRCMSleep (void) |
| Put the processor into sleep mode. More... | |
| void | PRCMDeepSleep (void) |
| Put the processor into deep-sleep mode. More... | |
| void | PRCMRetentionEnable (uint32_t ui32PowerDomain) |
| Enable retention on specific power domains. More... | |
| void | PRCMRetentionDisable (uint32_t ui32PowerDomain) |
| Disable retention on power domains. More... | |
| void PRCMAudioClockConfigSet | ( | uint32_t | ui32ClkConfig, |
| uint32_t | ui32SampleRate | ||
| ) |
Configure the audio clock generation.
Use this function to set the sample rate when using internal audio clock generation for the I2S module.
| ui32ClkConfig | is the audio clock configuration. The parameter is a bitwise OR'ed value consisting of:
|
| ui32SampleRate | is the desired audio clock sample rate. The supported sample rate configurations are: |
| void PRCMAudioClockConfigSetOverride | ( | uint32_t | ui32ClkConfig, |
| uint32_t | ui32MstDiv, | ||
| uint32_t | ui32BitDiv, | ||
| uint32_t | ui32WordDiv | ||
| ) |
Configure the audio clock generation with manual setting of clock divider.
Use this function to set the audio clock divider values manually.
| ui32ClkConfig | is the audio clock configuration. The parameter is a bitwise OR'ed value consisting of:
|
| ui32MstDiv | is the desired master clock divider. |
| ui32WordDiv | is the desired word clock divider. |
| ui32BitDiv | is the desired bit clock divider. |
| __STATIC_INLINE void PRCMAudioClockDisable | ( | void | ) |
Disable the audio clock generation.
Use this function to disable the audio clock generation.
Definition at line 490 of file prcm.h.
Referenced by PRCMAudioClockConfigSet(), and PRCMAudioClockConfigSetOverride().
| __STATIC_INLINE void PRCMAudioClockEnable | ( | void | ) |
| uint32_t PRCMClockConfigureGet | ( | uint32_t | ui32Domain | ) |
Get the clock configuration for a specific sub system in the MCU Voltage Domain.
Use this function to retrieve the clock division factor on a specific clock domain inside the MCU voltage domain.
| ui32Domain | defines the sub system for which to return the clock configuration. The 5 clock domains are: |
Get the clock configuration for a specific sub system in the MCU Voltage Domain.
Definition at line 335 of file prcm.c.
Referenced by SysCtrlPeripheralClockGet().
| void PRCMClockConfigureSet | ( | uint32_t | ui32Domains, |
| uint32_t | ui32ClkDiv | ||
| ) |
Setup the clock division factor for a subsystem in the MCU voltage domain.
Use this function to set up the clock division factor on a specific clock domain inside the MCU voltage domain.
The PRCM_DOMAIN_TIMER division rate will be constant and ungated for Run / Sleep / DeepSleep mode when it is slower than the PRCM_DOMAIN_PERIPH setting. When set faster than PRCM_DOMAIN_PERIPH setting the PRCM_DOMAIN_PERIPH will be used.
The PRCM_DOMAIN_CPU can only run with 48 or 24 MHz. The only two valid clock division factors are therefore 1 and 2 and it is always sourced from the HF source.
The PRCM_DOMAIN_SERIAL clock can run independently of the PRCM_DOMAIN_SYSBUS clock. This function can be used to setup the clock divison factor but this is only valid when the PRCM_DOMAIN_SYSBUS clock is disabled. When the PRCM_DOMAIN_SYSBUS clock is enabled, the clock division ratio for this clock will follow the PRCM_DOMAIN_SYSBUS clock.
The PRCM_DOMAIN_SERIAL clock sets the serial interface clock for SSI and UART. The clock source is the MCU domain root clock. The PRCM_DOMAIN_SERIAL clock is the only asynchronous clock in the MCU Voltage domain and is configured independently from all other clocks. It is the programmers responsibility to ensure that the PRCM_DOMAIN_SERIAL clock frequency setting is slower than 5/3 of the PRCM_DOMAIN_SYSBUS clock for UART operation and less than or equal to the PRCM_DOMAIN_SYSBUS clock for SSI operation. If both modules are active the lowest value of the two must be selected.
| ui32Domains | defines the clock domains to configure the clock on. The 5 clock domains are: |
| ui32ClkDiv | is the division factor to configure. The argument must be only one of the following values: |
Setup the clock division factor for a subsystem in the MCU voltage domain.
Definition at line 276 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| void PRCMDeepSleep | ( | void | ) |
Put the processor into deep-sleep mode.
This function places the processor into deep-sleep mode; it does not return until the processor returns to run mode. The peripherals that are enabled via PRCMPeripheralDeepSleepEnable() continue to operate and can wake up the processor.
Definition at line 775 of file prcm.c.
Referenced by PowerCtrlStateSet().
| __STATIC_INLINE void PRCMDomainDisable | ( | uint32_t | ui32Domains | ) |
Disable clock domains in the MCU voltage domain.
| ui32Domains | is a bitmask containing the clock domains to disable. The independent clock domains inside the MCU voltage domain are: |
| __STATIC_INLINE void PRCMDomainEnable | ( | uint32_t | ui32Domains | ) |
Enable clock domains in the MCU voltage domain.
| ui32Domains | is a bitmask containing the clock domains to enable. The independent clock domains inside the MCU voltage domain which can be configured are: |
Definition at line 638 of file prcm.h.
Referenced by SysCtrlPowerEverything().
| uint32_t PRCMInfClockConfigureGet | ( | uint32_t | ui32PowerMode | ) |
Use this function to retreive the set infrastructure clock configuration.
| ui32PowerMode | determines which Cortex M3 power mode to return the infrastructure clock divison ratio for. The three allowed power modes are: |
| void PRCMInfClockConfigureSet | ( | uint32_t | ui32ClkDiv, |
| uint32_t | ui32PowerMode | ||
| ) |
Configure the infrastructure clock.
Each CM3 power mode has its own infrastructure clock divison factor. This function can be used for setting up the division factor for the infrastructure clock in the available power modes for the CM3. The infrastructure clock is used for all internal logic in the PRCM, and is always running as long as power is on in the MCU voltage domain. This can be enabled and disabled from the AON Wake Up Controller.
| ui32ClkDiv | determines the division ratio for the infrastructure clock when the device is in the specified mode. Allowed division factors for all three Cortex M3 power modes are: |
| ui32PowerMode | determines the Cortex M3 operation mode for which to modify the clock divison factor. The three allowed power modes are: |
| __STATIC_INLINE bool PRCMLoadGet | ( | void | ) |
Check if any of the load sensitive register has been updated.
true : No registers have changed since the last load.false : Any register has changed.Definition at line 608 of file prcm.h.
Referenced by SysCtrlPowerEverything().
| __STATIC_INLINE void PRCMLoadSet | ( | void | ) |
Use this function to synchronize the load settings.
Most of the clock settings in the PRCM module should be updated synchronously. This is ensured by the implementation of a load registers that, when written to, will let the previous written update values for all the relevant registers propagate through to hardware.
The functions that require a synchronization of the clock settings are:
Definition at line 588 of file prcm.h.
Referenced by SysCtrlPowerEverything().
| __STATIC_INLINE void PRCMMcuPowerOff | ( | void | ) |
Request a power off of the MCU voltage domain.
Use this function to request a power off of the entire MCU voltage domain. This request will have no affect until deepsleep mode is requested.
Definition at line 310 of file prcm.h.
Referenced by PowerCtrlStateSet().
| __STATIC_INLINE void PRCMMcuPowerOffCancel | ( | void | ) |
Cancel a request for a power off of the MCU voltage domain.
Use this function to cancel a request for power off of the entire MCU voltage domain. This could be relevant if a transition to power down is regretted and an application must backtrack.
| __STATIC_INLINE void PRCMMcuUldoConfigure | ( | uint32_t | ui32Enable | ) |
Assert or deassert a request for the uLDO.
Use this function to request to switch to the micro Low Voltage Dropout regulator (uLDO). The uLDO has a much lower capacicty for supplying power to the system. It is therefore imperative and solely the programmers responsibility to ensure that a sufficient amount of peripheral modules have been turned of before requesting a switch to the uLDO.
Definition at line 360 of file prcm.h.
Referenced by PowerCtrlSourceSet().
| void PRCMPeripheralDeepSleepDisable | ( | uint32_t | ui32Peripheral | ) |
Disables a peripheral in deep-sleep mode.
This function causes a peripheral to stop operating when the processor goes into deep-sleep mode. Disabling peripherals while in deep-sleep mode helps to lower the current draw of the device, and can keep peripherals that require a particular clock frequency from operating when the clock changes as a result of entering deep-sleep mode. If enabled (via PRCMPeripheralRunEnable()), the peripheral will automatically resume operation when the processor leaves deep-sleep mode, maintaining its entire state from before deep-sleep mode was entered.
| ui32Peripheral | is the peripheral to disable in deep-sleep mode. The parameter must be one of the following: |
| void PRCMPeripheralDeepSleepEnable | ( | uint32_t | ui32Peripheral | ) |
Enables a peripheral in deep-sleep mode.
This function allows a peripheral to continue operating when the processor goes into deep-sleep mode. Since the clocking configuration of the device may change, not all peripherals can safely continue operating while the processor is in sleep mode. This in turn depends on the chosen power mode. It is the responsibility of the caller to make sensible choices.
| ui32Peripheral | is the peripheral to enable in deep-sleep mode. The parameter must be one of the following: |
Definition at line 688 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| void PRCMPeripheralRunDisable | ( | uint32_t | ui32Peripheral | ) |
Disables a peripheral in Run mode.
Disables a peripheral in Run mode
Peripherals are disabled with this function. Once disabled, they will not operate or respond to register reads/writes.
| ui32Peripheral | is the peripheral to disable. The parameter must be one of the following: |
| void PRCMPeripheralRunEnable | ( | uint32_t | ui32Peripheral | ) |
Enables a peripheral in Run mode.
Peripherals are enabled with this function. At power-up, some peripherals are disabled; they must be enabled in order to operate or respond to register reads/writes.
| ui32Peripheral | is the peripheral to enable. The parameter must be one of the following: |
Definition at line 608 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| void PRCMPeripheralSleepDisable | ( | uint32_t | ui32Peripheral | ) |
Disables a peripheral in sleep mode.
This function causes a peripheral to stop operating when the processor goes into sleep mode. Disabling peripherals while in sleep mode helps to lower the current draw of the device. If enabled (via PRCMPeripheralRunEnable()), the peripheral will automatically resume operation when the processor leaves sleep mode, maintaining its entire state from before sleep mode was entered.
| ui32Peripheral | is the peripheral to disable in sleep mode. The parameter must be one of the following: |
| void PRCMPeripheralSleepEnable | ( | uint32_t | ui32Peripheral | ) |
Enables a peripheral in sleep mode.
This function allows a peripheral to continue operating when the processor goes into sleep mode. Since the clocking configuration of the device does not change, any peripheral can safely continue operating while the processor is in sleep mode, and can therefore wake the processor from sleep mode.
| ui32Peripheral | is the peripheral to enable in sleep mode. The parameter must be one of the following: |
Definition at line 648 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| void PRCMPowerDomainOff | ( | uint32_t | ui32Domains | ) |
Turn off a specific power domain.
Use this function to power down domains inside the MCU voltage domain.
| ui32Domains | determines which domain to request a power down for. The domains that can be turned on/off are:
|
Definition at line 561 of file prcm.c.
Referenced by PowerCtrlStateSet().
| void PRCMPowerDomainOn | ( | uint32_t | ui32Domains | ) |
Turn power on in power domains in the MCU domain.
Use this function to turn on power domains inside the MCU voltage domain.
Power on and power off request has different implications for the different power domains.
| ui32Domains | determines which power domains to turn on. The domains that can be turned on/off are:
|
Definition at line 514 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| uint32_t PRCMPowerDomainStatus | ( | uint32_t | ui32Domains | ) |
Get the status for a specific power domain.
Use this function to retrieve the current power status of one or more power domains.
| ui32Domains | determines which domain to get the power status for. The parameter must be an OR'ed combination of one or several of:
|
Definition at line 728 of file prcm.c.
Referenced by SysCtrlPowerEverything().
| void PRCMRetentionDisable | ( | uint32_t | ui32PowerDomain | ) |
Disable retention on power domains.
Determines if a power domain should have retention disabled.
| ui32PowerDomain | is a bit maks of the domains in question. The parameter must be a bitwise OR'ed value of: |
| void PRCMRetentionEnable | ( | uint32_t | ui32PowerDomain | ) |
Enable retention on specific power domains.
Determines if power domain should have retention enabled.
| ui32PowerDomain | is a bit mask of the domains in question. The parameter must be a bitwise OR'ed value of: |
| __STATIC_INLINE void PRCMRfPowerDownWhenIdle | ( | void | ) |
| __STATIC_INLINE bool PRCMRfReady | ( | void | ) |
Return the access status of the RF Core.
Use this function to check if the RF Core is on and ready to be accessed. Accessing register or memories that are not powered and clocked will cause a bus fault.
true : RF Core can be accessed.false : RF Core domain is not ready for access. | __STATIC_INLINE void PRCMSleep | ( | void | ) |
Put the processor into sleep mode.
This function places the processor into sleep mode; it does not return until the processor returns to run mode. The peripherals that are enabled viaPRCMPeripheralSleepEnable() continue to operate and can wake up the processor.
| __STATIC_INLINE bool PRCMWdtResetStatus | ( | void | ) |
Read reset status for WatchDog Timer.
WDT reset is the only reset status available through the PRCM module. This function can be used to check whether or not a WDT reset has occured since last time this bit was cleared.
true : A WDT reset occured since last time the bit was cleared.false : A WDT reset has not occured since last clear. | #define I2S_SAMPLE_RATE_16K 0x00000001 |
Definition at line 173 of file prcm.h.
Referenced by PRCMAudioClockConfigSet().
| #define I2S_SAMPLE_RATE_24K 0x00000002 |
Definition at line 174 of file prcm.h.
Referenced by PRCMAudioClockConfigSet().
| #define I2S_SAMPLE_RATE_32K 0x00000004 |
Definition at line 175 of file prcm.h.
Referenced by PRCMAudioClockConfigSet().
| #define I2S_SAMPLE_RATE_48K 0x00000008 |
Definition at line 176 of file prcm.h.
Referenced by PRCMAudioClockConfigSet().
| #define PRCM_CLOCK_DIV_1 0x0000000 |
Definition at line 122 of file prcm.h.
Referenced by PRCMClockConfigureSet(), PRCMInfClockConfigureGet(), PRCMInfClockConfigureSet(), and SysCtrlPowerEverything().
| #define PRCM_CLOCK_DIV_128 0x0000007 |
Definition at line 129 of file prcm.h.
Referenced by PRCMClockConfigureSet().
| #define PRCM_CLOCK_DIV_16 0x0000004 |
Definition at line 126 of file prcm.h.
Referenced by PRCMClockConfigureSet().
| #define PRCM_CLOCK_DIV_2 0x0000001 |
Definition at line 123 of file prcm.h.
Referenced by PRCMClockConfigureSet(), PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_CLOCK_DIV_256 0x0000008 |
Definition at line 130 of file prcm.h.
Referenced by PRCMClockConfigureSet().
| #define PRCM_CLOCK_DIV_32 0x0000005 |
Definition at line 127 of file prcm.h.
Referenced by PRCMClockConfigureSet(), PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_CLOCK_DIV_4 0x0000002 |
Definition at line 124 of file prcm.h.
Referenced by PRCMClockConfigureSet().
| #define PRCM_CLOCK_DIV_64 0x0000006 |
Definition at line 128 of file prcm.h.
Referenced by PRCMClockConfigureSet().
| #define PRCM_CLOCK_DIV_8 0x0000003 |
Definition at line 125 of file prcm.h.
Referenced by PRCMClockConfigureSet(), PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_DEEP_SLEEP_MODE 0x00000004 |
Definition at line 115 of file prcm.h.
Referenced by PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_DOMAIN_CPU 0x00000020 |
Definition at line 148 of file prcm.h.
Referenced by PowerCtrlStateSet(), PRCMClockConfigureGet(), PRCMClockConfigureSet(), PRCMPowerDomainOff(), PRCMPowerDomainOn(), PRCMRetentionDisable(), PRCMRetentionEnable(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_PERIPH 0x00000004 |
Definition at line 142 of file prcm.h.
Referenced by PowerCtrlStateSet(), PRCMClockConfigureGet(), PRCMClockConfigureSet(), PRCMPowerDomainOff(), PRCMPowerDomainOn(), PRCMPowerDomainStatus(), PRCMRetentionDisable(), PRCMRetentionEnable(), SysCtrlPeripheralClockGet(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_POWER_OFF 0x00000002 |
Definition at line 156 of file prcm.h.
Referenced by PRCMPowerDomainStatus().
| #define PRCM_DOMAIN_POWER_ON 0x00000001 |
Definition at line 157 of file prcm.h.
Referenced by PRCMPowerDomainStatus(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_RFCORE 0x00000001 |
Definition at line 138 of file prcm.h.
Referenced by PowerCtrlStateSet(), PRCMDomainDisable(), PRCMDomainEnable(), PRCMPowerDomainOff(), PRCMPowerDomainOn(), PRCMPowerDomainStatus(), PRCMRetentionDisable(), PRCMRetentionEnable(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_SERIAL 0x00000002 |
Definition at line 140 of file prcm.h.
Referenced by PowerCtrlStateSet(), PRCMClockConfigureGet(), PRCMClockConfigureSet(), PRCMPowerDomainOff(), PRCMPowerDomainOn(), PRCMPowerDomainStatus(), SysCtrlPeripheralClockGet(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_SYSBUS 0x00000008 |
Definition at line 144 of file prcm.h.
Referenced by PRCMClockConfigureGet(), PRCMClockConfigureSet(), SysCtrlPeripheralClockGet(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_TIMER 0x00000040 |
Definition at line 150 of file prcm.h.
Referenced by PRCMClockConfigureGet(), PRCMClockConfigureSet(), SysCtrlPeripheralClockGet(), and SysCtrlPowerEverything().
| #define PRCM_DOMAIN_VIMS 0x00000010 |
Definition at line 146 of file prcm.h.
Referenced by PowerCtrlStateSet(), PRCMDomainDisable(), PRCMDomainEnable(), PRCMPowerDomainOff(), PRCMPowerDomainOn(), PRCMRetentionDisable(), PRCMRetentionEnable(), and SysCtrlPowerEverything().
| #define PRCM_PERIPH_CRYPTO 0x00000400 |
Definition at line 194 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_GPIO 0x00000500 |
Definition at line 197 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_I2C0 0x00000300 |
Definition at line 192 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_I2C1 0x00000301 |
Definition at line 193 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_I2S 0x00000600 |
Definition at line 198 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_SSI0 0x00000100 |
Definition at line 188 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_SSI1 0x00000101 |
Definition at line 189 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_TIMER0 0x00000000 |
Definition at line 184 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_TIMER1 0x00000001 |
Definition at line 185 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_TIMER2 0x00000002 |
Definition at line 186 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_TIMER3 0x00000003 |
Definition at line 187 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_TRNG 0x00000401 |
Definition at line 195 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_UART0 0x00000200 |
Definition at line 190 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_UART1 0x00000201 |
Definition at line 191 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_PERIPH_UDMA 0x00000408 |
Definition at line 196 of file prcm.h.
Referenced by SysCtrlPeripheralClockGet().
| #define PRCM_RUN_MODE 0x00000001 |
Definition at line 113 of file prcm.h.
Referenced by PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_SLEEP_MODE 0x00000002 |
Definition at line 114 of file prcm.h.
Referenced by PRCMInfClockConfigureGet(), and PRCMInfClockConfigureSet().
| #define PRCM_WCLK_SINGLE_PHASE 0x00000000 |
Definition at line 169 of file prcm.h.
Referenced by PRCMAudioClockConfigSet(), and PRCMAudioClockConfigSetOverride().