Functions | |
| __STATIC_INLINE void | TimerEnable (uint32_t ui32Base, uint32_t ui32Timer) |
| Enables the timer(s). More... | |
| __STATIC_INLINE void | TimerDisable (uint32_t ui32Base, uint32_t ui32Timer) |
| Disables the timer(s). More... | |
| void | TimerConfigure (uint32_t ui32Base, uint32_t ui32Config) |
| Configures the timer(s). More... | |
| void | TimerLevelControl (uint32_t ui32Base, uint32_t ui32Timer, bool bInvert) |
| Controls the output level. More... | |
| void | TimerTriggerControl (uint32_t ui32Base, uint32_t ui32Timer, bool bEnable) |
| Enables or disables the ADC trigger output. More... | |
| __STATIC_INLINE void | TimerEventControl (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Event) |
| Controls the event type. More... | |
| void | TimerStallControl (uint32_t ui32Base, uint32_t ui32Timer, bool bStall) |
| Controls the stall handling. More... | |
| void | TimerWaitOnTriggerControl (uint32_t ui32Base, uint32_t ui32Timer, bool bWait) |
| Controls the wait on trigger handling. More... | |
| __STATIC_INLINE void | TimerRtcEnable (uint32_t ui32Base) |
| Enable RTC counting. More... | |
| __STATIC_INLINE void | TimerRtcDisable (uint32_t ui32Base) |
| Disable RTC counting. More... | |
| __STATIC_INLINE void | TimerPrescaleSet (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Value) |
| Set the timer prescale value. More... | |
| __STATIC_INLINE uint32_t | TimerPrescaleGet (uint32_t ui32Base, uint32_t ui32Timer) |
| Get the timer prescale value. More... | |
| __STATIC_INLINE void | TimerPrescaleMatchSet (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Value) |
| Set the timer prescale match value. More... | |
| __STATIC_INLINE uint32_t | TimerPrescaleMatchGet (uint32_t ui32Base, uint32_t ui32Timer) |
| Get the timer prescale match value. More... | |
| __STATIC_INLINE void | TimerLoadSet (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Value) |
| Sets the timer load value. More... | |
| __STATIC_INLINE uint32_t | TimerLoadGet (uint32_t ui32Base, uint32_t ui32Timer) |
| Gets the timer load value. More... | |
| __STATIC_INLINE uint32_t | TimerValueGet (uint32_t ui32Base, uint32_t ui32Timer) |
| Gets the current timer value. More... | |
| __STATIC_INLINE void | TimerMatchSet (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Value) |
| Sets the timer match value. More... | |
| __STATIC_INLINE uint32_t | TimerMatchGet (uint32_t ui32Base, uint32_t ui32Timer) |
| Gets the timer match value. More... | |
| void | TimerIntRegister (uint32_t ui32Base, uint32_t ui32Timer, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the timer interrupt. More... | |
| void | TimerIntUnregister (uint32_t ui32Base, uint32_t ui32Timer) |
| Unregisters an interrupt handler for the timer interrupt. More... | |
| __STATIC_INLINE void | TimerIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Enables individual timer interrupt sources. More... | |
| __STATIC_INLINE void | TimerIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Disables individual timer interrupt sources. More... | |
| __STATIC_INLINE uint32_t | TimerIntStatus (uint32_t ui32Base, bool bMasked) |
| Gets the current interrupt status. More... | |
| __STATIC_INLINE void | TimerIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Clears timer interrupt sources. More... | |
| __STATIC_INLINE void | TimerSynchronize (uint32_t ui32Base, uint32_t ui32Timers) |
| Synchronizes the counters in a set of timers. More... | |
| void TimerConfigure | ( | uint32_t | ui32Base, |
| uint32_t | ui32Config | ||
| ) |
Configures the timer(s).
This function configures the operating mode of the timer(s). The timer module is disabled before being configured and is left in the disabled state.
The timers are comprised of two 16-bit timers that can operate independently or be concatenated to form a 32-bit timer.
When configuring for full-width timer ui32Config is set as one of the following values:
When configuring for a pair of half-width timers, each timer is separately configured. The timers are configured by setting ui32Config to the bitwise OR of one of each of the following three:
| ui32Base | is the base address of the timer module. |
| ui32Config | is the configuration for the timer. |
Configures the timer(s).
| __STATIC_INLINE void TimerDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Disables the timer(s).
This function disables operation of the timer module.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to disable. Must be one of: |
| __STATIC_INLINE void TimerEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Enables the timer(s).
This function enables operation of the timer module. The timer must be configured before it is enabled.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to enable. Must be one of: |
| __STATIC_INLINE void TimerEventControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| uint32_t | ui32Event | ||
| ) |
Controls the event type.
This function configures the signal edge(s) that triggers the timer when in capture mode.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to be adjusted; must be one of: |
| ui32Event | specifies the type of event; must be one of: |
| __STATIC_INLINE void TimerIntClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Clears timer interrupt sources.
The specified timer interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.
| ui32Base | is the base address of the timer module. |
| ui32IntFlags | is a bit mask of the interrupt sources to be cleared. The parameter must be the bitwise OR of any combination of the following:
|
| __STATIC_INLINE void TimerIntDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Disables individual timer interrupt sources.
This function disables the indicated timer interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32Base | is the base address of the timer module. |
| ui32IntFlags | is the bit mask of the interrupt sources to be disabled. The parameter must be the bitwise OR of any combination of the following:
|
| __STATIC_INLINE void TimerIntEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntFlags | ||
| ) |
Enables individual timer interrupt sources.
This function enables the indicated timer interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32Base | is the base address of the timer module. |
| ui32IntFlags | is the bit mask of the interrupt sources to be enabled. The parameter must be the bitwise OR of any combination of the following:
|
| void TimerIntRegister | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| void(*)(void) | pfnHandler | ||
| ) |
Registers an interrupt handler for the timer interrupt.
This function registers the handler to be called when a timer interrupt occurs. In addition, this function enables the global interrupt in the interrupt controller; specific timer interrupts must be enabled via TimerIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source via TimerIntClear().
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s); must be one of: |
| pfnHandler | is a pointer to the function to be called when the timer interrupt occurs. |
| __STATIC_INLINE uint32_t TimerIntStatus | ( | uint32_t | ui32Base, |
| bool | bMasked | ||
| ) |
Gets the current interrupt status.
This function returns the interrupt status for the timer module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| ui32Base | is the base address of the timer module. |
| bMasked | selects either raw or masked interrupt status:
|
| void TimerIntUnregister | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Unregisters an interrupt handler for the timer interrupt.
This function unregisters the handler to be called when a timer interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler is no longer called.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s); must be one of: |
| void TimerLevelControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| bool | bInvert | ||
| ) |
Controls the output level.
This function configures the PWM output level for the specified timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to adjust. Must be one of: |
| bInvert | specifies the output level.
|
| __STATIC_INLINE uint32_t TimerLoadGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Gets the timer load value.
This function gets the currently programmed interval load value for the specified timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer; must be one of: |
| __STATIC_INLINE void TimerLoadSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| uint32_t | ui32Value | ||
| ) |
Sets the timer load value.
This function configures the timer load value; if the timer is running then the value is immediately loaded into the timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to adjust; must be one of: |
| ui32Value | is the load value. |
| __STATIC_INLINE uint32_t TimerMatchGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Gets the timer match value.
This function gets the match value for the specified timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer; must be one of: |
| __STATIC_INLINE void TimerMatchSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| uint32_t | ui32Value | ||
| ) |
Sets the timer match value.
This function configures the match value for a timer. This value is used in capture count mode to determine when to interrupt the processor and in PWM mode to determine the duty cycle of the output signal. Match interrupts can also be generated in periodic and one-shot modes when the value of the counter matches this register.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to adjust; must be one of: |
| ui32Value | is the match value. |
| __STATIC_INLINE uint32_t TimerPrescaleGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Get the timer prescale value.
This function gets the value of the timer clock prescaler. The prescaler is only operational when in half-width mode and is used to extend the range of the half-width timer modes.
When in one-shot or periodic down count modes, ui32Value defines the prescaler for the timer counter. When acting as a true prescaler, the prescaler counts down to 0 before the value in timer registers are incremented.
In all other individual/split modes, ui32Value is a linear extension of the upper range of the timer counter, holding bits 23:16 in the 16-bit modes of the 16/32-bit timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer; must be one of: |
| __STATIC_INLINE uint32_t TimerPrescaleMatchGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Get the timer prescale match value.
This function gets the value of the input clock prescaler match value. When in a half-width mode that uses the counter match and prescaler, the prescale match effectively extends the range of the match. The prescaler provides the least significant bits when counting down in periodic and one-shot modes; in all other modes, the prescaler provides the most significant bits.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer; must be one of: |
| __STATIC_INLINE void TimerPrescaleMatchSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| uint32_t | ui32Value | ||
| ) |
Set the timer prescale match value.
This function configures the value of the input clock prescaler match value. When in a half-width mode that uses the counter match and the prescaler, the prescale match effectively extends the range of the match. The prescaler provides the least significant bits when counting down in periodic and one-shot modes; in all other modes, the prescaler provides the most significant bits.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to adjust; must be one of: |
| ui32Value | is the timer prescale match value which must be between 0 and 255 (both included). |
| __STATIC_INLINE void TimerPrescaleSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| uint32_t | ui32Value | ||
| ) |
Set the timer prescale value.
This function configures the value of the timer clock prescaler. The prescaler is only operational when in half-width mode and is used to extend the range of the half-width timer modes.
When in one-shot or periodic down count modes, ui32Value defines the prescaler for the timer counter. When acting as a true prescaler, the prescaler counts down to 0 before the value in timer registers are incremented.
In all other individual/split modes, ui32Value is a linear extension of the upper range of the timer counter, holding bits 23:16 in the 16-bit modes of the 16/32-bit timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to adjust; must be one of: |
| ui32Value | is the timer prescale value which must be between 0 and 255 (both included).
|
| __STATIC_INLINE void TimerRtcDisable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void TimerRtcEnable | ( | uint32_t | ui32Base | ) |
| void TimerStallControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| bool | bStall | ||
| ) |
Controls the stall handling.
This function controls the stall response for the specified timer. If the bStall parameter is true, then the timer stops counting if the processor enters debug mode; otherwise the timer keeps running while in debug mode.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to be adjusted; must be one of: |
| bStall | specifies the response to a stall signal.
|
| __STATIC_INLINE void TimerSynchronize | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timers | ||
| ) |
Synchronizes the counters in a set of timers.
This function synchronizes the counters in a specified set of timers. When a timer is running in half-width mode, each half can be included or excluded in the synchronization event. When a timer is running in full-width mode, only the A timer can be synchronized (specifying the B timer has no effect).
| ui32Base | is the base address of the timer module. This parameter must be the base address of Timer0 (in other words, GPT0_BASE). |
| ui32Timers | is the set of timers to synchronize. The parameter is the bitwise OR of any of the following: |
| void TimerTriggerControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| bool | bEnable | ||
| ) |
Enables or disables the ADC trigger output.
This function controls the ADC trigger output for the specified timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer to adjust; must be one of: |
| bEnable | specifies the desired ADC trigger state.
|
| __STATIC_INLINE uint32_t TimerValueGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer | ||
| ) |
Gets the current timer value.
This function reads the current value of the specified timer.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer; must be one of: |
| void TimerWaitOnTriggerControl | ( | uint32_t | ui32Base, |
| uint32_t | ui32Timer, | ||
| bool | bWait | ||
| ) |
Controls the wait on trigger handling.
This function controls whether or not a timer waits for a trigger input to start counting. When enabled, the previous timer in the trigger chain must count to its timeout in order for this timer to start counting. Refer to the part's data sheet for a description of the trigger chain.
| ui32Base | is the base address of the timer module. |
| ui32Timer | specifies the timer(s) to be adjusted; must be one of: |
| bWait | specifies if the timer should wait for a trigger input.
|
| #define TIMER_A 0x000000FF |
Definition at line 156 of file timer.h.
Referenced by TimerDisable(), TimerEnable(), TimerEventControl(), TimerIntRegister(), TimerIntUnregister(), TimerLevelControl(), TimerLoadGet(), TimerLoadSet(), TimerMatchGet(), TimerMatchSet(), TimerPrescaleGet(), TimerPrescaleMatchGet(), TimerPrescaleMatchSet(), TimerPrescaleSet(), TimerStallControl(), TimerTriggerControl(), TimerValueGet(), and TimerWaitOnTriggerControl().
| #define TIMER_B 0x0000FF00 |
Definition at line 157 of file timer.h.
Referenced by TimerDisable(), TimerEnable(), TimerEventControl(), TimerIntRegister(), TimerIntUnregister(), TimerLevelControl(), TimerLoadGet(), TimerLoadSet(), TimerMatchGet(), TimerMatchSet(), TimerPrescaleGet(), TimerPrescaleMatchGet(), TimerPrescaleMatchSet(), TimerPrescaleSet(), TimerStallControl(), TimerTriggerControl(), TimerValueGet(), and TimerWaitOnTriggerControl().
| #define TIMER_BOTH 0x0000FFFF |
Definition at line 158 of file timer.h.
Referenced by TimerDisable(), TimerEnable(), TimerEventControl(), TimerIntRegister(), TimerIntUnregister(), TimerLevelControl(), TimerLoadSet(), TimerMatchSet(), TimerPrescaleGet(), TimerPrescaleMatchSet(), TimerPrescaleSet(), TimerStallControl(), TimerTriggerControl(), and TimerWaitOnTriggerControl().
| #define TIMER_CFG_A_CAP_COUNT 0x00000003 |
Definition at line 107 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_CAP_COUNT_UP 0x00000013 |
Definition at line 108 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_CAP_TIME 0x00000007 |
Definition at line 109 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_CAP_TIME_UP 0x00000017 |
Definition at line 110 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_ONE_SHOT 0x00000021 |
Definition at line 103 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_ONE_SHOT_UP 0x00000031 |
Definition at line 104 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_PERIODIC 0x00000022 |
Definition at line 105 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_PERIODIC_UP 0x00000032 |
Definition at line 106 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_A_PWM 0x0000000A |
Definition at line 111 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_CAP_COUNT 0x00000300 |
Definition at line 116 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_CAP_COUNT_UP 0x00001300 |
Definition at line 117 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_CAP_TIME 0x00000700 |
Definition at line 118 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_CAP_TIME_UP 0x00001700 |
Definition at line 119 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_ONE_SHOT 0x00002100 |
Definition at line 112 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_ONE_SHOT_UP 0x00003100 |
Definition at line 113 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_PERIODIC 0x00002200 |
Definition at line 114 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_PERIODIC_UP 0x00003200 |
Definition at line 115 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_B_PWM 0x00000A00 |
Definition at line 120 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_ONE_SHOT 0x00000021 |
Definition at line 97 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_ONE_SHOT_UP 0x00000031 |
Definition at line 98 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_PERIODIC 0x00000022 |
Definition at line 99 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_PERIODIC_UP 0x00000032 |
Definition at line 100 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_RTC 0x01000000 |
Definition at line 101 of file timer.h.
Referenced by TimerConfigure().
| #define TIMER_CFG_SPLIT_PAIR 0x04000000 |
Definition at line 102 of file timer.h.
Referenced by TimerConfigure().