Functions | |
| void | TRNGConfigure (uint32_t ui32MinSamplesPerCycle, uint32_t ui32MaxSamplesPerCycle, uint32_t ui32ClocksPerSample) |
| Configure the true random number generator. More... | |
| __STATIC_INLINE void | TRNGEnable (void) |
| Enable the TRNG. More... | |
| __STATIC_INLINE void | TRNGDisable (void) |
| Disable the TRNG module. More... | |
| uint32_t | TRNGNumberGet (uint32_t ui32Word) |
| Get a random number from the generator. More... | |
| __STATIC_INLINE uint32_t | TRNGStatusGet (void) |
| Get the status of the TRNG. More... | |
| __STATIC_INLINE void | TRNGReset (void) |
| Reset the TRNG. More... | |
| __STATIC_INLINE void | TRNGIntEnable (uint32_t ui32IntFlags) |
| Enables individual TRNG interrupt sources. More... | |
| __STATIC_INLINE void | TRNGIntDisable (uint32_t ui32IntFlags) |
| Disables individual TRNG interrupt sources. More... | |
| __STATIC_INLINE uint32_t | TRNGIntStatus (bool bMasked) |
| Gets the current interrupt status of the TRNG module. More... | |
| __STATIC_INLINE void | TRNGIntClear (uint32_t ui32IntFlags) |
| Clears TRNG interrupt sources. More... | |
| __STATIC_INLINE void | TRNGIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for a TRNG interrupt. More... | |
| __STATIC_INLINE void | TRNGIntUnregister (void) |
| Unregisters an interrupt handler for a TRNG interrupt. More... | |
| void TRNGConfigure | ( | uint32_t | ui32MinSamplesPerCycle, |
| uint32_t | ui32MaxSamplesPerCycle, | ||
| uint32_t | ui32ClocksPerSample | ||
| ) |
Configure the true random number generator.
Use this function to set the minimum and maximum number of samples required in each generation of a new random number.
| ui32MinSamplesPerCycle | is the minimum number of samples pr. each generated random number. |
| ui32MaxSamplesPerCycle | is the maximum number of samples pr. each generated random number |
| ui32ClocksPerSample | defines the number of clocs cycles for each time a new sample is generated from the FROs. |
| __STATIC_INLINE void TRNGDisable | ( | void | ) |
| __STATIC_INLINE void TRNGEnable | ( | void | ) |
| __STATIC_INLINE void TRNGIntClear | ( | uint32_t | ui32IntFlags | ) |
Clears TRNG interrupt sources.
The specified TRNG interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being recognized again immediately upon exit.
| ui32IntFlags | is a bit mask of the interrupt sources to be cleared. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE void TRNGIntDisable | ( | uint32_t | ui32IntFlags | ) |
Disables individual TRNG interrupt sources.
This function disables the indicated TRNG interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32IntFlags | is the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE void TRNGIntEnable | ( | uint32_t | ui32IntFlags | ) |
Enables individual TRNG interrupt sources.
This function enables the indicated TRNG interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| ui32IntFlags | is the bit mask of the interrupt sources to be enabled. The parameter is the bitwise OR of any of the following: |
| __STATIC_INLINE void TRNGIntRegister | ( | void(*)(void) | pfnHandler | ) |
Registers an interrupt handler for a TRNG interrupt.
This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific UART interrupts must be enabled via TRNGIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source.
| pfnHandler | is a pointer to the function to be called when the UART interrupt occurs. |
| __STATIC_INLINE uint32_t TRNGIntStatus | ( | bool | bMasked | ) |
Gets the current interrupt status of the TRNG module.
This function returns the interrupt status for the specified TRNG. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| bMasked | selects either raw or masked interrupt status.
|
| __STATIC_INLINE void TRNGIntUnregister | ( | void | ) |
Unregisters an interrupt handler for a TRNG interrupt.
This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a Crypto interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
| uint32_t TRNGNumberGet | ( | uint32_t | ui32Word | ) |
Get a random number from the generator.
Use this function to get either the high or low part of the 64 bit generated number.
| ui32Word | determines if whether to return the high or low 32 bits. |
| __STATIC_INLINE void TRNGReset | ( | void | ) |
| __STATIC_INLINE uint32_t TRNGStatusGet | ( | void | ) |
Get the status of the TRNG.
Use this function to retrieve the status of the TRNG.
| #define TRNG_FRO_SHUTDOWN 0x00000002 |
Definition at line 96 of file trng.h.
Referenced by TRNGIntClear(), TRNGIntDisable(), and TRNGIntEnable().
| #define TRNG_HI_WORD 0x00000001 |
Definition at line 99 of file trng.h.
Referenced by TRNGNumberGet().
| #define TRNG_LOW_WORD 0x00000002 |
Definition at line 100 of file trng.h.
Referenced by TRNGNumberGet().
| #define TRNG_NUMBER_READY 0x00000001 |
Definition at line 95 of file trng.h.
Referenced by TRNGIntClear(), TRNGIntDisable(), and TRNGIntEnable().