Data Structures | |
| struct | tDMAControlTable |
| A structure that defines an entry in the channel control table. More... | |
Functions | |
| __STATIC_INLINE void | uDMAEnable (uint32_t ui32Base) |
| Enables the uDMA controller for use. More... | |
| __STATIC_INLINE void | uDMADisable (uint32_t ui32Base) |
| Disables the uDMA controller for use. More... | |
| __STATIC_INLINE uint32_t | uDMAErrorStatusGet (uint32_t ui32Base) |
| Gets the uDMA error status. More... | |
| __STATIC_INLINE void | uDMAErrorStatusClear (uint32_t ui32Base) |
| Clears the uDMA error interrupt. More... | |
| __STATIC_INLINE void | uDMAChannelEnable (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Enables a uDMA channel for operation. More... | |
| __STATIC_INLINE void | uDMAChannelDisable (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Disables a uDMA channel for operation. More... | |
| __STATIC_INLINE bool | uDMAChannelIsEnabled (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Checks if a uDMA channel is enabled for operation. More... | |
| __STATIC_INLINE void | uDMAControlBaseSet (uint32_t ui32Base, void *pControlTable) |
| Sets the base address for the channel control table. More... | |
| __STATIC_INLINE void * | uDMAControlBaseGet (uint32_t ui32Base) |
| Gets the base address for the channel control table. More... | |
| __STATIC_INLINE void * | uDMAControlAlternateBaseGet (uint32_t ui32Base) |
| Gets the base address for the channel control table alternate structures. More... | |
| __STATIC_INLINE void | uDMAChannelRequest (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Requests a uDMA channel to start a transfer. More... | |
| void | uDMAChannelAttributeEnable (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr) |
| Enables attributes of a uDMA channel. More... | |
| void | uDMAChannelAttributeDisable (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr) |
| Disables attributes of an uDMA channel. More... | |
| uint32_t | uDMAChannelAttributeGet (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Gets the enabled attributes of a uDMA channel. More... | |
| void | uDMAChannelControlSet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Control) |
| Sets the control parameters for a uDMA channel control structure. More... | |
| void | uDMAChannelTransferSet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Mode, void *pvSrcAddr, void *pvDstAddr, uint32_t ui32TransferSize) |
| Sets the transfer parameters for a uDMA channel control structure. More... | |
| void | uDMAChannelScatterGatherSet (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32TaskCount, void *pvTaskList, uint32_t ui32IsPeriphSG) |
| Configures a uDMA channel for scatter-gather mode. More... | |
| uint32_t | uDMAChannelSizeGet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex) |
| Gets the current transfer size for a uDMA channel control structure. More... | |
| uint32_t | uDMAChannelModeGet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex) |
| Gets the transfer mode for a uDMA channel control structure. More... | |
| __STATIC_INLINE void | uDMAIntRegister (uint32_t ui32Base, uint32_t ui32IntChannel, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the uDMA controller. More... | |
| __STATIC_INLINE void | uDMAIntUnregister (uint32_t ui32Base, uint32_t ui32IntChannel) |
| Unregisters an interrupt handler for the uDMA controller. More... | |
| __STATIC_INLINE void | uDMAIntClear (uint32_t ui32Base, uint32_t ui32ChanMask) |
| Clears uDMA interrupt done status. More... | |
| __STATIC_INLINE uint32_t | uDMAIntStatus (uint32_t ui32Base) |
| Get the uDMA interrupt status. More... | |
| __STATIC_INLINE void | uDMAIntSwEventEnable (uint32_t ui32Base, uint32_t ui32IntChannel) |
| Enable interrupt on software event driven uDMA transfers. More... | |
| __STATIC_INLINE void | uDMAIntSwEventDisable (uint32_t ui32Base, uint32_t ui32IntChannel) |
| Disable interrupt on software event driven uDMA transfers. More... | |
| __STATIC_INLINE uint32_t | uDMAGetStatus (uint32_t ui32Base) |
| Return the status of the uDMA module. More... | |
| __STATIC_INLINE void | uDMAChannelPrioritySet (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Set the priority of a uDMA channel. More... | |
| __STATIC_INLINE bool | uDMAChannelPriorityGet (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Get the priority of a uDMA channel. More... | |
| __STATIC_INLINE void | uDMAChannelPriorityClear (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Clear the priority of a uDMA channel. More... | |
| void uDMAChannelAttributeDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum, | ||
| uint32_t | ui32Attr | ||
| ) |
Disables attributes of an uDMA channel.
This function is used to disable attributes of a uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel to configure. |
| ui32Attr | is a combination of attributes for the channel. The parameter is the bitwise OR of any of the following:
|
| void uDMAChannelAttributeEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum, | ||
| uint32_t | ui32Attr | ||
| ) |
Enables attributes of a uDMA channel.
This function is used to enable attributes of a uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel to configure. |
| ui32Attr | is a combination of attributes for the channel. The parameter is the bitwise OR of any of the following:
|
| uint32_t uDMAChannelAttributeGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Gets the enabled attributes of a uDMA channel.
This function returns a combination of flags representing the attributes of the uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel to configure. |
| void uDMAChannelControlSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelStructIndex, | ||
| uint32_t | ui32Control | ||
| ) |
Sets the control parameters for a uDMA channel control structure.
This function is used to set control parameters for a uDMA transfer. These are typically parameters that are not changed often.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelStructIndex | is the bitwise OR of the uDMA channel number and:
|
| ui32Control | is the bitwise OR of five values:
|
| __STATIC_INLINE void uDMAChannelDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Disables a uDMA channel for operation.
This function disables a specific uDMA channel. Once disabled, a channel will not respond to uDMA transfer requests until re-enabled via uDMAChannelEnable().
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel number to disable. |
| __STATIC_INLINE void uDMAChannelEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Enables a uDMA channel for operation.
This function enables a specific uDMA channel for use. This function must be used to enable a channel before it can be used to perform a uDMA transfer.
When a uDMA transfer is completed, the channel will be automatically disabled by the uDMA controller. Therefore, this function should be called prior to starting up any new transfer.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel number to enable. |
| __STATIC_INLINE bool uDMAChannelIsEnabled | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Checks if a uDMA channel is enabled for operation.
This function checks to see if a specific uDMA channel is enabled. This can be used to check the status of a transfer, since the channel will be automatically disabled at the end of a transfer.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel number to check. |
true : Channel is enabled.false : Disabled. | uint32_t uDMAChannelModeGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelStructIndex | ||
| ) |
Gets the transfer mode for a uDMA channel control structure.
This function is used to get the transfer mode for the uDMA channel. It can be used to query the status of a transfer on a channel. When the transfer is complete the mode will be UDMA_MODE_STOP.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelStructIndex | is the bitwise OR of the uDMA channel number and: |
| __STATIC_INLINE void uDMAChannelPriorityClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Clear the priority of a uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | The uDMA channel to clear the priority for. |
| __STATIC_INLINE bool uDMAChannelPriorityGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Get the priority of a uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | The uDMA channel to get the priority for. |
| __STATIC_INLINE void uDMAChannelPrioritySet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Set the priority of a uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is uDMA channel to set the priority for. |
| __STATIC_INLINE void uDMAChannelRequest | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum | ||
| ) |
Requests a uDMA channel to start a transfer.
This function allows software to request a uDMA channel to begin a transfer. This could be used for performing a memory to memory transfer, or if for some reason a transfer needs to be initiated by software instead of the peripheral associated with that channel.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the channel number on which to request a uDMA transfer. |
| void uDMAChannelScatterGatherSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelNum, | ||
| uint32_t | ui32TaskCount, | ||
| void * | pvTaskList, | ||
| uint32_t | ui32IsPeriphSG | ||
| ) |
Configures a uDMA channel for scatter-gather mode.
This function is used to configure a channel for scatter-gather mode. The caller must have already set up a task list, and pass a pointer to the start of the task list as the pvTaskList parameter.
The ui32TaskCount parameter is the count of tasks in the task list, not the size of the task list.
The flag bIsPeriphSG should be used to indicate if the scatter-gather should be configured for a peripheral or memory scatter-gather operation.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelNum | is the uDMA channel number. |
| ui32TaskCount | is the number of scatter-gather tasks to execute. |
| pvTaskList | is a pointer to the beginning of the scatter-gather task list. |
| ui32IsPeriphSG | is a flag to indicate it is a peripheral scatter-gather transfer (else it will be memory scatter-gather transfer) |
| uint32_t uDMAChannelSizeGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelStructIndex | ||
| ) |
Gets the current transfer size for a uDMA channel control structure.
This function is used to get the uDMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items will be returned. If the transfer is complete, then 0 will be returned.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelStructIndex | is the bitwise OR of the uDMA channel number and: |
| void uDMAChannelTransferSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChannelStructIndex, | ||
| uint32_t | ui32Mode, | ||
| void * | pvSrcAddr, | ||
| void * | pvDstAddr, | ||
| uint32_t | ui32TransferSize | ||
| ) |
Sets the transfer parameters for a uDMA channel control structure.
This function is used to set the parameters for a uDMA transfer. These are typically parameters that are changed often. The function uDMAChannelControlSet() MUST be called at least once for this channel prior to calling this function.
The pvSrcAddr and pvDstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler will take care of this if the pointers are pointing to storage of the appropriate data type.
The two scatter/gather modes, MEMORY and PERIPHERAL, are actually different depending on whether the primary or alternate control structure is selected. This function will look for the UDMA_PRI_SELECT and UDMA_ALT_SELECT flag along with the channel number and will set the scatter/gather mode as appropriate for the primary or alternate control structure.
The channel must also be enabled using uDMAChannelEnable() after calling this function. The transfer will not begin until the channel has been set up and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that uDMAChannelEnable() must be called again after setting up the next transfer.
| ui32Base | is the base address of the uDMA port. |
| ui32ChannelStructIndex | is the bitwise OR of the uDMA channel number and:
|
| ui32Mode | is the type of uDMA transfer. The parameter should be one of the following values:
|
| pvSrcAddr | is the source address for the transfer. |
| pvDstAddr | is the destination address for the transfer. |
| ui32TransferSize | is the number of data items to transfer (NOT bytes). |
| __STATIC_INLINE void* uDMAControlAlternateBaseGet | ( | uint32_t | ui32Base | ) |
Gets the base address for the channel control table alternate structures.
This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.
| ui32Base | is the base address of the uDMA port. |
| __STATIC_INLINE void* uDMAControlBaseGet | ( | uint32_t | ui32Base | ) |
Gets the base address for the channel control table.
This function gets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel.
| ui32Base | is the base address of the uDMA port. |
| __STATIC_INLINE void uDMAControlBaseSet | ( | uint32_t | ui32Base, |
| void * | pControlTable | ||
| ) |
Sets the base address for the channel control table.
This function sets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel. The table must be aligned on a 1024 byte boundary. The base address must be set before any of the channel functions can be used. Setting the base address of the primary control table will automatically set the address for the alternate control table as the next memory location after the primary control table.
The size of the channel control table depends on the number of uDMA channels, and which transfer modes are used. Refer to the introductory text and the microcontroller datasheet for more information about the channel control table.
| ui32Base | is the base address of the uDMA port. |
| pControlTable | is a pointer to the 1024 byte aligned base address of the uDMA channel control table. The address must be an absolute address in system memory space. |
| __STATIC_INLINE void uDMADisable | ( | uint32_t | ui32Base | ) |
Disables the uDMA controller for use.
This function disables the uDMA controller. Once disabled, the uDMA controller will not operate until re-enabled with uDMAEnable().
| ui32Base | is the base address of the uDMA port. |
| __STATIC_INLINE void uDMAEnable | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void uDMAErrorStatusClear | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE uint32_t uDMAErrorStatusGet | ( | uint32_t | ui32Base | ) |
Gets the uDMA error status.
This function returns the uDMA error status. It should be called from within the uDMA error interrupt handler to determine if a uDMA error occurred.
| ui32Base | is the base address of the uDMA port. |
| __STATIC_INLINE uint32_t uDMAGetStatus | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void uDMAIntClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32ChanMask | ||
| ) |
Clears uDMA interrupt done status.
Clears bits in the uDMA interrupt status register according to which bits are set in ui32ChanMask. There is one bit for each channel. If a a bit is set in ui32ChanMask, then that corresponding channel's interrupt status will be cleared (if it was set).
| ui32Base | is the base address of the uDMA port. |
| ui32ChanMask | is a 32-bit mask with one bit for each uDMA channel. |
| __STATIC_INLINE void uDMAIntRegister | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntChannel, | ||
| void(*)(void) | pfnHandler | ||
| ) |
Registers an interrupt handler for the uDMA controller.
This sets and enables the handler to be called when the uDMA controller generates an interrupt.
| ui32Base | is the base address of the uDMA port. |
| ui32IntChannel | identifies which uDMA interrupt is to be registered.
|
| pfnHandler | is a pointer to the function to be called when the interrupt is activated. |
| __STATIC_INLINE uint32_t uDMAIntStatus | ( | uint32_t | ui32Base | ) |
| __STATIC_INLINE void uDMAIntSwEventDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntChannel | ||
| ) |
Disable interrupt on software event driven uDMA transfers.
This register disables the blocking of the uDMA status signals propagation to the hardware peripheral connected to the uDMA on the ui32IntChannel.
| ui32Base | is the base address of the uDMA port. |
| ui32IntChannel | identifies which uDMA interrupt to disable software interrupts for. |
| __STATIC_INLINE void uDMAIntSwEventEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntChannel | ||
| ) |
Enable interrupt on software event driven uDMA transfers.
| ui32Base | is the base address of the uDMA port. |
| ui32IntChannel | identifies which uDMA interrupt to enable software interrupts for. |
| __STATIC_INLINE void uDMAIntUnregister | ( | uint32_t | ui32Base, |
| uint32_t | ui32IntChannel | ||
| ) |
Unregisters an interrupt handler for the uDMA controller.
This function will disable and clear the handler to be called for the specified uDMA interrupt.
| ui32Base | is the base address of the uDMA port. |
| ui32IntChannel | identifies which uDMA interrupt to unregister.
|
| #define UDMA_ALT_SELECT 0x00000020 |
Definition at line 321 of file udma.h.
Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| #define UDMA_ARB_4 0x00008000 |
Definition at line 270 of file udma.h.
Referenced by uDMAChannelScatterGatherSet().
| #define UDMA_ARB_M 0x0003C000 |
Definition at line 279 of file udma.h.
Referenced by uDMAChannelControlSet().
| #define UDMA_ATTR_ALTSELECT 0x00000002 |
Definition at line 224 of file udma.h.
Referenced by uDMAChannelAttributeDisable(), uDMAChannelAttributeEnable(), and uDMAChannelAttributeGet().
| #define UDMA_ATTR_HIGH_PRIORITY 0x00000004 |
Definition at line 225 of file udma.h.
Referenced by uDMAChannelAttributeDisable(), uDMAChannelAttributeEnable(), and uDMAChannelAttributeGet().
| #define UDMA_ATTR_REQMASK 0x00000008 |
Definition at line 226 of file udma.h.
Referenced by uDMAChannelAttributeDisable(), uDMAChannelAttributeEnable(), and uDMAChannelAttributeGet().
| #define UDMA_ATTR_USEBURST 0x00000001 |
Definition at line 223 of file udma.h.
Referenced by uDMAChannelAttributeDisable(), uDMAChannelAttributeEnable(), and uDMAChannelAttributeGet().
| #define UDMA_DST_INC_32 0x80000000 |
Definition at line 253 of file udma.h.
Referenced by uDMAChannelScatterGatherSet().
| #define UDMA_DST_INC_M 0xC0000000 |
Definition at line 255 of file udma.h.
Referenced by uDMAChannelControlSet(), and uDMAChannelTransferSet().
| #define UDMA_DST_INC_NONE 0xC0000000 |
Definition at line 254 of file udma.h.
Referenced by uDMAChannelTransferSet().
| #define UDMA_DST_INC_S 30 |
Definition at line 256 of file udma.h.
Referenced by uDMAChannelTransferSet().
| #define UDMA_MODE_ALT_SELECT 0x00000001 |
Definition at line 244 of file udma.h.
Referenced by uDMAChannelModeGet(), and uDMAChannelTransferSet().
| #define UDMA_MODE_M 0x00000007 |
Definition at line 243 of file udma.h.
Referenced by uDMAChannelModeGet(), uDMAChannelSizeGet(), and uDMAChannelTransferSet().
| #define UDMA_MODE_MEM_SCATTER_GATHER 0x00000004 |
Definition at line 239 of file udma.h.
Referenced by uDMAChannelModeGet(), uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| #define UDMA_MODE_PER_SCATTER_GATHER 0x00000006 |
Definition at line 241 of file udma.h.
Referenced by uDMAChannelModeGet(), uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| #define UDMA_NEXT_USEBURST 0x00000008 |
Definition at line 281 of file udma.h.
Referenced by uDMAChannelControlSet().
| #define UDMA_NUM_CHANNELS 21 |
Definition at line 207 of file udma.h.
Referenced by uDMAChannelAttributeDisable(), uDMAChannelAttributeEnable(), uDMAChannelAttributeGet(), uDMAChannelControlSet(), uDMAChannelDisable(), uDMAChannelEnable(), uDMAChannelIsEnabled(), uDMAChannelModeGet(), uDMAChannelPriorityClear(), uDMAChannelPriorityGet(), uDMAChannelPrioritySet(), uDMAChannelRequest(), uDMAChannelScatterGatherSet(), uDMAChannelSizeGet(), uDMAChannelTransferSet(), uDMAIntSwEventDisable(), and uDMAIntSwEventEnable().
| #define UDMA_PRIORITY_HIGH 0x00000001 |
Definition at line 215 of file udma.h.
Referenced by uDMAChannelPriorityGet().
| #define UDMA_PRIORITY_LOW 0x00000000 |
Definition at line 214 of file udma.h.
Referenced by uDMAChannelPriorityGet().
| #define UDMA_SIZE_32 0x22000000 |
Definition at line 265 of file udma.h.
Referenced by uDMAChannelScatterGatherSet().
| #define UDMA_SIZE_M 0x33000000 |
Definition at line 266 of file udma.h.
Referenced by uDMAChannelControlSet().
| #define UDMA_SRC_INC_32 0x08000000 |
Definition at line 259 of file udma.h.
Referenced by uDMAChannelScatterGatherSet().
| #define UDMA_SRC_INC_M 0x0C000000 |
Definition at line 261 of file udma.h.
Referenced by uDMAChannelControlSet(), and uDMAChannelTransferSet().
| #define UDMA_SRC_INC_NONE 0x0c000000 |
Definition at line 260 of file udma.h.
Referenced by uDMAChannelTransferSet().
| #define UDMA_SRC_INC_S 26 |
Definition at line 262 of file udma.h.
Referenced by uDMAChannelTransferSet().
| #define UDMA_XFER_SIZE_M 0x00003FF0 |
Definition at line 283 of file udma.h.
Referenced by uDMAChannelSizeGet(), and uDMAChannelTransferSet().
| #define UDMA_XFER_SIZE_MAX 1024 |
Definition at line 282 of file udma.h.
Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| #define UDMA_XFER_SIZE_S 4 |
Definition at line 284 of file udma.h.
Referenced by uDMAChannelScatterGatherSet(), uDMAChannelSizeGet(), and uDMAChannelTransferSet().
| #define uDMATaskStructEntry | ( | ui32TransferCount, | |
| ui32ItemSize, | |||
| ui32SrcIncrement, | |||
| pvSrcAddr, | |||
| ui32DstIncrement, | |||
| pvDstAddr, | |||
| ui32ArbSize, | |||
| ui32Mode | |||
| ) |
A helper macro for building scatter-gather task table entries.
This macro is intended to be used to help populate a table of uDMA tasks for a scatter-gather transfer. This macro will calculate the values for the fields of a task structure entry based on the input parameters.
There are specific requirements for the values of each parameter. No checking is done so it is up to the caller to ensure that correct values are used for the parameters.
This macro is intended to be used to initialize individual entries of a structure of tDMAControlTable type, like this:
tDMAControlTable MyTaskList[] =
{
uDMATaskStructEntry(Task1Count, UDMA_SIZE_8,
UDMA_SRC_INC_8, MySourceBuf,
UDMA_DST_INC_8, MyDestBuf,
UDMA_ARB_8, UDMA_MODE_MEM_SCATTER_GATHER),
uDMATaskStructEntry(Task2Count, ... ),
}
| ui32TransferCount | is the count of items to transfer for this task. It must be in the range 1-1024. |
| ui32ItemSize | is the bit size of the items to transfer for this task. It must be one of: |
| ui32SrcIncrement | is the bit size increment for source data. It must be one of: |
| pvSrcAddr | is the starting address of the data to transfer. |
| ui32DstIncrement | is the bit size increment for destination data. It must be one of: |
| pvDstAddr | is the starting address of the destination data. |
| ui32ArbSize | is the arbitration size to use for the transfer task. This is used to select the arbitration size in powers of 2, from 1 to 1024. It must be one of: |
| ui32Mode | is the transfer mode for this task. Note that normally all tasks will be one of the scatter-gather modes while the last task is a task list will be AUTO or BASIC. It must be one of: |