#include <driverlib/interrupt.h>Go to the source code of this file.
Functions | |
| void | IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void)) |
| Registers a function to be called when an interrupt occurs. More... | |
| void | IntUnregister (uint32_t ui32Interrupt) |
| Unregisters the function to be called when an interrupt occurs. More... | |
| void | IntPriorityGroupingSet (uint32_t ui32Bits) |
| Sets the priority grouping of the interrupt controller. More... | |
| uint32_t | IntPriorityGroupingGet (void) |
| Gets the priority grouping of the interrupt controller. More... | |
| void | IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority) |
| Sets the priority of an interrupt. More... | |
| int32_t | IntPriorityGet (uint32_t ui32Interrupt) |
| Gets the priority of an interrupt. More... | |
| void | IntEnable (uint32_t ui32Interrupt) |
| Enables an interrupt. More... | |
| void | IntDisable (uint32_t ui32Interrupt) |
| Disables an interrupt. More... | |
| void | IntPendSet (uint32_t ui32Interrupt) |
| Pends an interrupt. More... | |
| bool | IntPendGet (uint32_t ui32Interrupt) |
| Query whether an interrupt is pending. More... | |
| void | IntPendClear (uint32_t ui32Interrupt) |
| Unpends an interrupt. More... | |
Variables | |
| void(* | g_pfnRAMVectors [NUM_INTERRUPTS])(void) |
| void(* g_pfnRAMVectors[NUM_INTERRUPTS])(void) |
Definition at line 141 of file interrupt.c.
Referenced by IntRegister(), and IntUnregister().