#include <stdbool.h>#include <stdint.h>#include <inc/hw_ints.h>#include <inc/hw_types.h>#include <inc/hw_nvic.h>#include <driverlib/debug.h>#include <driverlib/cpu.h>Go to the source code of this file.
Macros | |
| #define | INT_PRIORITY_MASK 0x000000E0 |
| #define | INT_PRI_LEVEL0 0x00000000 |
| #define | INT_PRI_LEVEL1 0x00000020 |
| #define | INT_PRI_LEVEL2 0x00000040 |
| #define | INT_PRI_LEVEL3 0x00000060 |
| #define | INT_PRI_LEVEL4 0x00000080 |
| #define | INT_PRI_LEVEL5 0x000000A0 |
| #define | INT_PRI_LEVEL6 0x000000C0 |
| #define | INT_PRI_LEVEL7 0x000000E0 |
Functions | |
| __STATIC_INLINE bool | IntMasterEnable (void) |
| Enables the processor interrupt. More... | |
| __STATIC_INLINE bool | IntMasterDisable (void) |
| Disables the processor interrupt. More... | |
| void | IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void)) |
| Registers a function to be called when an interrupt occurs. More... | |
| void | IntUnregister (uint32_t ui32Interrupt) |
| Unregisters the function to be called when an interrupt occurs. More... | |
| void | IntPriorityGroupingSet (uint32_t ui32Bits) |
| Sets the priority grouping of the interrupt controller. More... | |
| uint32_t | IntPriorityGroupingGet (void) |
| Gets the priority grouping of the interrupt controller. More... | |
| void | IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority) |
| Sets the priority of an interrupt. More... | |
| int32_t | IntPriorityGet (uint32_t ui32Interrupt) |
| Gets the priority of an interrupt. More... | |
| void | IntEnable (uint32_t ui32Interrupt) |
| Enables an interrupt. More... | |
| void | IntDisable (uint32_t ui32Interrupt) |
| Disables an interrupt. More... | |
| void | IntPendSet (uint32_t ui32Interrupt) |
| Pends an interrupt. More... | |
| bool | IntPendGet (uint32_t ui32Interrupt) |
| Query whether an interrupt is pending. More... | |
| void | IntPendClear (uint32_t ui32Interrupt) |
| Unpends an interrupt. More... | |
| __STATIC_INLINE void | IntPriorityMaskSet (uint32_t ui32PriorityMask) |
| Sets the priority masking level. More... | |
| __STATIC_INLINE uint32_t | IntPriorityMaskGet (void) |
| Gets the priority masking level. More... | |