#include <driverlib/ioc.h>Go to the source code of this file.
Functions | |
| void | IOCPortConfigureSet (uint32_t ui32IOId, uint32_t ui32PortId, uint32_t ui32IOConfig) |
| Set the configuration of an IO port. More... | |
| uint32_t | IOCPortConfigureGet (uint32_t ui32IOId) |
| Get the configuration of an IO port. More... | |
| void | IOCIOShutdownSet (uint32_t ui32IOId, uint32_t ui32IOShutdown) |
| Set wake-up on an IO port. More... | |
| void | IOCIOModeSet (uint32_t ui32IOId, uint32_t ui32IOMode) |
| Set the IO Mode of an IO Port. More... | |
| void | IOCIOIntSet (uint32_t ui32IOId, uint32_t ui32Int, uint32_t ui32EdgeDet) |
| Setup interrupt detection on an IO Port. More... | |
| void | IOCIOPortPullSet (uint32_t ui32IOId, uint32_t ui32Pull) |
| Set the pull on an IO port. More... | |
| void | IOCIOHystSet (uint32_t ui32IOId, uint32_t ui32Hysteresis) |
| Configure hysteresis on and IO port. More... | |
| void | IOCIOInputSet (uint32_t ui32IOId, uint32_t ui32Input) |
| Enable/disable IO port as input. More... | |
| void | IOCIOSlewCtrlSet (uint32_t ui32IOId, uint32_t ui32SlewEnable) |
| Enable/disable the slew control on an IO port. More... | |
| void | IOCIODrvStrengthSet (uint32_t ui32IOId, uint32_t ui32IOCurrent, uint32_t ui32DrvStrength) |
| Configure the drive strength and maxium current of an IO port. More... | |
| void | IOCIOPortIdSet (uint32_t ui32IOId, uint32_t ui32PortId) |
| Setup the Port ID for this IO. More... | |
| void | IOCIntEnable (uint32_t ui32IOId) |
| Enables individual IO edge detect interrupt. More... | |
| void | IOCIntDisable (uint32_t ui32IOId) |
| Disables individual IO edge interrupt sources. More... | |
| void | IOCPinTypeGpioInput (uint32_t ui32IOId) |
| Setup an IO for standard GPIO input. More... | |
| void | IOCPinTypeGpioOutput (uint32_t ui32IOId) |
| Setup an IO for standard GPIO output. More... | |
| void | IOCPinTypeUart (uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Cts, uint32_t ui32Rts) |
| Configure a set of IOs for standard UART peripheral control. More... | |
| void | IOCPinTypeSsiMaster (uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk) |
| Configure a set of IOs for standard SSI peripheral master control. More... | |
| void | IOCPinTypeSsiSlave (uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk) |
| Configure a set of IOs for standard SSI peripheral slave control. More... | |
| void | IOCPinTypeI2c (uint32_t ui32Base, uint32_t ui32Data, uint32_t ui32Clk) |
| Configure a set of IOs for standard I2C peripheral control. More... | |
| void | IOCPinTypeSpis (uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk) |
| Configure a set of IOs for standard SPIS peripheral control. More... | |
| void | IOCPinTypeAux (uint32_t ui32IOId) |
| Configure an IO for AUX control. More... | |