#include <inc/hw_types.h>#include <inc/hw_ccfg.h>#include <driverlib/aon_batmon.h>#include <driverlib/aon_rtc.h>#include <driverlib/osc.h>Go to the source code of this file.
Data Structures | |
| struct | OscHfGlobals_t |
Macros | |
| #define | RTC_CV_TO_MS(x) (( 1000 * ( x )) >> 16 ) |
| #define | RTC_CV_TO_US(x) (( 1000000 * ( x )) >> 16 ) |
Functions | |
| void | OSCClockSourceSet (uint32_t ui32SrcClk, uint32_t ui32Osc) |
| Configure the oscillator input to the a source clock. More... | |
| uint32_t | OSCClockSourceGet (uint32_t ui32SrcClk) |
| Get the source clock settings. More... | |
| void | OSCInterfaceEnable (void) |
| Enable CM3 access to the OSC_DIG module. More... | |
| uint32_t | OSCHF_GetStartupTime (uint32_t timeUntilWakeupInMs) |
| Returns maximum startup time (in microseconds) of XOSC_HF. More... | |
| void | OSCHF_TurnOnXosc (void) |
| Turns on XOSC_HF (but without switching to XOSC_HF). More... | |
| bool | OSCHF_AttemptToSwitchToXosc (void) |
| Switch to XOSC_HF if XOSC_HF is ready. More... | |
| void | OSCHF_SwitchToRcOscTurnOffXosc (void) |
| Switch to RCOSC_HF and turn off XOSC_HF. More... | |
| #define RTC_CV_TO_MS | ( | x | ) | (( 1000 * ( x )) >> 16 ) |
Definition at line 66 of file osc.c.
Referenced by OSCHF_GetStartupTime().
| #define RTC_CV_TO_US | ( | x | ) | (( 1000000 * ( x )) >> 16 ) |
Definition at line 67 of file osc.c.
Referenced by OSCHF_AttemptToSwitchToXosc(), and OSCHF_GetStartupTime().