#include <driverlib/prcm.h>Go to the source code of this file.
Macros | |
| #define | PRCM_PERIPH_INDEX(a) (((a) >> 8) & 0xf) |
| #define | PRCM_PERIPH_MASKBIT(a) (0x00000001 << ((a) & 0xf)) |
Functions | |
| void | PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode) |
| Configure the infrastructure clock. More... | |
| uint32_t | PRCMInfClockConfigureGet (uint32_t ui32PowerMode) |
| Use this function to retreive the set infrastructure clock configuration. More... | |
| void | PRCMClockConfigureSet (uint32_t ui32Domains, uint32_t ui32ClkDiv) |
| Setup the clock division factor for a subsystem in the MCU voltage domain. More... | |
| uint32_t | PRCMClockConfigureGet (uint32_t ui32Domain) |
| Get the clock configuration for a specific sub system in the MCU Voltage Domain. More... | |
| void | PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate) |
| Configure the audio clock generation. More... | |
| void | PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv) |
| Configure the audio clock generation with manual setting of clock divider. More... | |
| void | PRCMPowerDomainOn (uint32_t ui32Domains) |
| Turn power on in power domains in the MCU domain. More... | |
| void | PRCMPowerDomainOff (uint32_t ui32Domains) |
| Turn off a specific power domain. More... | |
| void | PRCMPeripheralRunEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in Run mode. More... | |
| void | PRCMPeripheralRunDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in Run mode. More... | |
| void | PRCMPeripheralSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in deep-sleep mode. More... | |
| void | PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in deep-sleep mode. More... | |
| uint32_t | PRCMPowerDomainStatus (uint32_t ui32Domains) |
| Get the status for a specific power domain. More... | |
| void | PRCMDeepSleep (void) |
| Put the processor into deep-sleep mode. More... | |
| void | PRCMRetentionEnable (uint32_t ui32PowerDomain) |
| Enable retention on specific power domains. More... | |
| void | PRCMRetentionDisable (uint32_t ui32PowerDomain) |
| Disable retention on power domains. More... | |
| #define PRCM_PERIPH_INDEX | ( | a | ) | (((a) >> 8) & 0xf) |
Definition at line 136 of file prcm.c.
Referenced by PRCMPeripheralDeepSleepDisable(), PRCMPeripheralDeepSleepEnable(), PRCMPeripheralRunDisable(), PRCMPeripheralRunEnable(), PRCMPeripheralSleepDisable(), and PRCMPeripheralSleepEnable().
| #define PRCM_PERIPH_MASKBIT | ( | a | ) | (0x00000001 << ((a) & 0xf)) |
Definition at line 143 of file prcm.c.
Referenced by PRCMPeripheralDeepSleepDisable(), PRCMPeripheralDeepSleepEnable(), PRCMPeripheralRunDisable(), PRCMPeripheralRunEnable(), PRCMPeripheralSleepDisable(), and PRCMPeripheralSleepEnable().