#include <driverlib/pwr_ctrl.h>Go to the source code of this file.
Functions | |
| void | PowerCtrlStateSet (uint32_t ui32Powerstate) |
| Force the system in to low power modes. More... | |
| void | PowerCtrlSourceSet (uint32_t ui32PowerConfig) |
| Set (Request) the main power source. More... | |