#include <inc/hw_memmap.h>
#include <inc/hw_types.h>
#include <inc/hw_adi.h>
#include <inc/hw_adi_0_rf.h>
#include <inc/hw_adi_1_synth.h>
#include <inc/hw_adi_2_refsys.h>
#include <inc/hw_adi_3_refsys.h>
#include <inc/hw_adi_4_aux.h>
#include <inc/hw_aon_ioc.h>
#include <inc/hw_aon_sysctl.h>
#include <inc/hw_aon_wuc.h>
#include <inc/hw_aux_wuc.h>
#include <inc/hw_ccfg.h>
#include <inc/hw_chip_def.h>
#include <inc/hw_ddi.h>
#include <inc/hw_fcfg1.h>
#include <inc/hw_ddi_0_osc.h>
#include <inc/hw_prcm.h>
#include <inc/hw_vims.h>
#include <inc/hw_aon_batmon.h>
#include <inc/hw_aon_rtc.h>
#include <driverlib/adi.h>
#include <driverlib/cpu.h>
#include <driverlib/chipinfo.h>
#include <driverlib/ddi.h>
#include <driverlib/prcm.h>
#include <driverlib/sys_ctrl.h>
#include <driverlib/aon_batmon.h>
Go to the source code of this file.
| #define CLK_LF_RCOSC_LF 0xC00000 |
| #define CLK_LF_XOSC_HF 0x000000 |
| #define CLK_LF_XOSC_LF 0x800000 |
| #define CPU_DELAY_MICRO_SECONDS |
( |
|
x | ) |
CPUdelay(((uint32_t)((( x ) * 48.0 ) / 5.0 )) - 1 ) |
| #define DELAY_20_USEC 0x140 |
Defined time delay assuming 48 MHz clock and resolution of 3 cycles.
Definition at line 124 of file setup.c.
| #define INCLUDE_VDDR_TEMPORARILY 1 |
Perform the necessary trim of the device which is not done in boot code
This function should only execute coming from ROM boot. The current implementation does not take soft reset into account. However, it does no damage to execute it again. It only consumes time.
Definition at line 150 of file setup.c.