#include <driverlib/spis.h>Go to the source code of this file.
Functions | |
| void | SPISDataPut (uint32_t ui32Data) |
| Puts a data element into the SPIS transmit FIFO. More... | |
| uint32_t | SPISTxGetValue (uint32_t ui32Index) |
| Get a specific value in the Tx Fifo. More... | |
| void | SPISDataGet (uint32_t *pui32Data) |
| Gets a data element from the SPIS Rx FIFO. More... | |
| uint32_t | SPISRxGetValue (uint32_t ui32Index) |
| Get a specific value in the Rx Fifo. More... | |
| uint32_t | SPISIntStatus (bool bMasked) |
| Gets the current interrupt status. More... | |