|
| void | SSIConfigSetExpClk (uint32_t ui32Base, uint32_t ui32SSIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth) |
| | Configures the synchronous serial port. More...
|
| |
| __STATIC_INLINE void | SSIEnable (uint32_t ui32Base) |
| | Enables the synchronous serial port. More...
|
| |
| __STATIC_INLINE void | SSIDisable (uint32_t ui32Base) |
| | Disables the synchronous serial port. More...
|
| |
| void | SSIDataPut (uint32_t ui32Base, uint32_t ui32Data) |
| | Puts a data element into the SSI transmit FIFO. More...
|
| |
| int32_t | SSIDataPutNonBlocking (uint32_t ui32Base, uint32_t ui32Data) |
| | Puts a data element into the SSI transmit FIFO. More...
|
| |
| void | SSIDataGet (uint32_t ui32Base, uint32_t *pui32Data) |
| | Gets a data element from the SSI receive FIFO. More...
|
| |
| int32_t | SSIDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data) |
| | Gets a data element from the SSI receive FIFO. More...
|
| |
| __STATIC_INLINE bool | SSIBusy (uint32_t ui32Base) |
| | Determines whether the SSI transmitter is busy or not. More...
|
| |
| __STATIC_INLINE uint32_t | SSIStatus (uint32_t ui32Base) |
| | Get the status of the SSI data buffers. More...
|
| |
| void | SSIIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| | Registers an interrupt handler for the synchronous serial port. More...
|
| |
| void | SSIIntUnregister (uint32_t ui32Base) |
| | Unregisters an interrupt handler for the synchronous serial port. More...
|
| |
| __STATIC_INLINE void | SSIIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Enables individual SSI interrupt sources. More...
|
| |
| __STATIC_INLINE void | SSIIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Disables individual SSI interrupt sources. More...
|
| |
| __STATIC_INLINE void | SSIIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Clears SSI interrupt sources. More...
|
| |
| __STATIC_INLINE uint32_t | SSIIntStatus (uint32_t ui32Base, bool bMasked) |
| | Gets the current interrupt status. More...
|
| |
| __STATIC_INLINE void | SSIDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| | Enable SSI DMA operation. More...
|
| |
| __STATIC_INLINE void | SSIDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| | Disable SSI DMA operation. More...
|
| |