A structure that defines an entry in the channel control table. More...
#include <udma.h>
Data Fields | |
| volatile void * | pvSrcEndAddr |
| The ending source address of the data transfer. More... | |
| volatile void * | pvDstEndAddr |
| The ending destination address of the data transfer. More... | |
| volatile uint32_t | ui32Control |
| The channel control mode. More... | |
| volatile uint32_t | ui32Spare |
| An unused location. More... | |
A structure that defines an entry in the channel control table.
These fields are used by the uDMA controller and normally it is not necessary for software to directly read or write fields in the table.
| volatile void* tDMAControlTable::pvDstEndAddr |
The ending destination address of the data transfer.
Definition at line 106 of file udma.h.
Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| volatile void* tDMAControlTable::pvSrcEndAddr |
The ending source address of the data transfer.
Definition at line 105 of file udma.h.
Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().
| volatile uint32_t tDMAControlTable::ui32Control |
The channel control mode.
Definition at line 107 of file udma.h.
Referenced by uDMAChannelControlSet(), uDMAChannelModeGet(), uDMAChannelScatterGatherSet(), uDMAChannelSizeGet(), and uDMAChannelTransferSet().
| volatile uint32_t tDMAControlTable::ui32Spare |
An unused location.
Definition at line 108 of file udma.h.
Referenced by uDMAChannelScatterGatherSet().