#include <inc/hw_types.h>#include <inc/hw_ccfg.h>#include <driverlib/aon_batmon.h>#include <driverlib/sys_ctrl.h>Go to the source code of this file.
Data Structures | |
| struct | PowerQualGlobals_t |
Macros | |
| #define | PD_STATE_CACHE_RET 1 |
| #define | PD_STATE_RFMEM_RET 2 |
| #define | PD_STATE_XOSC_LPM 4 |
Functions | |
| void | SysCtrlPowerEverything (void) |
| Power up everything. More... | |
| void | SysCtrlStandby (void) |
| Force the system in to standby mode. More... | |
| void | SysCtrlPowerdown (void) |
| Force the system in to power down. More... | |
| void | SysCtrlShutdown (void) |
| Force the system in to shutdown. More... | |
| uint32_t | SysCtrlClockGet (void) |
| Get the CPU core clock frequency. More... | |
| uint32_t | SysCtrlPeripheralClockGet (uint32_t ui32Peripheral, uint32_t ui32BusMode) |
| Get the clock for a peripheral. More... | |
| void | SysCtrlSetRechargeBeforePowerDown (XoscPowerMode_t xoscPowerMode) |
| Set Recharge values before entering Power Down. More... | |
| void | SysCtrlAdjustRechargeAfterPowerDown (void) |
| Adjust Recharge calculations to be used next. More... | |
| void | SysCtrl_DCDC_VoltageConditionalControl (void) |
| Turns DCDC on or off depending of what’s considered to be optimal usage. More... | |
| uint32_t | SysCtrlResetSourceGet (void) |
| Returns last reset source (including "wakeup from shutdown") More... | |
| #define PD_STATE_CACHE_RET 1 |
Definition at line 75 of file sys_ctrl.c.
Referenced by SysCtrlSetRechargeBeforePowerDown().
| #define PD_STATE_RFMEM_RET 2 |
Definition at line 76 of file sys_ctrl.c.
Referenced by SysCtrlSetRechargeBeforePowerDown().
| #define PD_STATE_XOSC_LPM 4 |
Definition at line 77 of file sys_ctrl.c.
Referenced by SysCtrlSetRechargeBeforePowerDown().