Instance: AON_BATMON
Component: AON_BATMON
Base address: 0x40095000
Always On (AON) Battery And Temperature MONitor (BATMON) residing in the AON domain
Note: This module only supports 32 bit Read/Write access from MCU.
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4009 5000 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4009 5004 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4009 500C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x4009 5010 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x4009 5014 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x4009 5018 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4009 501C |
|
|
RW |
32 |
0x0000 0028 |
0x0000 0020 |
0x4009 5020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4009 5024 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0028 |
0x4009 5028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4009 502C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0030 |
0x4009 5030 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0x4009 5034 |
|
Address offset |
0x0000 0000 |
||
|
Physical address |
0x4009 5000 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:2 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x0000 0000 |
||
|
1 |
CALC_EN |
Internal |
RW |
0 |
||
|
0 |
MEAS_EN |
Internal |
RW |
0 |
||
|
Address offset |
0x0000 0004 |
||
|
Physical address |
0x4009 5004 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|||||||||||||||||||||
|
31:2 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x0000 0000 |
|||||||||||||||||||||
|
1:0 |
PER |
Internal
|
RW |
0x0 |
|||||||||||||||||||||
|
Address offset |
0x0000 000C |
||
|
Physical address |
0x4009 500C |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:8 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x00 0000 |
||
|
7:0 |
CFG |
Internal |
RW |
0x00 |
||
|
Address offset |
0x0000 0010 |
||
|
Physical address |
0x4009 5010 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:6 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x000 0000 |
||
|
5:0 |
CFG |
Internal |
RW |
0x00 |
||
|
Address offset |
0x0000 0014 |
||
|
Physical address |
0x4009 5014 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:5 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x000 0000 |
||
|
4:0 |
CFG |
Internal |
RW |
0x00 |
||
|
Address offset |
0x0000 0018 |
||
|
Physical address |
0x4009 5018 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:6 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x000 0000 |
||
|
5:0 |
CFG |
Internal |
RW |
0x00 |
||
|
Address offset |
0x0000 001C |
||
|
Physical address |
0x4009 501C |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:6 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x000 0000 |
||
|
5:0 |
CFG |
Internal |
RW |
0x00 |
||
|
Address offset |
0x0000 0020 |
||
|
Physical address |
0x4009 5020 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:6 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x000 0000 |
||
|
5:4 |
CFG2 |
Internal |
RW |
0x2 |
||
|
3:0 |
CFG1 |
Internal |
RW |
0x8 |
||
|
Address offset |
0x0000 0024 |
||
|
Physical address |
0x4009 5024 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:9 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x00 0000 |
||
|
8 |
FALLB |
Internal |
RW |
0 |
||
|
7:6 |
HIGHLIM |
Internal |
RW |
0x0 |
||
|
5 |
LOWLIM |
Internal |
RW |
0 |
||
|
4 |
OVR |
Internal |
RW |
0 |
||
|
3:0 |
CFG |
Internal |
RW |
0x0 |
||
|
Address offset |
0x0000 0028 |
||
|
Physical address |
0x4009 5028 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:11 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x00 0000 |
||
|
10:8 |
INT |
Internal |
RO |
0x0 |
||
|
7:0 |
FRAC |
Internal |
RO |
0x00 |
||
|
Address offset |
0x0000 002C |
||
|
Physical address |
0x4009 502C |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:1 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x0000 0000 |
||
|
0 |
STAT |
Internal |
RW |
0 |
||
|
Address offset |
0x0000 0030 |
||
|
Physical address |
0x4009 5030 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:17 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x0000 |
||
|
16:8 |
INT |
Internal |
RO |
0x000 |
||
|
7:6 |
FRAC |
Internal |
RO |
0x0 |
||
|
5:0 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x00 |
||
|
Address offset |
0x0000 0034 |
||
|
Physical address |
0x4009 5034 |
Instance |
AON_BATMON |
|
Description |
Internal Register. Customers can control this through TI provided API |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:1 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RO std text) |
RO |
0x0000 0000 |
||
|
0 |
STAT |
Internal |
RW |
0 |
||
| © 2015. Texas Instruments | All Rights Reserved |