Instance: CPU_ITM
Component: CPU_ITM
Base address: 0xe0000000
Cortex-M's Instrumentation Trace Macrocell (ITM)
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0xE000 0000 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0xE000 0004 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0xE000 0008 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0xE000 000C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE000 0010 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0xE000 0014 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0xE000 0018 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0xE000 001C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0xE000 0020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0xE000 0024 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0xE000 0028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0xE000 002C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0030 |
0xE000 0030 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0xE000 0034 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0038 |
0xE000 0038 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 003C |
0xE000 003C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0040 |
0xE000 0040 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0044 |
0xE000 0044 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0048 |
0xE000 0048 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 004C |
0xE000 004C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0050 |
0xE000 0050 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0054 |
0xE000 0054 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0058 |
0xE000 0058 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 005C |
0xE000 005C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0060 |
0xE000 0060 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0064 |
0xE000 0064 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0068 |
0xE000 0068 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 006C |
0xE000 006C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0070 |
0xE000 0070 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0074 |
0xE000 0074 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0078 |
0xE000 0078 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 007C |
0xE000 007C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0E00 |
0xE000 0E00 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0E40 |
0xE000 0E40 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0E80 |
0xE000 0E80 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0FB0 |
0xE000 0FB0 |
|
|
RO |
32 |
0x0000 0003 |
0x0000 0FB4 |
0xE000 0FB4 |
|
Address offset |
0x0000 0000 |
||
|
Physical address |
0xE000 0000 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM0 |
A write to this location causes data to be written into the FIFO if TER.STIMENA0 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0004 |
||
|
Physical address |
0xE000 0004 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 1 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM1 |
A write to this location causes data to be written into the FIFO if TER.STIMENA1 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0008 |
||
|
Physical address |
0xE000 0008 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 2 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM2 |
A write to this location causes data to be written into the FIFO if TER.STIMENA2 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 000C |
||
|
Physical address |
0xE000 000C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 3 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM3 |
A write to this location causes data to be written into the FIFO if TER.STIMENA3 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0010 |
||
|
Physical address |
0xE000 0010 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 4 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM4 |
A write to this location causes data to be written into the FIFO if TER.STIMENA4 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0014 |
||
|
Physical address |
0xE000 0014 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 5 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM5 |
A write to this location causes data to be written into the FIFO if TER.STIMENA5 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0018 |
||
|
Physical address |
0xE000 0018 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 6 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM6 |
A write to this location causes data to be written into the FIFO if TER.STIMENA6 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 001C |
||
|
Physical address |
0xE000 001C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 7 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM7 |
A write to this location causes data to be written into the FIFO if TER.STIMENA7 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0020 |
||
|
Physical address |
0xE000 0020 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 8 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM8 |
A write to this location causes data to be written into the FIFO if TER.STIMENA8 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0024 |
||
|
Physical address |
0xE000 0024 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 9 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM9 |
A write to this location causes data to be written into the FIFO if TER.STIMENA9 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0028 |
||
|
Physical address |
0xE000 0028 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 10 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM10 |
A write to this location causes data to be written into the FIFO if TER.STIMENA10 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 002C |
||
|
Physical address |
0xE000 002C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 11 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM11 |
A write to this location causes data to be written into the FIFO if TER.STIMENA11 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0030 |
||
|
Physical address |
0xE000 0030 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 12 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM12 |
A write to this location causes data to be written into the FIFO if TER.STIMENA12 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0034 |
||
|
Physical address |
0xE000 0034 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 13 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM13 |
A write to this location causes data to be written into the FIFO if TER.STIMENA13 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0038 |
||
|
Physical address |
0xE000 0038 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 14 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM14 |
A write to this location causes data to be written into the FIFO if TER.STIMENA14 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 003C |
||
|
Physical address |
0xE000 003C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 15 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM15 |
A write to this location causes data to be written into the FIFO if TER.STIMENA15 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0040 |
||
|
Physical address |
0xE000 0040 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 16 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM16 |
A write to this location causes data to be written into the FIFO if TER.STIMENA16 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0044 |
||
|
Physical address |
0xE000 0044 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 17 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM17 |
A write to this location causes data to be written into the FIFO if TER.STIMENA17 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0048 |
||
|
Physical address |
0xE000 0048 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 18 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM18 |
A write to this location causes data to be written into the FIFO if TER.STIMENA18 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 004C |
||
|
Physical address |
0xE000 004C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 19 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM19 |
A write to this location causes data to be written into the FIFO if TER.STIMENA19 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0050 |
||
|
Physical address |
0xE000 0050 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 20 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM20 |
A write to this location causes data to be written into the FIFO if TER.STIMENA20 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0054 |
||
|
Physical address |
0xE000 0054 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 21 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM21 |
A write to this location causes data to be written into the FIFO if TER.STIMENA21 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0058 |
||
|
Physical address |
0xE000 0058 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 22 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM22 |
A write to this location causes data to be written into the FIFO if TER.STIMENA22 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 005C |
||
|
Physical address |
0xE000 005C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 23 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM23 |
A write to this location causes data to be written into the FIFO if TER.STIMENA23 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0060 |
||
|
Physical address |
0xE000 0060 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 24 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM24 |
A write to this location causes data to be written into the FIFO if TER.STIMENA24 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0064 |
||
|
Physical address |
0xE000 0064 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 25 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM25 |
A write to this location causes data to be written into the FIFO if TER.STIMENA25 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0068 |
||
|
Physical address |
0xE000 0068 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 26 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM26 |
A write to this location causes data to be written into the FIFO if TER.STIMENA26 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 006C |
||
|
Physical address |
0xE000 006C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 27 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM27 |
A write to this location causes data to be written into the FIFO if TER.STIMENA27 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0070 |
||
|
Physical address |
0xE000 0070 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 28 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM28 |
A write to this location causes data to be written into the FIFO if TER.STIMENA28 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0074 |
||
|
Physical address |
0xE000 0074 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 29 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM29 |
A write to this location causes data to be written into the FIFO if TER.STIMENA29 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0078 |
||
|
Physical address |
0xE000 0078 |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 30 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM30 |
A write to this location causes data to be written into the FIFO if TER.STIMENA30 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 007C |
||
|
Physical address |
0xE000 007C |
Instance |
CPU_ITM |
|
Description |
ITM Stimulus Port 31 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
STIM31 |
A write to this location causes data to be written into the FIFO if TER.STIMENA31 is set. Reading from the stimulus port returns the FIFO status in bit [0]: 0 = full, 1 = not full. The polled FIFO interface does not provide an atomic read-modify-write, so it's users responsibility to ensure exclusive read-modify-write if this ITM port is used concurrently by interrupts or other threads. |
RW |
0x0000 0000 |
||
|
Address offset |
0x0000 0E00 |
||
|
Physical address |
0xE000 0E00 |
Instance |
CPU_ITM |
|
Description |
ITM Trace Enable Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31 |
STIMENA31 |
Bit mask to enable tracing on ITM stimulus port 31. |
RW |
0 |
||
|
30 |
STIMENA30 |
Bit mask to enable tracing on ITM stimulus port 30. |
RW |
0 |
||
|
29 |
STIMENA29 |
Bit mask to enable tracing on ITM stimulus port 29. |
RW |
0 |
||
|
28 |
STIMENA28 |
Bit mask to enable tracing on ITM stimulus port 28. |
RW |
0 |
||
|
27 |
STIMENA27 |
Bit mask to enable tracing on ITM stimulus port 27. |
RW |
0 |
||
|
26 |
STIMENA26 |
Bit mask to enable tracing on ITM stimulus port 26. |
RW |
0 |
||
|
25 |
STIMENA25 |
Bit mask to enable tracing on ITM stimulus port 25. |
RW |
0 |
||
|
24 |
STIMENA24 |
Bit mask to enable tracing on ITM stimulus port 24. |
RW |
0 |
||
|
23 |
STIMENA23 |
Bit mask to enable tracing on ITM stimulus port 23. |
RW |
0 |
||
|
22 |
STIMENA22 |
Bit mask to enable tracing on ITM stimulus port 22. |
RW |
0 |
||
|
21 |
STIMENA21 |
Bit mask to enable tracing on ITM stimulus port 21. |
RW |
0 |
||
|
20 |
STIMENA20 |
Bit mask to enable tracing on ITM stimulus port 20. |
RW |
0 |
||
|
19 |
STIMENA19 |
Bit mask to enable tracing on ITM stimulus port 19. |
RW |
0 |
||
|
18 |
STIMENA18 |
Bit mask to enable tracing on ITM stimulus port 18. |
RW |
0 |
||
|
17 |
STIMENA17 |
Bit mask to enable tracing on ITM stimulus port 17. |
RW |
0 |
||
|
16 |
STIMENA16 |
Bit mask to enable tracing on ITM stimulus port 16. |
RW |
0 |
||
|
15 |
STIMENA15 |
Bit mask to enable tracing on ITM stimulus port 15. |
RW |
0 |
||
|
14 |
STIMENA14 |
Bit mask to enable tracing on ITM stimulus port 14. |
RW |
0 |
||
|
13 |
STIMENA13 |
Bit mask to enable tracing on ITM stimulus port 13. |
RW |
0 |
||
|
12 |
STIMENA12 |
Bit mask to enable tracing on ITM stimulus port 12. |
RW |
0 |
||
|
11 |
STIMENA11 |
Bit mask to enable tracing on ITM stimulus port 11. |
RW |
0 |
||
|
10 |
STIMENA10 |
Bit mask to enable tracing on ITM stimulus port 10. |
RW |
0 |
||
|
9 |
STIMENA9 |
Bit mask to enable tracing on ITM stimulus port 9. |
RW |
0 |
||
|
8 |
STIMENA8 |
Bit mask to enable tracing on ITM stimulus port 8. |
RW |
0 |
||
|
7 |
STIMENA7 |
Bit mask to enable tracing on ITM stimulus port 7. |
RW |
0 |
||
|
6 |
STIMENA6 |
Bit mask to enable tracing on ITM stimulus port 6. |
RW |
0 |
||
|
5 |
STIMENA5 |
Bit mask to enable tracing on ITM stimulus port 5. |
RW |
0 |
||
|
4 |
STIMENA4 |
Bit mask to enable tracing on ITM stimulus port 4. |
RW |
0 |
||
|
3 |
STIMENA3 |
Bit mask to enable tracing on ITM stimulus port 3. |
RW |
0 |
||
|
2 |
STIMENA2 |
Bit mask to enable tracing on ITM stimulus port 2. |
RW |
0 |
||
|
1 |
STIMENA1 |
Bit mask to enable tracing on ITM stimulus port 1. |
RW |
0 |
||
|
0 |
STIMENA0 |
Bit mask to enable tracing on ITM stimulus port 0. |
RW |
0 |
||
|
Address offset |
0x0000 0E40 |
||
|
Physical address |
0xE000 0E40 |
Instance |
CPU_ITM |
|
Description |
ITM Trace Privilege Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:4 |
RESERVED4 |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
RW |
0x000 0000 |
||
|
3:0 |
PRIVMASK |
Bit mask to enable unprivileged (User) access to ITM stimulus ports: |
RW |
0x0 |
||
|
Address offset |
0x0000 0E80 |
||
|
Physical address |
0xE000 0E80 |
Instance |
CPU_ITM |
|
Description |
ITM Trace Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|||||||||||||||||||||
|
31:24 |
RESERVED24 |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
RW |
0x00 |
|||||||||||||||||||||
|
23 |
BUSY |
Set when ITM events present and being drained. |
RW |
0 |
|||||||||||||||||||||
|
22:16 |
ATBID |
Trace Bus ID for CoreSight system. Optional identifier for multi-source trace stream formatting. If multi-source trace is in use, this field must be written with a non-zero value. |
RW |
0x00 |
|||||||||||||||||||||
|
15:10 |
RESERVED10 |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
RW |
0x00 |
|||||||||||||||||||||
|
9:8 |
TSPRESCALE |
Timestamp prescaler
|
RW |
0x0 |
|||||||||||||||||||||
|
7:5 |
RESERVED5 |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
RW |
0x0 |
|||||||||||||||||||||
|
4 |
SWOENA |
Enables asynchronous clocking of the timestamp counter (when TSENA = 1). If TSENA = 0, writing this bit to 1 does not enable asynchronous clocking of the timestamp counter. |
RW |
0 |
|||||||||||||||||||||
|
3 |
DWTENA |
Enables the DWT stimulus (hardware event packet emission to the TPIU from the DWT) |
RW |
0 |
|||||||||||||||||||||
|
2 |
SYNCENA |
Enables synchronization packet transmission for a synchronous TPIU. |
RW |
0 |
|||||||||||||||||||||
|
1 |
TSENA |
Enables differential timestamps. Differential timestamps are emitted when a packet is written to the FIFO with a non-zero timestamp counter, and when the timestamp counter overflows. Timestamps are emitted during idle times after a fixed number of two million cycles. This provides a time reference for packets and inter-packet gaps. If SWOENA (bit [4]) is set, timestamps are triggered by activity on the internal trace bus only. In this case there is no regular timestamp output when the ITM is idle. |
RW |
0 |
|||||||||||||||||||||
|
0 |
ITMENA |
Enables ITM. This is the master enable, and must be set before ITM Stimulus and Trace Enable registers can be written. |
RW |
0 |
|||||||||||||||||||||
|
Address offset |
0x0000 0FB0 |
||
|
Physical address |
0xE000 0FB0 |
Instance |
CPU_ITM |
|
Description |
ITM Lock Access Register |
||
|
Type |
WO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
LOCK_ACCESS |
A privileged write of 0xC5ACCE55 enables more write access to Control Registers TER, TPR and TCR. An invalid write removes write access. |
WO |
0x0000 0000 |
||
|
Address offset |
0x0000 0FB4 |
||
|
Physical address |
0xE000 0FB4 |
Instance |
CPU_ITM |
|
Description |
ITM Lock Status Register |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:3 |
RESERVED3 |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
RO |
0x0000 0000 |
||
|
2 |
BYTEACC |
Reads 0 which means 8-bit lock access is not be implemented. |
RO |
0 |
||
|
1 |
ACCESS |
Write access to component is blocked. All writes are ignored, reads are permitted. |
RO |
1 |
||
|
0 |
PRESENT |
Indicates that a lock mechanism exists for this component. |
RO |
1 |
||
| © 2015. Texas Instruments | All Rights Reserved |