Instance: EFUSE
Component: EFUSE
Base address: 0x10000000
Efuse area
|
Register Name |
Type |
Register Width (Bits) |
IR |
|
RW |
32 |
3 |
|
|
RW |
32 |
4 |
|
|
RW |
32 |
5 |
|
|
RW |
32 |
6 |
|
|
RW |
32 |
7 |
|
|
RW |
32 |
8 |
|
|
RW |
32 |
9 |
|
|
RW |
32 |
10 |
|
|
RW |
32 |
11 |
|
|
RW |
32 |
12 |
|
IR |
3 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ID_31_0 |
Bit[31:0] of the 128-bit die ID |
RW |
0xXXXX XXXX |
||
|
IR |
4 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ID_63_32 |
Bit[63:32] of the 128-bit die ID |
RW |
0xXXXX XXXX |
||
|
IR |
5 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ID_95_64 |
Bit[95:64] of the 128-bit die ID |
RW |
0xXXXX XXXX |
||
|
IR |
6 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ID_127_96 |
Bit[127:96] of the 128-bit die ID |
RW |
0xXXXX XXXX |
||
|
IR |
7 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4). |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
ULL_MCU_RAM1_REP |
Bits[2:0] of MCU RAM1 repair |
RW |
0x0 |
||
|
28:19 |
ULL_MCU_RAM2_REP |
Bits[9:0] of MCU RAM2 repair |
RW |
0x000 |
||
|
18:9 |
ULL_MCU_RAM3_REP |
Bits[9:0] of MCU RAM3 repair |
RW |
0x000 |
||
|
8:1 |
ULL_AUX_RAM_REP |
Bits[7:0] of AUX RAM repair |
RW |
0x00 |
||
|
0 |
TAP_DAP_LOCK |
If TAP_DAP_LOCK == SCAN_DATA2_BOOT.TAP_DAP_LOCK_N: Device locked |
RW |
0 |
||
|
IR |
8 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4). |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:17 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RW std text) |
RW |
0x0000 |
||
|
16:7 |
ULL_MCU_RAM0_REP |
Bits[9:0] of MCU RAM0 repair |
RW |
0x000 |
||
|
6:0 |
ULL_MCU_RAM1_REP |
Bits[9:3] of MCU RAM1 repair |
RW |
0x00 |
||
|
IR |
9 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4). |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31 |
FLASH_RDY |
0: FW halts CPU during boot with all DAP/TAPs unlocked after having configured flash module for read capability. |
RW |
1 |
||
|
30 |
STANDBY_MODE_SEL_INT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 0, this value will be written to FLASH:CFG.STANDBY_MODE_SEL by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0 |
||
|
29:28 |
STANDBY_PW_SEL_INT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 0, this value will be written to FLASH:CFG.STANDBY_PW_SEL by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0x0 |
||
|
27 |
DIS_STANDBY_INT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 0, this value will be written to FLASH:CFG.DIS_STANDBY by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0 |
||
|
26:24 |
VIN_AT_X_INT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 0, this value will be written to [FLASH.FSEQPMP.VIN_AT_X] by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0x0 |
||
|
23 |
STANDBY_MODE_SEL_EXT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 1, this value will be written to FLASH:CFG.STANDBY_MODE_SEL by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0 |
||
|
22:21 |
STANDBY_PW_SEL_EXT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 1, this value will be written to FLASH:CFG.STANDBY_PW_SEL by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0x0 |
||
|
20 |
DIS_STANDBY_EXT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 1, this value will be written to FLASH:CFG.DIS_STANDBY by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0 |
||
|
19:17 |
VIN_AT_X_EXT |
If AON_SYSCTL:PWRCTL.EXT_REG_MODE = 1, this value will be written to FLASH:FSEQPMP.VIN_AT_X by FW during boot. This register bit field will be updated by FW with trim value from FCFG1 later in the boot sequence. |
RW |
0x0 |
||
|
16:9 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RW std text) |
RW |
0x00 |
||
|
8:1 |
CRC |
Checksum of SCAN_DATA0 row bits[31:0] and SCAN_DATA1 row bit[31:0] and SCAN_DATA2_TRIM row bit[0]. This field is included in the scan chain. |
RW |
0xXX |
||
|
0 |
TAP_DAP_LOCK_N |
If TAP_DAP_LOCK == SCAN_DATA2_BOOT.TAP_DAP_LOCK_N: [CPU_MMAP::AON_WUC.LOCKCFG.SECURITY_STATE] = 0, ie device is locked. |
RW |
0 |
||
|
IR |
10 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4). |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:30 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RW std text) |
RW |
0x0 |
||
|
29 |
ROM_BOOT |
0: FW will halt CPU immediatly after release of reset and the reading of this bit. |
RW |
1 |
||
|
28:25 |
TRIM3P4 |
Value will be written to FLASH:FSEQPMP.TRIM_3P4 by FW during boot. |
RW |
0x5 |
||
|
24:21 |
VCG2P5CT |
Value will be written to FLASH:FVNVCT.VCG2P5CT by FW during boot. |
RW |
0xX |
||
|
20:17 |
VREADCT |
Value will be written to FLASH:FVREADCT.VREADCT by FW during boot. |
RW |
0xX |
||
|
16:13 |
TRIM_0P8 |
Value will be written to FLASH:FSEQPMP.TRIM_0P8by FW during boot. |
RW |
0x8 |
||
|
12:10 |
TRIM_SADLY |
This value will be written to bit[12:10] of FLASH:BANK_0_EFUSE by FW during boot. |
RW |
0x1 |
||
|
9:5 |
TRIM_NMOS |
This value will be written to bit[9:5] of FLASH:BANK_0_EFUSE by FW during boot. |
RW |
0xXX |
||
|
4:0 |
TRIM_PMOS |
This value will be written to bit[4:0] of FLASH:BANK_0_EFUSE by FW during boot. |
RW |
0xXX |
||
|
IR |
11 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RW std text) |
RW |
0x0 |
||
|
28:27 |
SET_RCOSC_HF_COARSE_RESISTOR |
Value will be written to DDI_0_OSC:ATESTCTL.SET_RCOSC_HF_FINE_RESISTOR by FW during boot. |
RW |
0xX |
||
|
26:23 |
TRIMMAG |
Value will be written to ADI_3_REFSYS:REFSYSCTL2.TRIM_VREF by FW during boot. |
RW |
0xX |
||
|
22:18 |
TRIMIREF |
Value will be written to ADI_2_REFSYS:REFSYSCTL0.TRIM_IREF by FW during boot. |
RW |
0xXX |
||
|
17:16 |
ITRIM_DIG_LDO |
Value is read by FW and is used in the calculation to find the value that is written to ADI_2_REFSYS:SOCLDOCTL3.ITRIM_DIGLDO during boot. |
RW |
0x0 |
||
|
15:12 |
VTRIM_DIG |
Value will be written to ADI_2_REFSYS:SOCLDOCTL1.VTRIM_DIG by FW during boot. |
RW |
0xX |
||
|
11:8 |
VTRIM_COARSE |
Value will be written to ADI_2_REFSYS:SOCLDOCTL1.VTRIM_COARSE by FW during boot. |
RW |
0xX |
||
|
7:0 |
RCOSCHF_CTRIM |
The boot FW will use this value as a trim target for the RCOSCHF cap trim. FW calculates the delta between current register bit field value of DDI_0_OSC:RCOSCHFCTL.RCOSCHF_CTRIM and this field. 1/16 of this delta value is added to DDI_0_OSC:RCOSCHFCTL.RCOSCHF_CTRIM in each loop of a total of 16. The 2 MSB bits of the value read and written from/to DDI_0_OSC:RCOSCHFCTL.RCOSCHF_CTRIM register bit field will be inverted by FW. |
RW |
0xXX |
||
|
IR |
12 |
||
|
Description |
Note: Efuse row number = (Address Offset / 4) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:27 |
Reserved |
Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior.(RW std text) |
RW |
0x00 |
||
|
26:25 |
BOD_BANDGAP_TRIM_CNF |
Configuration of ROM boot FW trim algorithm for Bandgap and VDDS BOD. |
RW |
0x1 |
||
|
24 |
VDDR_ENABLE_PG1 |
This value will be written to ADI_3_REFSYS:DCDCCTL2.TURNON_EA_SW by FW during boot. |
RW |
0 |
||
|
23 |
VDDR_OK_HYS |
Value will be written to ADI_3_REFSYS:DCDCCTL1.VDDR_OK_HYST by FW during boot. |
RW |
0 |
||
|
22:21 |
IPTAT_TRIM |
Value will be written to ADI_3_REFSYS:DCDCCTL1.IPTAT_TRIM by FW during boot. |
RW |
0x0 |
||
|
20:16 |
VDDR_TRIM |
Value will be written to ADI_3_REFSYS:DCDCCTL0.VDDR_TRIM by FW during boot. |
RW |
0xXX |
||
|
15:11 |
TRIMBOD_INTMODE |
Value will be written to ADI_3_REFSYS:REFSYSCTL1.TRIM_VDDS_BOD by FW during boot if AON_SYSCTL:PWRCTL.EXT_REG_MODE = 0. |
RW |
0xXX |
||
|
10:6 |
TRIMBOD_EXTMODE |
Value will be written to ADI_3_REFSYS:REFSYSCTL1.TRIM_VDDS_BOD by FW during boot if AON_SYSCTL:PWRCTL.EXT_REG_MODE = 1. |
RW |
0xXX |
||
|
5:0 |
TRIMTEMP |
Value will be written to ADI_3_REFSYS:REFSYSCTL3.TRIM_VBG by FW during boot. |
RW |
0xXX |
||
| © 2015. Texas Instruments | All Rights Reserved |