Code Composer Studio IDE
Code Composer Studio™ (CCStudio) is an integrated development environment (IDE) for Texas Instruments’ (TI) embedded processor families. CCStudio comprises a suite of tools used to develop and debug embedded applications. It includes compilers for each of TI's device families, source code editor, project build environment, debugger, profiler, simulators, real-time operating system and many other features. The intuitive IDE provides a single user interface taking you through each step of the application development flow. Familiar tools and interfaces allow users to get started faster than ever before and add functionality to their application thanks to sophisticated productivity tools.
Code Red Technologies
The Code Red Tools Suite is a complete software development platform for 32-bit microcontroller devices available to Stellaris® Cortex-M based microcontrollers. Code Red integrates Code Trace™ Real Time Trace capability delivering features never before available to microcontroller developers. Code Trace capitalizes on the serial wire viewing (SWV) technology in Stellaris microcontrollers to deliver unprecedented visibility during debug. Code Trace delivers high accuracy profiling, interrupt statistics, interrupt tracing, RTOS event tracing and a useful and unique no overhead host-strings viewing mechanism, which provides printf style debugging and logging without any of the intrusiveness typical to other embedded debug methods. Interrupt tracing provides impressive graphical visualization of what is really going on in a real time system.
CodeSourcery, Inc.
CodeSourcery builds software tools that enable its customers to get the most out of hardware platforms ranging from embedded devices to supercomputers. Sourcery G++, a complete software development environment based on the GNU Toolchain, is the leading choice of software engineers, operating system vendors, semiconductor companies, and device manufacturers. CodeSourcery's products and services deliver on the promise of open-source software and open standards.
IAR Embedded Workbench
IAR Embedded Workbench is a set of development tools for building and debugging embedded applications using assembler, C and C++. It provides a completely integrated development environment including a project manager, editor, build tools and debugger. IAR Embedded Workbench supports MSP430 and TI ARM based microcontrollers. It provides hardware debug systems and RTOSs, and generates very compact and efficient code. IAR Systems is the world's leading provider of software tools for embedded systems that enable large and small companies to develop premium products based on 8-, 16-, and 32-bit microcontrollers.
Keil
Keil microcontroller development tools for Cortex™-M devices support every level of developer from the professional applications engineer to the student just learning about embedded software development. The industry-standard tools from ARM (RealView® Compilation Tools including C/C++ Compiler, Macro Assembler, and Linker) and Keil (Debuggers, Real-time Kernels, Single-board Computers, and Emulators) support over 700 of the most popular ARM microcontrollers and help you get your projects completed on schedule.
Lauterbach GmbH
TRACE32 is a set of modular microprocessor development tools. The modular hardware and software supports up to 350 different CPUs. Lauterbach provides low cost tools as well as sophisticated high end In-Circuit Emulators. Lauterbach GmbH is the world largest producer of hardware assisted debug tools. Our engineering team has more than 30 years experience in making world class debuggers and emulators. Lauterbach is an internationally well-established company with blue chip customers from every corner of the globe. The company has it′s own branch offices in the United Kingdom, Italy, France, Japan, China and on both the east and west coasts of the United States supporting Lauterbach products.
MSPGCC
Includes the GNU C compiler (GCC), the assembler and linker (binutils), the debugger (GDB), and some other tools needed to make a complete development environment for the MSP430. These tools can be used on Windows, Linux, BSD and most other flavors of Unix.
Rowley CrossWorks
CrossWorks is our exceptional integrated development environment for microcontrollers. It includes a first-class editor, an intuitive project manager, integrated FLASH programming, and a feature-packed debugger. Rowley supports TI’s MSP430 microcontrollers.