Microcontrollers (MCU)

Design Support

Getting Started

Selection Tool

Training & Events

Developer Network

University

 531 views

This application report describes how to build an isolated FET interface for the MSP430 Flash Emulation Tool (FET). When developing and debugging line-powered MSP430 applications such as motor control, electricity energy meters, power monitoring systems etc. it is important to have electrical isolation for the development tool such that the personnel involved and the connected electronic equipment, like the host PC, is protected. The simple interface solution presented in this report uses two dual ISO150 isolated bidirectional digital couplers to achieve the required isolation. This solution not only provides electrical isolation for protection but also eliminates ground loops, which is a requirement while debugging high-performance analog applications. This document includes the schematics, layout, and bill of materials for building this interface. The Gerber files for the PCB are provided in the zip file associated with this application report.

Associated Files: