Microcontrollers (MCU)

Design Support

Getting Started

Selection Tool

Training & Events

Developer Network

University

 26 views

The template dialog box in the IAR tool quickly creates a project with a default configuration for RAM and flash modes. Creating a new project includes a main program shell, low-level init file for the specified device, and appropriate linker files, sets up the custom build for the High-End Timer (HET), and sets all project parameters for immediate compiling and loading of code. These files are TMS470 specific and are an addition to the default files provided by IAR.

Associated Files: