Microcontrollers (MCU)

Design Support

Getting Started

Selection Tool

Training & Events

Developer Network

University

 

For this lab we are using the Three Phase BLDC Motor Kit with DRV8312 and Piccolo MCU (DRV8312-C2-KIT) (the DRV8302-HC-C2-KIT or DRV8301-HC-C2-KIT can also be used) with a Piccolo F28035 controlCARD subsystem to run the sensorless InstaSPIN BLDC technique.

These are the tasks that must be done to spin motors:

  1. Make sure all physical connections and jumper settings on the kit are correct
  2. Flash the InstaSPIN BLDC object file (.out) onto the controlCARD
  3. Launch the GUI
  4. Start spinning motors