|
7,121 views
For this lab we are using the Three Phase BLDC Motor Kit with DRV8312 and Piccolo MCU (DRV8312-C2-KIT) (the DRV8302-HC-C2-KIT or DRV8301-HC-C2-KIT can also be used) with a Piccolo F28035 controlCARD subsystem to run the sensorless InstaSPIN BLDC technique.
These are the tasks that must be done to spin motors:
- Make sure all physical connections and jumper settings on the kit are correct
- Flash the InstaSPIN BLDC object file (.out) onto the controlCARD
- Launch the GUI
- Start spinning motors
|