New Stellaris® ARM® Cortex™-M4F MCUs
Continuing to empower developers with leading ARM®-based embedded processing solutions, TI now has a new low power, floating-point Stellaris® Cortex™-M4F microcontroller generation. All of the new LM4Fx Stellaris microcontrollers provide floating point for performance headroom and best-in-class power consumption to address portability and power budgets. Developers can also select from a variety of high-performance analog, memory and connectivity options to best satisfy design parameters across a broad range of applications, such as industrial automation, motion control, health and fitness and more. The new Stellaris MCUs are the first Cortex-M-based microcontrollers to be built on 65 nanometer technology, paving the roadmap to higher speeds, larger memory and even lower power. Get started with the LM4F232 Evaluation Kit.

New 220MHz Hercules™ RM48L952 now sampling
The highest performance 220MHz RM48L952 Hercules ARM® Safety MCU devices for medical and industrial safety-critical applications are now sampling. The RM4x series of MCUs are designed for high-performance safety-critical applications and have been developed with the capability to meet the requirements of the IEC 61508 SIL-3 safety standard.

5V tolerant MSP430™ MCU? No problem!
Ideal for capacitive touch, motor control, LED lighting and power management applications, the new MSP430F51x2 series extends TI’s ultra-low power portfolio with a feature rich device, as it provides 2 high precision timers designed for fine measurement or 5V driving applications. Each 16-bit precision timer integrates three capture and compare registers and support of high resolution mode running up to 256MHz, equivalent to 4ns resolution.
In addition, learn more about Timer D in this application report and see the Capacitive Touch Sense Library.

New! Sub-1 GHz RF performance line
TI’s new CC1120 sub-1 GHz RF performance line delivers more than 30 times better range in crowded wireless environments as compared to competitive offerings. It provides unmatched connectivity for low-power wireless applications in the security, Smart Grid, industrial, wireless healthcare, home and building automation, and other spaces. The sub-1 GHz RF performance line family meets the market’s most stringent RF requirements and provides an industry-leading ability to filter out other RF sources.

New low cost sub-1 GHz value line device family
The sub-1GHz value line family offers developers low-cost connectivity solutions for sub-1 GHz RF applications such as remote controls, toys, home and building automation, and security systems. The CC110L transceiver, CC113L receiver and CC115L transmitter devices are all based on TI’s sub-1GHz CC1101 RF technology, and are pin-, register- and code-compatible, as well as backwards compatible with existing sub-1 GHz systems. In high volume, the value line offers a two-chip, one-way RF link for less than USD $1.00.
Order your value line development kit at www.ti.com/rfvalueline
|
|
|
New Literature, app notes and guides |
See the updated Stellaris® MCU Brochure
The new Stellaris MCU brochure provides a detailed overview of the industry’s leading family of robust, real-time MCUs based on the revolutionary ARM® Cortex™-M series MCU technology.

Contactless NFC Bootstrap Loader Using MSP430F5529 and TRF7970A
Near Field Communication, or NFC, is a technology which allows contactless communication between devices providing end users with an easier and more convenient way to make transactions. The integration of NFC in next-generation cell phones, laptops, and tablets will provide end users and developers with a complete new range of possibilities to explore. One of the areas of interest during development of such applications is the capability to upgrade firmware in the field, and the purpose of this application report is to explain the implementation of a bootstrap loader (BSL) based on the MSP430F5xx/F6xx devices.

Hercules™ MCU Compatibility Considerations
This application report provides a summary of the main changes required for porting an application written on the Hercules TMS570LS20x/10x series of microcontrollers over to the Hercules TMS570LS31x/21x series of microcontrollers. A brief description of the process technology differences is also included.

Hercules™ MCU Functional Safety Manual
This document is a safety manual for the Hercules safety critical microcontroller product family. The product family utilizes a common safety architecture which is implemented in multiple application focused products.

RM48 Hercules™ ARM® Safety MCU Development Kit User’s Guide
This document describes the board level operations of the RM48 Hercules Development Kit (HDK). The HDK is based on the Texas Instruments RM48 microcontroller.

TMS570LS31 Hercules™ ARM® Safety MCU Development Kit User’s Guide
This document describes the board level operations of the TMS570LS31 Hercules Development Kit (HDK). The HDK is based on the Texas Instruments TMS570LS3137 337 BGA microcontroller.

Performance Measurement App Note
This application report describes methods for measuring code execution time of the TMS470 and TMS570 microcontrollers.
The Concerto family is a multi-core system-on-chip microcontroller (MCU) with independent communication and real-time control subsystems. This datasheet features the F28M35x, the first series in the Concerto family.

C2000™ Concerto™ MCU Datasheet
The Concerto family is a multi-core system-on-chip microcontroller (MCU) with independent communication and real-time control subsystems. This datasheet features the F28M35x, the first series in the Concerto family.
|
|

|
|
|
Tool and Software Updates |
New MSP430 LaunchPad BoosterPacks!
TPL0501EVM is a new BoosterPack based on TI’s TPL0501, a single channel, linear-taper digital potentiometer with 256 wiper positions. This device can be used as a three-terminal potentiometer or as a two-terminal rheostat. The internal registers of the TPL0501 can be accessed using a SPI-compatible interface. Comes with a preprogrammed MSP430™ MCU device with demo code, as well as a PC-based open source GUI. Available now for $20!
TPL0401EVM is a new BoosterPack based on TI’s TPL0401, an I²C bus controlled, single channel, linear-taper digital potentiometer with 128 wiper positions. The position of the wiper can be adjusted using an I²C interface. The part has a 10k end-to-end resistance and can operate with a supply voltage range of 2.7V to 5.5V. Comes with a preprogrammed MSP430™ MCU device with demo code, as well as a PC-based open source GUI. Available now for $25!

CC430-based Sub-GHz Spectrum Analyzer now available!
The MSP-SA430-SUB1GHZ Spectrum Analyzer is a CC430-based reference design that can be used to implement an easy and affordable tool to jumpstart RF development in the sub GHz frequency range. More and more electronic devices include a built-in RF link. RF transceivers are inexpensive, but the equipment to design and debug such systems is not. The CC430-based spectrum analyzer provides an affordable development tool that reduces the time needed on expensive measurement equipment. The system is recognized as a USB device and is operated from a powerful yet simple graphical user interface that is available for free to download.

New MSP430™ MCU Production Programmer – MSP-GANG
The MSP Gang Programmer is an MSP430 device programmer that can program up to eight identical MSP430 flash or FRAM devices at the same time. The MSP Gang Programmer connects to a host PC using a standard RS-232 or USB connection and provides flexible programming options that allow the user to fully customize the process.
|
|
New Smart Grid Group on TI’s e2e Community
Across the smart grid application spectrum, TI supports every stage of the design process, from device selection and software development to tools and system solutions. Find smarter grid solutions on TI’s e2e Community – and find articles, videos and other contributions authored by TI’s Smart Grid experts. Here you will find methods for getting your design to market faster, compliance with worldwide standards, and developing smart energy systems, using the world’s most current technology.
%%DYN_BLOCK%%
|
|
| Upcoming events and training |
MCU Workshops
Check out the list of upcoming MCU workshops and get hands-on, in-person training on your favorite device!

Interested in Motor Control?
Learn more about TI’s newest motor control technology for low-cost BLDC applications. InstaSPIN-BLDC is a sensorless control technique based on the premise that “simple is better”.

Sharpen your MSP430™ MCU skills with online training
Whether you’re interested in the MSP430 Value Line or the Chronos Watch ecosystem, you can learn everything you need to know about the MSP430 in MCU in our online training repository! These trainings allow the user to decide between online videos, virtual presentations, on-site education or can get you to the MSP experts in the E2E forum.

Missed C2000 Office Hours?
Don’t worry – you can view all the archived Q&A.
%%DYN_BLOCK%%
|
|
|