Texas Instruments
Productivity Solutions Home PageTI Map/SearchFeedbackTI Home
Avigo HomeProduct InformationAvigo On The WebInternational InformationGetting the Most from AvigoAvigo Support

 

 

Avigo Manager Update

Avigo Manager Version 1.1, Build 2.2 is now available. This build contains the following improvements:

World Time

  • Avigo Manager can now delete and edit cities correctly.
  • The World Time City column no longer disappears when you click Greenwich Mean Time.
Importing and Exporting Data
  • You can now use upper- and lower-case special characters when transferring data between Avigo and the PC.
  • When updating a data table between Avigo and the PC, Avigo Manager no longer appends the changed fields as if they were new fields, but rather updates the data within.
Backing Up and Restoring Data
  • When backing up an Avigo that has private entries, if you do not type in your password, Avigo Manager displays an error message. When you click OK on the message box, the box closes correctly without locking up the system.
  • While restoring data to Avigo, Avigo Manager no longer produces errors if you choose Restore again from the File menu. Instead, the restore operation completes correctly.
Sketches
  • Sketch names can be up to 16 characters. Previously, Avigo Manager let you use more than 16 characters in a sketch name, but Avigo did not. Now Avigo Manager uses only the first 16 characters of a sketch name.
  • Avigo Manager now sets the default file extension to .bmp for sketches.
  • When you click X to cancel an operation in the sketch function, the operation cancels successfully.
Data Tables
  • When you cancel an operation to a data table, the operation cancels successfully.
Miscellaneous
  • The Avigo Manager buttons now highlight correctly.
  • When changing the infrared port number, Avigo Manager correctly opens the Port Settings dialog when you choose it from the File menu. Previously the dialog would not open if a connection failure occurred just prior to opening the dialog.
  • When performing time-consuming operations, Avigo Manager displays an hour-glass cursor.
  • Right-clicking a file name in the Open dialog box no longer causes garbage to appear.
  • Lets you select different languages during installation.
  • Lets you use read-only categories with group calendaring.
  • Resolved problem changing to a new function prior to completion of the current function.
  • Proper startup directory is now selected on file functions.

To find out what version you are currently running, start the software, and select "About Avigo Manager" from the "Help" menu. The latest version is Avigo Manager V 1.1 (Build 2.2), and can be downloaded below.

 
Avigo Manager V 1.1 (Build 2.2)

FTP - Avigo Manager V 1.1 (Build 2.2) (5.9 MB)
HTTP - Avigo Manager V 1.1 (Build 2.2) (5.9 MB)

 

   

     Contacting TI

     Avigo Manuals

     Avigo FAQ Index

Expanded OutlineSoftware Updates
  Internal Software
Avigo Manager
IntelliSync for Avigo

Collapsed OutlineAvigo Developers Corner

Productivity Solutions Home PageTI Map/SearchFeedbackTI Home
(c) Copyright 1998 Texas Instruments Incorporated. All rights reserved.
Trademarks