| Q1. |
Are there any limits to how large an Avigo entry can be? |
| Q2. |
What PIM's can I use to synchronize with Avigo? |
| Q3. |
I am receiving errors when trying to import/export Excel or Lotus 1-2-3 spreadsheet data between Avigo. How can I correct this? |
| Q4. |
Are there any special steps I should follow if my PIM data is currently in the Lotus Organizer 2.x format and I need to synchronize using Intellisync's Lotus Organizer 97 translator that is bundled with Avigo? |
| Q5. |
How do I fix : When I use Avigo Manager's Import Expense function a file is created but it does not contain my expense data? |
| Q6. |
Can I write my own software for Avigo? Is an API listing or SDK available? |
| Q7. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Sync could not be completed: Application section does not exist" occurs? |
| Q8. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Unable to Complete Translation" occurs? |
| Q9. |
How can I utilize Avigo's infrared port? |
| Q10. |
What is T9? |
| Q11. |
What processor / operating system (OS) does Avigo use? |
| Q12. |
Why does Avigo emit a buzzing sound when I turn on the backlight? |
| Q13. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Synchronization could not be completed: Unable to Complete Request" (Internal Error #4094) occurs? |
| Q14. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Synchronization could not be completed: Unable to load source application API. Verify application is installed." occurs? |
| Q15. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Synchronization could not be completed: Error encountered while updating record status." (Internal Error #504) occurred? |
| Q16. |
How to fix: When I attempt to synchronize using Intellisync, Avigo, and my Lotus Organizer 97 database, the error "Synchronization could not be completed: Unable to establish connection to the handheld device." (Internal Error #500 or Internal Error #507) occurs? |
| Q17. |
How do I troubleshoot the serial communications process? |
| Q18. |
Serial Port communications and your modem. |
| Q19. |
Checking for a defective Serial Port. |
| Q20. |
Advanced serial communications troubleshooting tips. |
| Q21. |
Why does Avigo prompt me for a password when I turn it on? |
| Q22. |
How can I prevent Avigo from automatically sorting my Data Tables? |
| Q23. |
Avigo doesn't seem to be returning the correct numbers for Week: and Weeks Remaining: in the Calendar application. |
| Q24. |
Where can I find the Financial Calculator for Avigo? |
| Q25. |
How to fix: When I select the Applications section in the Avigo Manager software, the error "Invalid Argument to date encode" occurs? |
| Q26. |
How to fix: The time for some cities in my World Time clock are not correct. |