How to fix: When I select the Applications section in the Avigo Manager software, the error "Invalid Argument to date encode" occurs?
This error will occur in the Avigo Manager software when it encounters an application on Avigo whose date information has been entered incorrectly. In order to correct this problem, you will need to perform a full reset of Avigo. This will be the only way to remove the conflicting application. Before resetting, however, you should synchronize your current information to the PC, save all Avigo data tables to the PC, and verify that all applications are still available on the PC. After the reset, you can send all of this information back to the handheld. A handful of users may receive this error, even though there are currently no applications stored to Avigo. These users must still perform a full reset.