Passwords (Secret Codes)
When do I enter my password: before or after the entry?
|
|   |
Enter a password before you view or create a secret entry.
For instructions, select your model:
PS-2000
To set up the password, follow these steps:
| 1. |
Press Tel or Memo. (If you want to create secret
files for both telephone and memo entries, you must perform this
procedure twice: once for Tel and once for Memo.) |
| 2. |
Press Shift, then press Secret. KEY WORD? appears on the display.
Note: If nothing happens when you press Shift, Secret, you already have a secret code.
|
| 3. |
Type your password. (The password can be up to six letters and/or numbers.) |
| 4. |
Press Shift, then press Secret again. |
To use the secret password:
| 1. |
Press Tel or Memo. The NAME or MEMO IN prompt is displayed. |
| 2. |
Type your secret code. |
| 3. |
Press Shift, then Secret. If you enter the code correctly,
and NAME or MEMO IN are
displayed. You can now access your secret entries. (If you enter the
code incorrectly, OPEN ERROR! is displayed and the display returns
to the open files. Enter the correct code and press Shift, Secret.) |
| 4. |
To retrieve a secret entry, enter the entire name (or the first
letter of the name) that you want to recall and press or .
You may also press or to scroll through the names until you
find the desired entry. |
PS-2100+, 2400+, and 2460i
To set up the password, follow these steps:
| 1. |
Press Tel or Schdl. (If you want to do secret
files for both telephone and memo entries, you must perform this
procedure twice: once for Tel and once for Schdl.) |
| 2. |
Press Secret. KEY WORD? appears on the display.
Note: If nothing happens when you press Secret, you already
have a secret code. |
| 3. |
Type your password. (The password can be up to six letters and/or numbers.) |
| 4. |
Press Secret again. |
To use the secret password:
| 1. |
Press Tel or Schdl. The NAME or MEMO IN prompt is displayed. |
| 2. |
Type your secret code. |
| 3. |
Press Secret. If you enter the code correctly,
and NAME or MEMO IN are
displayed. You can now access your secret entries. (If you enter
the code incorrectly, OPEN ERROR! is displayed and the display
returns to the open files. Enter the correct code and press Secret.) |
| 4. |
To retrieve a secret entry, enter the entire name (or the first
letter of the name) that you want to recall and press or .
You may also press or
to scroll through the names
until you find the desired entry. |
All 3000 series models
For the PS-3000 series, you can add password protection for Telephone and Schedule entries.
To set up the password, follow these steps:
| 1. |
Press Tel or Schdl. |
| 2. |
Press Secret. KEY WORD? appears on the display.
Note: If nothing happens when you press Secret, you already
have a secret code. |
| 3. |
Type your password. |
| 4. |
Press Secret again. |
PS-6560i
For the PS-6560i, you can add password protection for (Secret) Notes.
To set up the password, follow these steps:
| 1. |
Press Options. |
| 2. |
Press 6 (Set/Change Password). |
| 3. |
Type your password. |
| 4. |
Press Enter. You will now be able to view and create
new secret entries. |
All 6700, 6800, and 6900 series models
For the PS-6700, PS-6800 and PS-6900 series, you can add password
protection for (Secret) Notes. To set up the password, follow these steps:
| 1. |
Press Options. |
| 2. |
Press 5 (Set Custom Options). |
| 3. |
Press 1 (Set/Change Password). |
| 4. |
Type your password. |
| 5. |
Press Enter. You will now be able to view and create
new secret entries. |
|
| I forgot my password. What do I do now? |
|   |
If you forget your password, you must reset your organizer.
To reset models in the 2000 and 3000 series:
To reset, turn the unit over and use a pen or paper clip to press
the small RESET button. Turn the unit over again. RESET?
appears on the display.
| |
To erase only secret files, press Enter. RESET! is displayed,
and all secret files are erased. |
| |
To cancel the reset operation and keep your files, press any key
other than Enter. |
| |
To erase your open files in addition to your secret files, press
the RESET button a second time; then press Enter.
This also resets the date and time to the factory setting. |
| |
To cancel the reset operation, press any key other than Enter.
Only your open files remain intact. |
To reset models PS-6700, PS-6800, PS-6760Si, PS-6860Si, PS-6960Si using the keyboard:
WARNING: Resetting these
organizers deletes the password as well as all other information.
If you have a PC Connectivity Kit, be sure to backup your data prior to
reset -- you will lose all data when you reset.
To reset (and erase the memory) for any of these units, do the following:
| 1. |
Make sure the unit is off. |
| 2. |
Press the , , and
keys at the same time. |
| 3. |
Turn on the unit while still holding these keys. |
| 4. |
After the unit is on, release the keys. This will trigger a beep. |
| 5. |
Turn the unit off. |
| 6. |
Turn the unit on. All data in the organizer's memory has now been erased. |
To reset models PS-6700, PS-6800, PS-6760Si, PS-6860Si, PS-6960Si by removing the batteries:
Take both batteries out. Press the On key or the INDIGLO
night-light key (if you have one) repeatedly until the menu display
disappears. (This should take about 1 minute.) When the display is
no longer visible, the memory is cleared and you may reinsert the
batteries. Your password and all other data have been erased.
|
Compatibility
Is the PS-6155 software Windows 95 compatible? |
| |
Yes. Although the PS-6155 software is a 16-bit
application, Windows 95 can manage 16-bit applications as well
as 32-bit applications. |
| Can I transfer my old files to my new unit? |
| |
New PS-6155 software (Version 2.0): If you are
upgrading from PS-6155 version 1.X to version 2.0, you can simply
open your PS-6155 version 1.X .PSD file in version 2.0 of the PS-6155
software. The version 1.X .PSD file will be automatically upgraded
to the version 2.0 standard. Be aware that you will no longer be
able to use the .PSD file with PS-6155 version 1.X software after
conversion to the 2.0 standard.
New organizer: If you have purchased a new organizer and wish
to copy the data from your old organizer, you can do so if you have
the PS-6155 software and the dock station. Connect the new organizer
to the dock station, open the PS-6155 software, and click Link, Send.
TImeRunner files: If you have TImeRunner (.TIL) PC files, you
can import them into a PS-6155 file. You can either create a new file
for the TImeRunner entries, or import the TImeRunner entries into a
file that already contains entries, adding the TImeRunner entries to
the entries in the PS-6155 file.
Before importing a file of TImeRunner entries into the PS-6155 software,
you must create the .TIL file using either the PS-9020 or IS-8150
Link software.
Note: When you import a TImeRunner file, only the entries are
imported. None of the option settings (password, address list names
or defaults, or keywords) are imported.
To import the TImeRunner entries:
| 1. |
Open or create a file into which you want to import the
TImeRunner entries. The file must be a .PSD file. |
| 2. |
From the File menu, select Import, and then select
TImeRunner File (TIL). The Import TImeRunner File
window is displayed. |
| 3. |
Select the .TIL file you want to import (as you would normally
in a Windows program). After you select the file, the import process begins.
A progress indicator bar reports the import status. |
| 4. |
When the import is complete, a message is displayed to let you
know how many entries were imported. Click OK. |
Note: Conflict resolution is not supported for the importing
of TImeRunner files. As a result, you may have duplicate entries if
you import a TImeRunner file into an existing file.
|
| Can I use my electronic organizer with PC organizer software other than the PS-6155? |
| |
Yes. If you are using a PC program such as Lotus Organizer, Day Runner, TImeRunner, Schedule +, Act, Sidekick, Now Up-to-Date, Ascend, or Maximizer, you can coordinate your PC and organizer files using the PS-6155 Connectivity Kit. To do this, you will have to export your non-TI software to a .CSV file and then import the .CSV file into the PS-6155. |
Synchronization and Transmission Problems
What does synchronize mean? How does synchronization work?
|
| |
Synchronized personal organizer units have the ability
to simultaneously update the entries on the organizer and the PC,
making both files identical.
If you have a PS-6760Si, a PS-6860Si, or a PS-6960Si, you can
synchronize the files on your organizer and your PC in one step.
When you choose the Synchronize command, the PS-6155 software
determines if PC and organizer entries have been changed in some way
(for example, additions, deletions, or modifications), and updates
the PC and/or organizer entries accordingly. After synchronization is
completed, no difference exists between the entries on the PC and the
entries on the organizer. |
| What is the difference between synchronized and non-synchronized units?
|
| |
With synchronized organizers you can update the contents
of organizer memory and its corresponding PC-resident file with one
command. The software merges the two files, so that any additions,
deletions, or modifications made to either file are updated in both
files.
Although you can update the PC and organizer files on a non-synchronized
organizer, it requires a series of actions. |
| How do I update the PC and organizer files
if I have a non-synchronized unit? |
| |
WARNING:
It is very important that you complete
the steps below in the correct order. If you have a blank PC file,
for example, and you send entries to the organizer first, you will
erase the entries on the organizer since the PC file will be copied
over the organizer file.
To update the two files for a non-synchronized organizer:
| 1. |
Copy organizer entries to the PC file. (Click on Link, Receive.)
If a conflict occurs between .PSD entries and corresponding organizer
entries, you can resolve the conflict by selecting an option in the
dialog box that appears. |
| 2. |
On the PC, delete any unwanted entries. |
| 3. |
On the PC, update Organizer Options if desired. (Click on
Category, Organizer Options.) |
| 4. |
Send all categories of entries to the organizer. (Click on
Link, Send.)
The PC file is now synchronized with the organizer's memory. |
|
| Why won't my unit synchronize? |
| |
You must have a synchronized organizer model (models
PS-6760Si, PS-6860Si, and PS-6960Si). If you have one of these
models and are unable to synchronize your organizer with your PC,
there is probably a communication problem between the organizer and
the PC.
To resolve the problem, ensure that:
| |
The PS-6155 cable is properly connected to the PC's serial port. |
| |
The organizer is properly seated in the dock-station cradle. |
| |
The correct organizer model is selected on the Connection window.
(Click on Setup, then click on Connection...) |
| |
The correct serial port (COM1, COM2, COM3, or COM4) is selected
on the Connection window. (Click on Setup, then Connection...) |
| |
You have previously set the Date and Time on the organizer by
choosing Options, 4 (Set Date and Time). Otherwise, the organizer
will not turn on automatically. |
| |
You have not locked the organizer with a password. If the
organizer is locked, unlock it by choosing Options, 2 (Lock/Unlock
the Unit) and following on-screen instructions. |
| |
The organizer is not in calculator or edit mode. |
| |
A .PSD file that corresponds to the current organizer memory is
open on the PC. |
After checking these items, try again. Refer to the online help for
additional assistance.
Note: The time required for synchronization is dependent on the
number of new, modified, or deleted entries to be handled. As a
result, synchronizing may take a few seconds to several minutes.
|
| Can I synchronize certain categories? |
| |
The current release of the PS-6155 software does not
allow synchronization of selected categories of information. The
entire memory of the organizer is synchronized with its corresponding
PC-resident file.
|
| I am receiving a transmission error. What should I do first? |
| |
| |
Make sure your system meets the requirements for the PS-6155 software. |
| |
Make sure the correct Organizer Model and Serial Port (COM port) are selected in the PS-6155 software (under Setup, Connection). |
| |
Make sure the COM port you are using does not have a conflict with another device (an internal modem, for example). |
| |
Look for an IRQ conflict with another device such as a serial mouse or an internal modem. |
| |
If you use a notebook computer, make sure the port you are using is turned on. (For computers running Windows 95, you can check this by clicking on Start Menu, Settings, Control Panel, System, then looking at the properties for the COM ports.) |
| |
Try turning off your notebook's power management before you attempt to use the 6155 Connectivity Kit. The battery conservation mechanisms often create difficulties. |
| |
Check the Startup group to see if any additional programs are being loaded when Windows starts that might interfere with serial communication (the Microsoft Office toolbar, for example). If you have numerous items in your Startup group, we recommend copying them to a temporary location, clearing the Startup group, and rebooting to see if this clears your transmission error.
To check the Startup group:
Windows 95: Click StartMenu, Programs, Startup.
Windows 3.1, Windows for Workgroups: Double-click Program Manager, Startup.
|
| |
See if another serial device (an external modem, for example) will work on the serial port you are trying to use. |
| |
Make sure the COM driver you are using is the standard driver: COMM.DRV. (Check your Windows\System folder.) |
|
| My transmission reaches a certain percentage complete and then displays a transmission error. What should I do? |
| |
This could be happening because the data is being transferred too quickly, causing a "back-up" in the serial port. There are several things you can do to try to eliminate this.
| |
Eliminate any applications that may be distracting the processor from the communication task. (Close all other applications, and disable screen savers and virus scanners.) |
| |
Adjust the Transmit Buffer. |
| - |
In Windows 3.1, 3.11, and Windows for Workgroups 3.11, disable the entire Transmit Buffer. |
|
WARNING: We do not recommend that you try this unless you are experienced in making changes to your system files (such as the SYSTEM.INI). If you do attempt this change, make a backup copy of the file before you begin. |
| To disable the buffer: |
| Add COMXFIFO=0 to the [386Enh] section of the SYSTEM.INI file (substitute the number of the COM port you are using for X in COMXFIFO). When you finish, you can enable the buffer again by returning the setting to COMXFIFO=1. |
| If you have Windows for Workgroups 3.11, you can also set the size of the transmit buffer by adding COMXTXFIFO=12 (substituting the the number of the COM port you are using for the first X) or adjust the receive buffer by adding COMXRXFIFO=8 (substituting the number of the COM port you are using for the first X). You generally should adjust only the transmit buffer. |
| - | In Windows 95, adjust the Transmit Buffer by following these steps: |
|
- Click on Start Menu, Settings, Control Panel.
- From the Control Panel, click on the System icon.
- Click on the Device Manager tab.
- Double-click on the Ports section, if necessary, and then double-click on the COM port you are using.
- Click on the Port Settings tab, then click on the Advanced button at the bottom of the dialog box.
- Move the Transmit Buffer selector all the way to Low, and move the Receive Buffer selector to High.
|
|
| I am receiving an Internal Error message? What should I do? |
| |
Internal Error messages indicate that there may be a problem with one or more of the helper files that the PS-6155 software requires to run. Other software may have overwritten these files with a different version, or they may not be installed in the correct directory. You can usually eliminate this problem by closing all applications and reinstalling the PS-6155 software. In Windows 95, you should install the software from Safe Mode.
If you are still having difficulty and would like a listing of the helper files (with date, size, and location), please contact Customer Support. For prompt assistance, please be prepared to provide Customer Support with the Internal Error you are receiving and your PS-6155 software version. |
Erasing/Resetting the Organizer
How can I reset my unit?
|
| |
Resetting an organizer is a quick way to completely empty
the contents of the organizer’s memory. All data is lost when a reset
is done, so be sure to back up the organizer file before doing a reset.
To reset models in the 2000 and 3000 series:
Turn the unit over and use a pen or paper clip to press the
small RESET button. Turn the unit over again. RESET? appears
on the display.
| |
To erase only secret files, press Enter. RESET! is displayed,
and all secret files are erased. |
| |
To cancel the reset operation and keep your files, press any
key other than Enter. |
| |
To erase your open files in addition to your secret files, press
the RESET button a second time; then press Enter.
This also resets the date and time to the factory setting. |
| |
To cancel the reset operation, press any key other than Enter.
Only your open files remain intact. |
To reset models PS-6700, PS-6800, PS-6760Si, PS-6860Si, PS-6960Si using the keyboard:
| 1. |
Make sure the unit is off. |
| 2. |
Hold down the ,
, and
keys at the same time. |
| 3. |
Turn on the unit while still holding these keys. |
4. |
After the unit is on release the keys. This will trigger a beep. |
| 5. |
Turn the unit off. |
| 6. |
Turn the unit on. All data in the organizer’s memory has now been erased. |
To reset models PS-6700, PS-6800, PS-6760Si, PS-6860Si, PS-6960Si by removing the batteries:
Take both batteries out. Press the On key or the INDIGLO
night-light key (if you have one) repeatedly until the menu display
disappears. (This should take about 1 minute.) When the display is
no longer visible, the memory is cleared and you may reinsert the
batteries. Your password and all other data have been erased.
|
INDIGLO®
What is INDIGLO®?
|
| |
INDIGLO® night-light is a feature on some TI
organizers that lets you see the display information in low light
conditions. INDIGLO® night-light is activated by pushing a button
on the organizer. It will stay on for a few seconds and then turn off.
|
| Why won't INDIGLO® night-light stay on? Why does it shut off so fast?
|
| |
In order to conserve battery power, INDIGLO® night-light
turns off after a few seconds.
|
System Requirements
What are system requirements? |
| |
System requirements are conditions that your
PC hardware and software components must meet or exceed in order for
your TI organizer and PC link software to be able to work with your PC.
Hardware and software requirements normally indicate the type of
platform required (for example, IBM PC), the operating system (for
example, Windows 95), central processing unit (80386 or higher),
graphics card (VGA or better), system (RAM) memory (4 MB available,
8 MB recommended), available hard drive space, type of installation
drive, type of pointing device (mouse), and communication port
configuration. |
| What are the system requirements for the PS-6155 Connectivity Kit software: |
| |
| |
MS-Windows version 3.1 or later. |
| |
MS-DOS operating system version 3.1 or later. (MS-DOS version 5.0 or later recommended.) |
| |
IBM 386 or better. (A PC with 80386 or higher processor.) |
| |
VGA video board (or better).
|
| |
4 MB available RAM. (8 MB recommended.) |
| |
At least one 3½-inch diskette drive. |
| |
Hard disk with 6 MB available storage space. |
| |
Mouse (or other compatible pointing device). |
| |
A serial communication port configured as COM1, COM2, COM3, or COM4.
| |
Batteries
What kind of battery does my organizer use? |
| |
The PS-20/20, PS-2000, PS-2100, PS-2460i, PS-3010,
PS-3600+, PS-3660i, PS-3960i, PS-6100 organizers use any of the
following batteries (or the equivalent):
- Duracell DL2025
- Panasonic CR2025
- Toshiba CR2025
- Eveready E-2025
- Ray-O-Vac CR2025
The PS-6300, PS-6360i, PS-6500, PS-6560i, PS-6700, PS-6760Si, PS-6800,
PS-6860Si, and PS-6960i organizers use any of the following batteries
(or the equivalent):
- Duracell DL2032
- Panasonic CR2032
- Toshiba CR2032
- Eveready E-2032
- Ray-O-Vac CR2032
Depending on the model organizer you have, replace both batteries when
one or more of the following conditions exist:
| |
The indicator is
displayed. |
| |
The display contrast will not adjust. |
| |
The display becomes erratic or slow. |
| |
The CHECK BATTERIES screen indicates that one or both batteries
need to be replaced. |
|
| The WARNING! screen is displayed when you press On/Off
to turn the organizer on. |
| |
The clock stops running. |
To prevent loss of data, replace batteries:
| |
When the indicator
is displayed. |
| |
Before the old ones are completely discharged. |
| |
One at a time and in the order indicated on the WARNING! screen. |
| |
Within a short time to minimize the length of time the organizer
is without full power. |
| |
Without touching any keys during the procedure. |
Important! Never replace batteries one minute before or after
midnight and never remove both batteries at the same time. Either
of these actions will result in loss of data. (Hint: Although
you can replace the battery without losing data, it is a good idea to
keep a written record of your stored data or to back up your data to
your PC using the PS-6155 connectivity kit.)
Caution: Do not incinerate the old battery or leave it within
reach of small children.
|
Adding, Editing, Deleting Entries on the Organizer
These instructions apply only to the 6500, 6700, 6800, and 6900 series organizers. The databanks (2000 and 3000 series) do not include addresses.
How do I add an address? |
| |
All address entries are stored together in a master list in alphabetical order.
In addition to the master address list, you can name and assign address entries to one, two, or all three custom address lists.
You can even set up the organizer so entries are automatically assigned to the list(s) of your choice. These lists allow you to
personalize and organize your address entries in the way that suits you best.
To enter a new address:
- Press Addresses to display the Addresses menu.
- Press 2 to select Enter New Address. ENTER NAME: is displayed on the top line.
- Enter the name. For personal names, you might want to enter the last name first since the organizer sorts (places in alphabetical order) from the left side.
- When you finish, press Enter. ENTER PHONE NUMBER(S): is displayed on the top line.
- Enter as many phone numbers as you need. Press
after each number to move to the next line for the next phone number.
The first 13 digits of the first phone number will be displayed in the Phone Scan list.
- Press Enter. ENTER ADDRESS AND INFO: is displayed on the top line.
- Enter one or more addresses and as much information as you need.
Press
as needed to move to the next line.
- Press Enter. CHOOSE ADDRESS LIST(S): is displayed on the top line.
If necessary, the entry temporarily moves up to make room for the address list choices. You can assign the entry to one, two, all, or none of the three custom address lists.
Note: If you have not named your lists, LIST 1, LIST 2, and LIST 3 are displayed. For naming instructions, consult the Personal Organizer Guidebook or the online Help in the PS-6155 software.
- Press
, , , or or to move between the lists, or Enter to move down the lists. Press (the X key) to mark your choice(s).
- If necessary, use the cursor keys (
, , , or ) to go back to any part of the entry you need to change. Type over it or use Ins or Del.
- Press Save.
|
How do I edit an entry? |
| |
- Display the entry you want to edit.
- Press Edit. The cursor is displayed and the prompts reappear to guide you.
- Press
, , , or to move to the part of the entry you want to change. Then you can either:
Type over existing information.
Press Ins to activate the insert cursor and insert information.
Press Del to delete a character.
- When you have finished making changes, either:
Press Save to save the changed entry.
Press Cancel to display a menu that allows you to cancel the changes or keep the changed entry.
|
How do I delete an entry? |
| |
- Display the entry you want to delete.
- Press Del. The DELETE ENTRY? screen is displayed.
- You can either:
Press 1 to keep the entry.
Press 2 to delete the entry.
Note: You cannot delete an entry from a scan list.
|
Setting The Time and Date
How do I set time and date? |
| |
For 2000 series:
- Press Time. The currently set date and time are displayed.
- Press Time Set (the Z key on the 2000, the B key on the 2400). The cursor moves to the first space of the top line.
- Enter the year, month, and date. Enter two digits for each. For example, to enter Friday, May 1, 1996, key in 96 05 01.
- Press Day (the X key) until the correct day of the week is displayed.
- Press 8
to move the cursor to the lower line.
- If necessary, press AM/PM (the C key) to change AM to PM, or PM to AM.
- Enter the time. Enter two digits for the hour and two digits for the minutes. For example, to enter 2:45, enter 02 45.
- Press Time Set to complete the setting. The seconds are automatically set to zero.
For 3000 series:
- Press the Time key. The currently set date and time are displayed.
- Press the Time Set key.
- Enter the year, month, and date. Enter two digits for each. For example, to enter Friday, May 1, 1996, key in 96 05 01.
- Press Day (the B key) until the correct day of the week is displayed.
- Press 8
to move the cursor to the lower line.
- If necessary, press the AM/PM key to change AM to PM, or PM to AM.
- Enter the time. Enter two digits for the hour and two digits for the minutes. For example, to enter 2:45, enter 02 45.
- Press the Time Set key to complete the setting. The seconds are automatically set to zero.
For 6500 series:
Before you can use the organizer's features that require date and time, such as Reminder entries, alarms, or the cities and times feature, you must set the date and time.
- Press Options to display the first screen of the Options menu.
- Press 3 to select Set Date and Time.
- Enter the current date in MM/DD/YY format, using two digits each for the month, day, and year.
- Enter the current time in 12-hour format. If the first digit you enter is 2, 3, 4, 5, 6, 7, 8, or 9, the cursor automatically moves to the second space for the hour. Then enter the minutes.
If necessary, press AM (the A key) or PM (the P key).
- When you finish entering the date and time, press Enter.
- Press
, , , or (the X key) to mark the format you prefer.
For example, for November 29, 1996, you can choose MM/DD to display 11/29/96, or DD/MM to display 29/11/96. You can also choose either 12-hour time (with AM and PM) or 24-hour time.
- When you finish, press Enter.
- Press
to mark whether or not the time you set is daylight savings time. (The
symbol displayed after a time indicates daylight savings time.)
- When you finish, press Enter.
For 6700, 6800, 6900 series:
Before you can use the organizer's features that require date and time, such as Reminder entries, alarms, or the cities and times feature, you must set the date and time.
- Press Options to display the first screen of the Options menu.
- Press 4 to select SET DATE AND TIME.
- Enter the current date in MM/DD/YY format, entering two digits each for the month, day, and year.
- Enter the current time in 12-hour format. If the first digit you enter is 2, 3, 4, 5, 6, 7, 8, or 9, the cursor automatically moves to the second space for the hour. Then enter the minutes.
If necessary, press AM (the A key) or PM (the P key).
- When you finish entering the date and time, press Enter.
- Press
, , , or to move between selections. Press (the X key) to mark the format you prefer.
For example, for November 29, 1996, you can choose MM/DD to display 11/29/96, or DD/MM to display 29/11/96. You can also choose either 12-hour time (with AM and PM) or 24-hour time.
- When you finish, press Enter.
- Press
to mark whether or not the time you set is daylight savings time. (The symbol displayed after a time indicates daylight savings time.)
- When you finish, press Enter.
|
Is the change of time setting for daylight savings automatic? |
| |
No, you must manually reset the time when the time change occurs.
|
How do I set a daily alarm? |
| |
For 2000 series:
The PS-2000 databanks do not include an alarm. For the PS-2100+, the PS-2400+, and the PS-2460i, you can set a daily alarm by following these steps:
- Press Time.
- Press Alarm (
).
- Press Time Set.
- If the time for which you are setting an alarm is PM, press AM/PM to change to PM.
- Enter the time for which you want to set the alarm. Enter two digits for the hour and two digits for the minutes. For example, to enter 2:45, enter 02 45.
- Press Time Set
For the 3000 series:
- Press Time.
- Press Alarm (
).
- Press Time Set.
- Press AM/PM.
- Enter the time for which you want to set the alarm. Enter two digits for the hour and two digits for the minutes. For example, to enter 2:45, enter 02 45.
- Press Time Set.
For the 6500 series:
- Press Options.
- Press 4 (Set Daily Alarms).
- Select an alarm or press Enter to accept the default selection.
- Enter the time. Be sure to change AM or PM if applicable.
- Press Enter to save the alarm setting.
When the alarm time arrives, the alarm sounds and the alarm indicator on the display flashes. To stop both the alarm sound and the flashing indicator, press any key. If you do not press a key to acknowledge an alarm immediately, the alarm sound stops after approximately 30 seconds, but the indicator continues to flash until you press 
For the 6700, 6800, 6900 series:
- Press Options.
- Press 3 (Set Daily Alarms).
- Select an alarm or press Enter to accept the default selection.
- Enter the time. Be sure to change AM or PM if applicable.
- Press Enter to save the alarm setting.
When the alarm time arrives, the alarm sounds and the alarm indicator on the display flashes. To stop both the alarm sound and the flashing indicator, press any key. If you do not press a key to acknowledge an alarm immediately, the alarm sound stops after approximately 30 seconds but the indicator continues to flash until you press 
|
How do I set an alarm for a reminder? |
| |
For 2000 series:
The PS-2000 databanks do not permit you to set alarms. For other 2000 series databanks, you can set an alarm for a reminder by following these steps:
- Press Schdl until the MEMO IN prompt and SCHDL are displayed.
- Enter a description for the appointment.
- Press Enter to move the cursor to the lower line.
- Enter the date. (You must enter two digits for the month and two digits for the day. For example, for April 7, enter 0407.)
- If the time you are entering is PM, press AM/PM to change to PM. (P is displayed on the screen.)
- Enter the time for the appointment. (You must enter two digits for the hour and two digits for the minutes. For example, for 6:00, enter 0600 if you are using the 12-hour format.)
- Press Alarm
. ((\)) is displayed on the screen, indicating that the schedule alarm is set.
- Press Enter. MEMO IN is displayed.
For the 3000 series:
- Press Alarm (
) repeatedly until ((\)) is displayed on the right edge of the screen, indicating that the schedule alarm is set. (All schedule entries will now have an alarm.)
- Press Schdl until the MEMO IN prompt and SCHDL are displayed.
- Enter a description for the appointment.
- Press
to move the cursor to the lower line.
- Enter the date. (You must enter two digits for the month and two digits for the day. For example, for April 7, enter 0407.)
- If the time you are entering is PM, press AM/PM to change to PM. (P is displayed on the screen.)
- Enter the time for the appointment. (You must enter two digits for the hour and two digits for the minutes. For example, for 6:00, enter 0600 if you are using the 12-hour format.)
- Press Enter. MEMO IN is displayed.
For the 6500, 6700, 6800, 6900 series:
- Press Reminders to display the Reminders menu.
Note: To change the date on the top line, press 
- Select ENTER NEW REMINDER by either:
Pressing to move the » pointer to 2 and then pressing Enter.
- To enter the date June 14, 1996 (for example), press 0 6 1 4 9 6. The day of the week (Mon, Tue, Wed, and so on) is automatically displayed.
- To enter 11:30 for the start time, press 1 1 3 0. The AM/PM setting automatically defaults to AM. If you need to change to PM, type P over the A in AM.
- Press
to move to the first space for the ending time. To enter 1:30, press 0 1 3 0.
- Press
Alarm to set an alarm to ring as a notification of the appointment. A bell symbol is displayed at the right of the
appointment.
Note: You can set the alarm any time after you enter a valid start time (until you press Save).
- Press Enter.
- Type the description LUNCH MEETING WITH PAUL and press Enter.
When entering a description, remember that part of the first line will be displayed in the summary lists. These lists are displayed when you press Day Scan or Scans.
Note: If you make a mistake, press or to move to the incorrect character. Then type over it or use Ins or Del.
If the description is longer than two lines, it temporarily moves up to make room for DAYS NOTICE. It returns after the number of days notice is entered.
- Press 5 for an advance notice five days before the meeting.
The specified number of days before the appointment, the organizer will display an
"advance notice" (indicated by !!) in the Day Scan summary list.
- Press Save. Your entry is displayed.
In order for the alarms that you set with the reminders to be activated, you must set the reminder alarm. You can set the reminder alarm to ring from 1 to 99 minutes ahead of set appointment times.
- Press Option to display the first screen of the Options menu.
- Press 5 to select SET CUSTOM OPTIONS. The first screen of the Custom Options menu is displayed.
- Press
to display the second screen of the Custom Options menu.
- Press 6 to select SET UP REMINDER ALARM.
Note:You can also press 6 from the first screen of the Custom Options menu without displaying the second screen.
- Enter the number of minutes (1 to 99) before appointment times that you want alarms to ring. (To enter two digits, press
before entering the first digit.)
- When you finish, press Save.
|
Can I turn alarms on and off? Can I set the volume? |
| |
For the 6500 series:
You cannot change the volume, but you can turn all alarms on or off by doing the following:
- Press Options.
- Press 9 to select Set Custom Options.
- Press 1 to select Turn Alarms On/Off.
- The default setting is On. Press
(the X key) to select Off.
- Press Save.
For the 6700, 6800, 6900 series:
You cannot change the volume, but you can turn all alarms on or off by doing the following:
- Press Options.
- Press 7 to select Turn Alarms On/Off.
- The default setting is On. Press
(the X key) to select Off.
- Press Save.
|
Airport X-Rays
Can I carry my TI organizer through an airport x-ray or metal detector? |
| |
TI has conducted tests that indicate your TI organizer should not have any problems with airport x-rays or metal detectors.
|
Warranty Information
Do I need a sales receipt for in-warranty service? |
| |
Yes. Before you return an electronic organizer, you should contact Customer Support (1-800-TI-CARES, 1-800-842-2737) to arrange for the return.
A defective electronic organizer will be replaced with the same or comparable reconditioned model (at TI's option) when it is returned, postage prepaid, to a Texas Instruments Service Facility. Texas Instruments cannot assume responsibility for loss or damage during incoming shipment. For your protection, carefully package the electronic organizer for shipment and insure it with the carrier. Be sure to enclose the following:
your full return address
a daytime phone number
a note describing the problem you experienced
a copy of the sales receipt or other proof of purchase to determine warranty status
Please ship the organizer postage prepaid; C.O.D. shipments cannot be accepted.
|
PS-6155 Connectivity Kit
If I have the PS-6155, what advantage will upgrading to the new Version 2.0 software provide? |
| |
The primary advantage is the addition of the synchronization feature. (Synchronization will be important to you if you have one of these models: PS-6760Si, PS-6860Si, or PS-6960Si.) Using synchronization, you can make changes to your PC or organizer entries, and, with just a click on the synchronize button , make the PC and organizer files identical.
The Version 2.0 software also includes:
a new, easy-to-use toolbar.
the ability to exclude duplicate entries if you are using a non-synchronized organizer.
automatic loading of the last file you edited when you open the software program.
|
What do I need to know if I have an internal modem?
In most cases your use of the PS-6155 software should not affect your internal modem. If you experience communication problems between the PC and the organizer and you change settings for your Communications Port (such as the Receive Buffer rate and Transmit Buffer rate), these changes could affect the performance of an internal or external modem, so be sure to return to your original setup after you use the PS-6155 software.
If I purchase a new organizer, do I have to purchase a new dock station?
No. Your old dock station should work with a new organizer. If you upgrade to Version 2.0 of the PS-6155 software, you will still be able to use the same dock station. See the PC Connectivity Kit page at http://www.ti.com/organizers/docs/ps6155.htm to download the new software.
What is the difference between a COM port and a serial port?
A serial port and a COM port, while closely related, are not the same. A serial port is a physical connection on the computer where a serial communications device, such as the PS-6155 dock station or a modem, attaches to the computer. Most computers have several serial ports (for the mouse and modem) and one parallel port (for the printer).
Serial communication involves the transmission of data one bit at a time, while information within the computer is transmitted using parallel communication, in which several bits of data are transmitted simultaneously. A COM port is an address in memory that Windows uses to access a serial port. In order to establish successful serial communication, the COM port address must match the address used by the serial port. When the addresses match, then there should be no communication problem, but if you have the PS-6155 set up to use a COM port that has no physical serial port associated with it, problems can occur. If you are experiencing problems with your computer's current configuration, please contact the manufacturer of your computer for assistance in reconfiguring your computer.
Will the software work with Windows NT or other operating systems?
Although the PS-6155 software is a 16-bit system, it can be used on machines that are running Windows 95, since Windows 95 can handle both 16- and 32-bit applications. The current release of the PS-6155 software does not run on Windows NT.
What is the file format for PSD file?
A .PSD file is a PC database file. It contains organizer entries that you create using the PS-6155 software, receive from the organizer, or import from a PIM (personal information manager) or other database software. It can contain all of the elements of an organizer file.
|
|
To turn power management off:
- From the Start Menu, click on Settings, Control Panel.
- In the Control Panel dialog box, click on the Power icon.
- In the Power Properties dialog box, click on the Power Management drop-down list and select Off.
- Click on OK.
|
|
To start the machine in safe mode:
- Click on the Start Menu, then click on Shut Down.
- In the Shut Down Windows dialog box, select Restart the computer and click on Yes.
- As the computer goes through the start up process, watch for the prompt "Now starting Windows 95." When you see this, press the F8 key. The computer will display a menu for various system modes.
- Select the Safe Mode option, then allow the computer to finish the reboot process. After Windows reopens, install the software, then reboot the machine in the normal manner.
|
|
IRQs (Interrupt Requests):
IRQs (Interrupt Requests) are settings that help manage the various devices attached to your computer. Each device has an assigned signal setting that it uses for communication with the computer's processor.
To view IRQ listings on PC running operating systems other than Windows 95:
- Go to a DOS prompt and start MSD.
- In the MSD application, select IRQ (Q).
- Check the list of assignments for conflicts.
To view IRQ listings on Windows 95 machines:
- Right click on the My Computer icon to display the menu.
- Click on Properties.
- Click on the Device Manager tab.
- Double-click on Computer (or click on Computer, then click on Properties).
- Click on the Interrupt Request button if it is not already selected.
- Check the list of assignments for conflicts.
You should be aware that there is usually a built-in conflict between COM ports 1 and 3 and COM ports 2 and 4 (if they exist). Since you will not usually be using both ports at the same time, COM 1 and COM 3 are normally assigned the same IRQ setting.
You could also check to be sure that your internal modem, for example, is not using the same COM port as your connectivity software. If so, try switching to a different COM port.
| | | | |