SNOSC84D August 2012 – February 2015 LMH6882
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
For related documentation see the following:
AN-2235 Circuit Board Design for LMH6517/21/22 and Other High-Speed IF/RF Feedback Amplifiers, SNOA869
SPI is a trademark of Motorola, Inc.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.