The TLC555 is a monolithic timing circuit fabricated using the TI LinCMOS process. The
timer is fully compatible with CMOS, TTL, and MOS logic and operates at frequencies up to 2 MHz.
Because of its high input impedance, this device uses smaller timing capacitors than those used by
the NE555. As a result, more accurate time delays and oscillations are possible. Power consumption
is low across the full range of power supply voltage.
Like the NE555, the TLC555 has a trigger level equal to approximately one-third of the
supply voltage and a threshold level equal to approximately two-thirds of the supply voltage. These
levels can be altered by use of the control voltage terminal (CONT). When the trigger input (TRIG)
falls below the trigger level, the flip-flop is set and the output goes high. If TRIG is above the
trigger level and the threshold input (THRES) is above the threshold level, the flip-flop is reset
and the output is low. The reset input (RESET) can override all other inputs and can be used to
initiate a new timing cycle. If RESET is low, the flip-flop is reset and the output is low.
Whenever the output is low, a low-impedance path is provided between the discharge terminal (DISCH)
and GND. All unused inputs should be tied to an appropriate logic level to prevent false triggering.
While the CMOS output is capable of sinking over 100 mA and sourcing over 10 mA, the
TLC555 exhibits greatly reduced supply-current spikes during output transitions. This minimizes the
need for the large decoupling capacitors required by the NE555.
The TLC555 is a monolithic timing circuit fabricated using the TI LinCMOS process. The
timer is fully compatible with CMOS, TTL, and MOS logic and operates at frequencies up to 2 MHz.
Because of its high input impedance, this device uses smaller timing capacitors than those used by
the NE555. As a result, more accurate time delays and oscillations are possible. Power consumption
is low across the full range of power supply voltage.
Like the NE555, the TLC555 has a trigger level equal to approximately one-third of the
supply voltage and a threshold level equal to approximately two-thirds of the supply voltage. These
levels can be altered by use of the control voltage terminal (CONT). When the trigger input (TRIG)
falls below the trigger level, the flip-flop is set and the output goes high. If TRIG is above the
trigger level and the threshold input (THRES) is above the threshold level, the flip-flop is reset
and the output is low. The reset input (RESET) can override all other inputs and can be used to
initiate a new timing cycle. If RESET is low, the flip-flop is reset and the output is low.
Whenever the output is low, a low-impedance path is provided between the discharge terminal (DISCH)
and GND. All unused inputs should be tied to an appropriate logic level to prevent false triggering.
While the CMOS output is capable of sinking over 100 mA and sourcing over 10 mA, the
TLC555 exhibits greatly reduced supply-current spikes during output transitions. This minimizes the
need for the large decoupling capacitors required by the NE555.