SBOS839J March 2017 – September 2019 TLV9061 , TLV9062 , TLV9064
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
The transfer function of the circuit in Figure 38 is given in Equation 1.
The load current (ILOAD) produces a voltage drop across the shunt resistor (RSHUNT). The load current is set from 0 A to 1 A. To keep the shunt voltage below 100 mV at maximum load current, the largest shunt resistor is defined using Equation 2.
Using Equation 2, RSHUNT equals 100 mΩ. The voltage drop produced by ILOAD and RSHUNT is amplified by the TLV906x to produce an output voltage of approximately 0 V to 4.95 V. Equation 3 calculates the gain required for the TLV906x to produce the required output voltage.
Using Equation 3, the required gain equals 49.5 V/V, which is set with the RF and RG resistors. Equation 4 sizes the RF and RG, resistors to set the gain of the TLV906x to 49.5 V/V.
Selecting RF to equal 165 kΩ and RG to equal 3.4 kΩ provides a combination that equals approximately 49.5 V/V. Figure 39 shows the measured transfer function of the circuit shown in Figure 38. Notice that the gain is only a function of the feedback and gain resistors. This gain is adjusted by varying the ratio of the resistors and the actual resistor values are determined by the impedance levels that the designer wants to establish. The impedance level determines the current drain, the effect that stray capacitance has, and a few other behaviors. There is no optimal impedance selection that works for every system, you must choose an impedance that is ideal for your system parameters.