| In
this issue:
TI-RFid
Signature Sponsor of RFID World
As the leading supplier of the broadest range of RFID products
in the industry, TI-RFid Systems has signed to be the Signature
Sponsor of RFID World Conference and Exhibition, a first
of its kind industry event that focuses exclusively on RFID
technology and applications. The event will take place May
13 and 14, 2003 at the Ft. Lauderdale Convention Center
in Ft. Lauderdale, Florida.
RFID World Conference & Expo is a high profile networking,
educational, and technology event that offers hands-on demonstrations
of next generation RFID solutions across a broad array of
industry applications. This groundbreaking event is the
perfect forum for RFID partners and providers to initiate
proactive planning and improve trading partner relationships
with buyers from key industry segments such as supply chain
and logistics, retail and catalog application, smart labels
and more. The event will also conduct special workshops
for systems integrators and value-added resellers (VARs).
"Through the support of this and other industry initiatives,
Texas Instruments has shown that it is without question
the leader in the RFID industry," said event director
Timothy Downs. "We look forward to showcasing TI's
expertise, and hearing from TI's customers as they present
innovative applications that utilize TI-RFid technology."
For more information please visit: http://www.shorecliffcommunications.com/rfid/default.asp?showid=R001&info=306
SkyeTek
Introduces SkyeRead M1 Reader
SkyeTek, LLC, a developer of RFID systems and applications
based in Boulder Colorado, recently announced its SkyeRead
M1 high-performance 13.56MHz RFID reader, which uses TI’s
S6700 Multi-Protocol Transceiver IC. Compliant with 13.56
MHz standards ISO 15693 and ISO 14443, the SkyeRead M1 is
a low-profile (4 mm), low-cost (1,000 units are priced at
$49 USD) reader. The small 38 mm x 40 mm footprint with
on-board antenna and several host interface options (RS-232,
TTL, SPI, and I2C) makes this plug and play device extremely
versatile and easy to use. An external antenna can be connected
for custom applications and to increase read range from
the standard 3-4 inches (~9cm) to up to 10 inches (25cm).
Other features include contactless identification with no
line of sight, simultaneous multiple tag reading capability,
and a simple ASCII protocol interface.
For more information contact SkyeTek at (720) 565-0441,
rfid@skyetek.com,
or visit www.skyetek.com
back to top
Accurate
Scores Keep Motorcycle Racers on Track
Competitors in Hare Scramble and Enduro off-road motorcycle
racing are speeding through designated checkpoints during
races thanks to TI’s RFID technology. Software developer
John Bouma developed a program called Race Timer that uses
TI- RFid tags and readers to improve scoring by minimizing
lag-time, maximizing the amount of riders on the track at
one time, and eliminating concerns about the accuracy of
collected data — all of which have improved the overall
professionalism of the sport.
In the past, teams were comprised of up to 20 individuals
with roughly 120 riders on the track at one time. As the
riders approached the single gate checkpoint, they needed
to come to a complete stop to pass through individually,
because their time was recorded manually using punch cards.
The use of barcodes on riders’ helmets improved the
scoring process since data could be analyzed for lap times,
starting times, and overall and class standings. However,
riders still needed to come to a complete stop at the checkpoint
to be scanned trackside, which slowed the event and limited
the number of participants.
Today, using TI-RFid technology, riders can continue racing
through checkpoints. By strategically placing antennas throughout
the racing trails and attaching a TI transponder with read/write
capabilities to the rider’s chest protector or front
fender, the racer’s time is recorded when he or she
passes by the antenna at each checkpoint. The software automatically
reads the rider’s transponder and determines his status
at each checkpoint, displaying his number, registered class,
rank, and distance behind the closest rider in his class
at that location.
TI-RFid has also enhanced the registration process by reducing
queue time and paperwork. At registration, each rider is
given a transponder, which is linked to a database containing
all of the rider’s pertinent information, including
name, racing number, and competing class. Once assigned,
a transponder is valid throughout a rider’s career,
and information can easily be updated on the spot using
its read/write capabilities.
The sport is increasing in popularity with an average of
400 riders on the track at a time. While it would have been
impossible to track and score this many riders using manual
methods, the new scoring system with TI-RFid technology
can now easily support 1,000 riders on the track simultaneously.
For more information on Race Timer, contact Bouma at boumaj@postyard.com
or visit his Web site at www.postyard.com/vchss/software.htm
back to top |
| Distributor
Profile: Dynasys |
| Website |
www.rfidusa.com |
| Phone |
727/443-6600 |
| Contact |
Bob
Scher, CEO |
| Description |
Dynasys
is the U.S. distributor and a complete technical support
center for TI-RFid’s products. The company’s
expertise is in understanding, supporting, and rapidly
fulfilling RFID hardware application requirements. |
| Major
Markets |
All
industrial markets, wherever automatic data collection
is required. |
1) What primary opportunities do you see for RFID
today?
We
see many potential market opportunities for RFID solutions
particularly for physical security and asset tracking. Sophisticated
access control solutions exist, such as TI-RFid long-range
readers and TI ISO 15693 cards, which allow security managers
to monitor all personnel as they enter and exit a gate.
We’re also working with a large medical supplier on
an RFID electronic inventory system to monitor medical devices
stored in operating room cabinets. This system will monitor
hundreds of hospital inventories and trigger an alarm when
inventory falls below a specified level. Each product is
labeled with a Tag-it inlay and is read using a TI-RFid
reader and Dynasys RFID antenna integrated in the storage
cabinet. Inventory data is posted on the Internet in real
time and can be retrieved from any remote location.
2) How are you helping your customers adopt RFID?
We provide complete education for prospective customers
by offering RFID starter kits and RFID equipment demonstrations
in our laboratory. Additionally, our staff shares their
industry and technology expertise through presentations
at industry conferences.
back to top |
| Opinion:
13.56 MHz Satisfies Today’s
Security Needs |
|
Given the challenges placed on security professionals, today’s
access control systems need to work harder and do more than
ever before. New and retrofit systems must control levels
of access, grant temporary status, assure authorization,
control access to remote company sites or locations inside
a single building, as well as monitor equipment. From employee
badges to biometrics, security managers are evaluating new
access control solutions to meet these new challenges with
technology that is still simple to use, cost-effective and
easy to deploy.
A number of market factors are coming together to create
new demand for 13.56 MHz RFID solutions including:
- New concerns over personnel and facility security
- The emergence of multi-function cards for access,
authorization and
stored-value transactions
- Technology advancements of the ISO 15693 vicinity
card standards
- New price and functionality of 13.56 MHz technology
In fact, Frost & Sullivan predicts that by 2006, RFID
cards will represent more than 80% of the access control
market.
Security and access control providers are embracing the
ISO 15693 vicinity card standard because of its new level
of security and authentication, interoperability across
all suppliers and applications, additional memory, faster
data transfer rates and multiple card reading capability.
The ISO 15693 vicinity card standard offers solution providers
and dealers a clear migration path and safe investment in
a technology that provides their customers with a new level
of security, and the assurance of interoperability.
The trend toward a single RFID card for multiple applications
will continue as more joint access control / transaction
applications are implemented, like those that are now common
on college campuses and in hospitals. And with the wide
acceptance of RFID for wireless payment, 13.56 MHz technology
will continue to fuel this migration toward multiple-use
vicinity cards and financial transaction tokens.
At a price level comparable to current 125 kHz proximity
card solutions, and substantial increases in functionality
and performance, 13.56 MHz is expected to dominate the market.
by Kelly Stark
Access Control Business Manager
TI-RFid Systems
back to top |
Further
Questions?
Contact our TI-RFid Systems Product Information Center at 1-888-937-6536
or click Questions?
and a customer service representative will be in contact with
you.
To
subscribe, click
here.
To
unsubscribe, reply to this message with "unsubscribe"
in the subject line and type your email address in the message.
|
| Question
of the Month |
In which market do you
think RFID is growing the fastest? |
| TI Events |
| Transponder
Roadshow
18 February, 2003
Duesseldorf, Germany
Transponder
Roadshow
25 March, 2003
Muenchen, Germany
ISC
West
March 26- 28, 2003
Las Vegas, Nevada, USA
RFID
World
May 12-14, 2003
Ft. Lauderdale, Florida, USA
Transponder
Roadshow
20 May, 2003
Dresden-Radebeul, Germany
IFSEC
19-22 May, 2003
Birmingham, UK
Retail
Systems
June 9-12, 2003
Chicago, Illinois, USA |
|