TI-RFid eNews
August 2004
 
     

Feature of the Month:

In this issue:

Feature: White Paper Compares HF/UHF for Item-Level Pharmaceutical Applications


Philips, TAGSYS and Texas Instruments have collaborated on a joint white paper, "Item Level Visibility in the Pharmaceutical Supply Chain: A Comparison of HF and UHF RFID Technologies." As established providers of radio frequency identification (RFID) technologies, the companies combined their expertise to detail the technical capabilities, deployment characteristics, and applicability of passive high-frequency (HF) and ultra-high frequency (UHF) technology for pharmaceutical item-level pedigree tracking applications. The white paper also highlights some of the existing commercial pharmaceutical and healthcare pilots and implementations.

The pharmaceutical industry is looking to RFID as a primary way of improving the safety and efficiency of the international drug supply chain through counterfeit prevention, decreased shrinkage and diversion, improved inventory management, and faster product recalls. According to the Food and Drug Administration, RFID provides the most promising approach for reliably tracking, tracing and authenticating pharmaceutical products, and it is recommending widespread use of RFID at the item level by 2007. Despite industry momentum for RFID, there are still many misconceptions and issues to be resolved, including the choice of frequency. While much of the focus has been on passive tags in the UHF bandwidth, the paper also provides an in-depth perspective on HF technology, discussing the technical and deployment characteristics that make it the most effective path with the lowest risk for item-level identification and pedigree tracking.

"RFID has the opportunity to transform the pharmaceutical supply chain," said Lisa Clowers, vice president, supply chain processes and technologies, Healthcare Distribution Management Association (HDMA). "We continue to support collaboration with all members of the healthcare distribution supply chain to explore the appropriate RFID frequencies to drive industry adoption."

To download a copy of "Item-Level Visibility in the Pharmaceutical Supply Chain: A Comparison of HF and UHF RFID Technologies,” visit any of the authors’ Web sites at www.semiconductors.philips.com, www.tagsys.net or www.ti-rfid.com. Access the paper directly at http://www.ti.com/tiris/docs/manuals/whtPapers/jointPharma.pdf.

back to top

TI Tag-it™ Technology Compliant with ISO/IEC 18000-3

Tag-it ImageIn standards news, Texas Instruments is announcing that its ISO/IEC 15693, high-frequency (HF) 13.56 MHz tags and readers are also compliant with the ISO/IEC 18000-3 standard. The ISO/IEC 15693 standard initially developed for contactless smart cards has been adopted for item management under the name of ISO/IEC 18000-3 Mode 1.

For applications such as libraries, manufacturing, supply chain, pharmaceutical/hospital and access control, the merging of these two standards allows the same radio frequency technology to be used for identifying assets as well as people. Using TI’s HF ISO technology, companies can simplify their systems and reduce their installation costs for HF RFID.

TI has been manufacturing its Tag-it™ISO/IEC 15693 compliant 13.56 MHz inlays and readers since the standard was finalized in 1999. The company has produced hundreds of millions of high-frequency ISO inlays for a number of different markets. The ISO 18000-3 standard is at the final draft international standard (FDIS) stage and is scheduled for publication by the ISO secretariat by the end of 2004.

back to top

SafeTzone Adds Cashless Spending Option to Theme Park Guest Location System

SafeTzone ImageLaunched in several theme parks and a shopping mall throughout the United States, SafeTzone Technologies Corporation has now added a cashless payment option to its Guest Location solution. Participating venues--Wild Rivers (Irvine, California), Great America (Santa Clara, California) Wannado City (Ft. Lauderdale, Florida) and many more --offer watch-like RF devices containing TI’s 23mm passive low frequency transponders, combined with active RF technology, to groups or families for instant real-time location of group members and amenities at in-park kiosks.

SafeTzone Image MonitorWild Rivers added SafeTzone’s Cashless Spending Module to its system this summer, allowing patrons to also use the wristbands as "electronic wallets." Guests can use cash or a credit card to create a spending account -which is accessed by passing the wristband over a reader at the point-of-sale. TI’s low frequency transponder provides a unique identifier, connecting the person to the appropriate patron account, allowing the vendor to debit payment for the items against the amount remaining in the account. Parents can even set spending limits for each child, allowing children to buy their favorite keepsake or snack, while eliminating the worry of overspending or wet, lost or stolen money.

"TI’s technology is an essential component of the overall system - providing the all-important first link," said Regan Kelly, co-founder of SafeTzone. "A guest account is created when each guest receives his or her wristband, and can only be accessed at a kiosk when the correct transponder is presented. Now that we’re offering a payment option, the issue of access to accounts and security of guest information is that much more important - TI’s passive RFID technology allows us to ensure that information is only accessible to the person with the right wristband."

SafeTzone plans to expand its Guest Location Services to a U.S. ski resort this winter as well as other family destinations in both the US and Europe.

For more information on SafeTzone Technologies, contact Regan E. Kelly by phone at 949-855-8987 x105, or via e-mail at regan.kelly@safetzone.com, or visit the company’s Web site at http://www.safetzone.com.

back to top

Precision Dynamics Unveils RFID/Bar Code Reader

Precision Dynamics Corporation (PDC), a Team Tag-it™ member and leader in automatic wristband identification, demonstrated a prototype of its new multi-function RFID/bar code reader at the Smart Healthcare Conference in June. The new dual handheld reader, created in collaboration with SkyeTek, will improve patient identification accuracy and patient safety in the medical industry. Combining an RFID reader/writer and a two-dimensional imaging bar code scanner into a tethered reader, the device captures information from RFID tags, including TI’s 13.56 MHz tags, as well as 1-D and 2-D bar codes.

"In recognizing the need to facilitate the interoperability between RFID and bar codes, we developed a device that can read/write to an RFID wristband and read a bar code," said Irwin Thall, PDC RFID manager for healthcare, in a recent press release. "The new device will easily connect to point-of-care mobile carts and devices such as EKG machines, pulse oximeters and infusion pumps, allowing for seamless and efficient patient administration, tracking and care."

Improvements in pharmaceutical identification technology are needed. According to the Institute of Medicine, 98,000 people in the United States die each year due to medical errors - mostly as a result of patient, specimen or medication misidentification - and the economic impact reaches almost $29 billion annually. By automatically filling in form fields, eliminating repetitive data-entry into medical devices, and decreasing common manual errors, the reader will benefit healthcare practitioners and patients alike.

With anticipated first shipments slated for September 2004, this product, easily compatible with most medical devices, will enforce the real-time confirmation of the "Five Rights of Medication Safety" - Right Patient, Right Drug, Right Dose, Right Route and Right Time (visit www.5rights.com).

For more information on PDC’s new reader, call 800-847-0670 x1320, or visit www.pdcorp.com.

back to top

Dynasys Launches Online RFID Superstore

Dynasys Technologies, an authorized distributor and technical support center for TI-RFid products since 2000, has launched an expanded version of its Web site to include an RFID Superstore. The new site features expanded listings of all TI-RFid products as well as Dynasys customer applications, and a comprehensive listing of educational RFID resources including articles, white papers, presentations, FAQs and industry links.

The company plans to offer an eStore for online product purchases as well as online customer service in the near future.

For more information, visit the RFID Superstore at http://www.rfidusa.com/superstore or contact Bob Scher, CEO, Dynasys Technologies Inc. at bobs@dyna-sys.com or at 727-443-6600.

back to top

RFID Educational Events Expand to Europe and Asia

TI-sponsored RFID educational opportunities are making their way around the globe this fall. Event producer, Shorecliff Communications LLC, is expanding its conference series to include European and Asian destinations through the RFID Europe Conference Series, RFID China and RFID Japan. Now integrators, IT professionals, engineers and executives internationally can reap the benefits of sessions covering the basics of RFID and EPC technology, step-by-step guides for RFID integration, and insight on the various solutions available in the market today.

RFID Europe Conference Series

The RFID Europe Conference Series provides three opportunities for attendees to learn the basics of RFID from industry leaders and technology experts, in collaboration with RFID International. The daylong program offers insight to help participants select, build and deploy RFID systems. In addition, technology experts will address the overall business case for RFID and discuss how enterprise users, integrators and value-added resellers can improve their businesses by incorporating RFID into their solutions portfolios. The events will be held on October 19, 2004 in London, England, October 21, 2004 in Brussels, Belgium, and on October 27, 2004 in Munich, Germany.

RFID China and RFID Japan

RFID China and RFID Japan are the first conferences providing comprehensive RFID technology information from leading technology suppliers and showcasing a comprehensive suite of RFID technologies and applications in these countries. The conference and exhibition will give attendees the opportunity to choose from a variety of classes, workshops and discussions with exhibiting solutions providers. Events will be held on October 7, 2004 in Tokyo, Japan and October 11-12, 2004 in Beijing, China.

For additional details or to register, contact Shorecliff Communications by phone at +1 800-608-9641 or via e-mail at info@scievents.com, or visit www.shorecliffcommunications.com.

back to top

Further Questions?
Contact our TI-RFid Systems Product Information Center at 1-888-937-6536 or click here and a customer service representative will be in contact with you.


TI Events

     
Equipmag 2004
September 13 - 16, 2004
Paris, France

Frontline Solutions
September 13 - 15, 2004
Chicago, IL USA

LogIntern 2004 - Auto-ID Show
September 29 - October 1, 2004
Nuremberg, Germany

RFID Japan
October 7, 2004
Tokyo, Japan

RFID China
October 11- 12, 2004
Beijing, China


RFID Europe Conference

October 19, 2004
London, England

October 21, 2004
Brussels, Belgium

October 27, 2004
Munich, Germany


RFID Boot Camps

September 13, 2004
Las Vegas, IL USA

October 4, 2004
New York, NY USA

November 8, 2004
San Francisco, CA USA

November 16, 2004
Orlando, FL USA

November 29, 2004
Boston, MA USA


Texas Instruments
6550 Chase Oaks Blvd. M/S 8470
Plano, TX 75023

To unsubscribe, click here