))) home ))) news ))) in the news ))) 2003 )))
Paul Demery
April 2003
Most direct merchants prefer nice orderly warehouses—a place for everything and everything in its place. But not FigLeaves.com. The U.K.-based, fashion-driven retailer of intimate apparel prefers a jumbled system that randomly stores products in whatever bins are available.
“Our warehouse is dynamic,” says Daniel Nabarro, chairman and founder of the fast-growing FigLeaves. “There’s no point in having a warehouse with empty space, so our whole warehouse is always optimized to new stock. We never have to worry about creating space for different categories, because we just stick products in any old bin.”
While it sounds like a sure way to mess up orders, Nabarro reports FigLeaves.com exceeds 99.9% accuracy in order filling. Its key to success: It uses radio frequency identification, or RFID, along with bar codes to quickly find and sort products to fill orders efficiently and accurately, Nabarro says. The intentionally unorganized system maximizes use of the company’s single, small warehouse, where managers avoid dedicating space to any one product or category because of constantly changing demand for its many varieties of intimate apparel.
While the challenge of moving and organizing products fast enough to get the right ones in front of consumers at the right time is as old as retailing itself, it has taken on new urgency in the world of web-based retailing where fast, accurate order fulfillment is crucial to success as well as in store-based retailing where the fast pace of product introduction and changing consumer tastes has mandated quicker movement to stores.
The retail industry has made great strides with supply chain and warehouse management systems that give retailers more control over the way products flow from production to warehouses and into store and online displays. But merchandise often still moves too slowly and remains too far out of sight, such as when a pallet of containers must be unloaded to scan dozens of difficult-to-reach bar codes. But now, RFID tags on products and shipping materials, under a system called electronic product code, or ePC, and strategically placed RFID readers report the movement of products to a dock worker’s or back-office manager’s computer. Those workers then get a real-time look at a product’s key data, such as SKU and serial numbers as well as current location and intended destination.
Although it’s still at an early stage of use in the retail industry, RFID is already supporting several retailers’ efforts to increase visibility and efficiency in the way they move goods, both at the distribution center level and at the b2c fulfillment level. RFID has been an integral part of manufacturing for years to track the flow of products in high-priced assembly operations, such as automobiles. But the cost per tag has only recently declined to where it can be economical enough to track a general range of goods in retail supply chains. And with further declines, it’s just a matter of time before more retailers like FigLeaves use RFID on every product, analysts say.
Although projections of the retail industry’s investment in RFID are sketchy, it’s easy to see how fast the technology will grow, says Peter Abell, a supply chain analyst for AMR Research Inc. Wal-Mart Stores Inc. has said it plans to have all containers and pallets it receives RFID-tagged by early 2005. “That’s tens of billions of tags, and that’s just Wal-Mart,” Abell says. And with other large retailers, such as The Home Depot Inc. and Target Corp., signed up as members of the Auto-ID Center, an industry group committed to RFID’s development, the use of RFID systems will mushroom over the next several years, he adds.
Right now, most RFID projects operate over private networks. For example, a pallet of RFID-tagged containers passes by a reader when it arrives in a store. The reader identifies and records the products’ SKUs and serial numbers on a screen. It also forwards that information over a private network to update a corporate database, such as in a merchandising management system, or to pull more information from a database to further describe the products in the containers.
But RFID proponents foresee a more ambitious use that would send such information over the Internet for a broader range of connections. That capability would allow information on delivered goods to be exchanged with databases outside a corporate network, such as in a supplier’s back-end system. So if a retailer needs more information on what’s inside RFID-tagged containers, for example, the RFID reader will identify the SKU and serial numbers and read any other information on the tag, then pull additional information that’s still needed through an Internet connection with the supplier’s databases.
“The vision of the Auto-ID Center is that objects will communicate through the Internet,” says Greg Gilbert, director of RFID strategies for Manhattan Associates Inc., a provider of supply chain software and a member of the Auto-ID Center. “So when you read an RFID tag, you can communicate through Internet protocols with a database that has the information you need.”
Connecting with suppliers’ databases, however, will require a level of cooperation from suppliers that may not be easily obtained. Many vendors may be disinclined to invest in the equipment needed to place RFID tags on their product containers. To make it easier for suppliers to participate with RFID, Manhattan Associates has released a test version of a web-based application, Infolink, in which a retailer provides the RFID infrastructure.
It works like this: the retailer provides its suppliers with blank RFID tags and a printer/encoder from Zebra Technologies Corp. The supplier accesses the retailer’s web-based Infolink application to access the retailer’s order information, such as the number of products to be shipped and their identifying SKU numbers. The supplier then clicks on the printer/encoder to encode the information on the RFID tag’s silicon chip as well as print out human-readable information on a paper label. The RFID tag is generally attached to the back of the label.
No companies have implemented the Infolink RFID system yet, though Gilbert says several companies are talking with Manhattan Associates about conducting pilots. Because Infolink is still in a test phase, Manhattan Associates declines to give a price. Gilbert says the cost will vary based on the number of suppliers and the number of transactions as well as the amount of information stored on the tag’s silicon chips.
Broad RFID usage is still a few years away, so analysts expect RFID to appear more in customized deployments designed to smooth out particular challenges that retailers face, such as speeding up the process by which shipments of products are checked in and warehoused. “They’ll pick a pain point to where RFID produces the best ROI,” says William Allen, marketing manager for Texas Instruments Radio Frequency Identification Systems, a division of Texas Instruments Inc.
At FigLeaves, the pain point was operating an efficient pick-and-pack system in its randomly filled warehouse. The e-retailer carries 108 brands and 18,000 SKUs, and sales have been surging, doubling for Christmas 2002 over the year before. Yet even with all that activity, the FigLeaves system of storing products randomly in its warehouse has proved to be highly effective, Nabarro says. “The only way we find anything in our warehouse is through complete computer-tracking of each item, so any SKU can be in any location,” he says. “Less than one pick fails per 1,000; it’s more like one per 5,000.”
To make it all work, FigLeaves has undertaken several initiatives that require communicating information to a database and then marrying that information with other information. For starters, FigLeaves scans the bar codes on all products as workers place them in bins. The scan reader reports the location of products to a database. FigLeaves also has placed RFID tags on totes, or plastic containers, that pickers use to fill orders from warehouse stock. The tags carry numbers that identify the totes.
When a customer places an order, the database links the order with the product location information. When the order is ready to be picked, the system assigns a tote number to the order. The database then reports via a computer on the tote trolley to pickers which products are in an order and where to find them in the warehouse. An employee picks an item from a bin and scans the bar code. The system identifies the correct compartment by reading the RFID tag, then activates a light on the compartment.
Before FigLeaves deployed RFID tags, warehouse employees would pick individual orders separately. Now, with RFID tags enabling the company to track each tote, pickers fill multiple orders simultaneously and accurately, Nabarro says. Each FigLeaves tote has eight compartments for different orders, and there are three totes on each trolley that pickers push through the warehouse. So each trolley has 24 orders to fill.
When the filled trolley arrives at the packing department, employees read information connected to each tote’s RFID tag to identify each order before packing and shipping it. A networked computer or handheld device pulls additional information about the order to create the packing slip and shipping label. Nabarro says the picking and packing systems are so easy to operate that new employees learn how to use them in minutes.
In the same way that FigLeaves uses RFID tags to identify totes, U.K.-based retailer Marks & Spencer is placing RFID tags made by Texas Instruments on more than 3 million trays used to deliver chilled foods to its grocery departments. The RFID tags are replacing bar codes because they are faster to scan, more durable and reusable, says Allen of Texas Instruments. The trays, which are delivered in batches of 24 on trolleys, can be scanned automatically all at once by passing through an RFID checkpoint, instead of being scanned individually and by hand when outfitted with bar codes.
Jim Evans, an RFID technology developer at RFID system provider Intermec Technologies Corp., says the Marks & Spencer project could become common in the grocery industry, where the need to track trays of fresh produce is critical due to sanitation requirements and the limited time within which fresh produce can be sold. “If a retailer gets a produce shipment too late, it may not be able to accept it,” he says.
Produce display trays are typically reused after being returned to a supplier, but only if retailers and their suppliers can verify they’ve been sanitized before being refilled. Verification can be time-consuming and difficult. But with production supervisors using handheld devices to record information about each tray, with identification based on the RFID tag, regarding when they were cleaned and when produce was picked and shipped, a retailer can see all that information when checking a shipment into a store. “So the retailer gets a traveling manifest of what’s in the shipment, where it came from, and when it was shipped,” Evans says.
Eventually, RFID proponents say retailers and their suppliers will place RFID tags on each product instead of just on containers. Nabarro of FigLeaves says placing RFID tags on each of his apparel products will make it easier and faster to scan each item when it’s stored as well as when it’s picked to fulfill an order. Unlike bar codes, which require a scanner to point right at them and nearly touch them, RFID tags can be read by simply waving a wand within three feet of a product, regardless of whether the tag is in view. When checking hundreds of products, that difference can save a huge amount of time, Nabarro says. Under his current system, even though the computer system tells a warehouse worker where to find ordered products, pickers must still scan the bar codes on individual products to enter their identifying information to the FigLeaves computer system.
But for FigLeaves and many other retailers, putting RFID tags on individual products will first require a reduction in the price of tags, which now cost FigLeaves about 35 cents each, Nabarro says. The price varies depending on the amount of information that’s stored on them; the more information, the larger the silicon chip, which drives up the cost.
Although RFID tag prices have fallen in recent years—with common prices declining from about $5 a couple of years ago to under $1 today—Nabarro and others say they’ll consider tags for each product when the price gets closer to 5 cents. Some industry experts say it’s difficult to predict at this point when, or if, prices will fall that far—at least for most retailers. For large companies that can buy in bulk, several industry experts say, per-tag prices can already get to 10 cents or less, though this could require ordering hundreds of millions of tags.
AMR’s Abell, however, projects that as Wal-Mart and other large companies begin to deploy immense numbers of RFID tags and readers over the next several years, prices will drop significantly. He figures it’s possible that, within 10 years, per-tag prices could get as low as 2 cents, making them cost-effective for most products.
In an ideal RFID project, RFID readers (currently priced at $300-$500 or more, but expected to drop within a few years to $100) positioned throughout a supply chain, in warehouse and distribution centers, and even on store shelves, could track tags placed on individual products. Each time a tagged product passes a reader, a signal could flash to a manager’s computer screen as well as to a back-end database to provide real-time information on product movement and location. So a store manager could check to see where a product or container of products was en route to a store or distribution center and corporate managers could access a web site to check on the status of merchandise throughout the chain.
In one test conducted by a national U.S. apparel retailer, the company realized a 12% increase in sales when it used RFID readers to monitor the movement of RFID-tagged shirts and bluejeans as customers picked them off store shelves, sending information on product movement to a back-end database to support a more effective replenishment system, says Allen of Texas Instruments.
That retailer, which Allen says he’s not at liberty to name, has put off further testing or deployment of that system, but other companies are already beginning similar tests.
The Gillette Co. recently began to test the deployment of as many as 500 million RFID tags on retail packages of razor blades and other products to track their movement from production to the point of sale. The project, using RFID tags manufactured by Alien Technology Corp., is being developed in cooperation with the Auto-ID Center and the Massachusetts Institute of Technology.
As in the apparel retailer’s test, Gillette will use RFID tags and readers to monitor when products are removed from store shelves and forward that information to retail managers’ computer screens as well as to back-end databases. At least some of its RFID tags will also be designed to activate anti-theft alarms, such as those many retailers already have installed near their exits. “It will alert retail staff when stocks become low or are being stolen and will enable automatic re-ordering of products,” vice president Dick Cantwell, who’s heading up Gillette’s RFID initiative, said in announcing the project in January.
By offering visibility right down to store shelves and making that sales activity easily accessible over the web, retailers can better manage distribution throughout an entire chain of stores, Allen says. “If a national retailer sees that a particular area of the country has a sharp increase in sales of particular items, and that another part of the country has low sales of those items, it can shift inventory to the stores that need it most,” he says.
Allen notes that by enabling retailers to closely monitor the movement of products and containers, they’ll be able to reduce shrinkage and, therefore, lower the amount of inventory they have to keep in distribution centers. “Now they have to keep more inventory in the supply chain in order to make up for the fact that, on average, they don’t now where 15% of their inventory is,” he says. “But RFID will help everyone along the distribution line know where cartons are supposed to go, so they don’t get lost in the first place.”
As retailers begin to realize the opportunities RFID offers in saving operating costs and increasing sales, the perceived value of RFID will rise, says Abell of AMR. “Even at 10 cents, 15 cents, or more, tags are cheaper than the cost of not fixing the problems that the technology solves,” he says.