[an error occurred while processing this directive]
[an error occurred while processing this directive]

)))  home  )))  news  )))  in the news  )))  2003  )))

[an error occurred while processing this directive]
TI-RFid™ News Sub Menu [an error occurred while processing this directive]
[an error occurred while processing this directive]
[an error occurred while processing this directive]
ComputerWorld

))) Wireless Gets Down to Business

Stacy Collet
May 5, 2003

From retail storefronts to the military's front lines, wireless technology now permeates nearly every sector of the U.S. economy. The technology has come a long way from simple bar-code reading with wireless PDAs. Today, tags affixed to retail garments taken into a dressing room can wirelessly signal a wall-mounted screen to display color choices and fabric information. College students can do research in the cafeteria instead of the library, and forklift operators can save themselves hundreds of miles of travel in factories by receiving product requests from computers mounted on their vehicles.

By the end of 2002, seven out of 10 companies had adopted wireless technology, according to a survey of 1,251 U.S. and Canadian companies in 18 industries by IDC in Framingham, Mass.

“Economics and technology are making wireless available to a lot more people,” says Ken Dulaney, an analyst at Gartner Inc. in Stamford, Conn. “We're seeing it increase in its capabilities. People know what it can do, and they're working on projects that make sense — updating them more into back-end systems.”

Purchases of wireless hardware reached $2.2 billion in 2002 and are expected to top $3.9 billion by 2006, according to research firm In-Stat/MDR. Units sold will skyrocket from 18 million to 75 million in 2006, which suggests that the cost of deploying wireless will continue to fall.

To learn how wireless is being adapted to meet changing needs, we took a look at the most innovative uses of it in 10 sectors of the economy.

Education
The Challenges of Being First

Three years ago, Carnegie Mellon University was voted “Most Wired Campus” by the online publication Yahoo Internet Life for its pioneering use of wireless access in more than 30 buildings.

Today, five years after the university installed its first wireless LAN, administrators are looking to upgrade the system with new standards and faster speeds, which will require 1,200 new access points for the 7,000 registered wireless devices on campus.

It's a problem facing many institutions. Some 87% of schools and institutions surveyed by IDC now use wireless technology, and 90% say bandwidth and network availability issues top their list of technology challenges.

Rough estimates of the cost of Carnegie Mellon's upgrade are about $3 million, three times what the university has spent so far on wireless. What's more, funding isn't as plentiful as it was five years ago, says Chuck Bartel, director of network services.

But one simple truth has bumped the project up the priority list: “If you don't deploy it yourself, it will probably get deployed by someone else, and in a manner you don't want,” most likely by tech-savvy students, Bartel says.

Bartel is concerned that if students don't have the wireless access they need, they'll find cheap hardware at a local electronics store and bring it onto campus. “If we haven't put the proper security in the mix, anybody can access university data,” Bartel says.

The combination of wireless access and tech-savvy students uncovers another truth — a network that's always available sometimes shouldn't be.

“At times,” says Bartel, “faculty doesn't want access to the Internet or instant messaging between students” — during tests, for example. But now that wireless is being embedded into laptops and handheld devices, “it's a little more problematic,” he notes.

But don't expect this technology institution to step back from the bleeding edge anytime soon. Carnegie Mellon is developing new uses for its wireless network in handhelds, laptops, robots and wearable computers.

Students in one graduate-level development course are working on intelligent agents embedded in handheld devices that will offer weather reports, restaurant options and even the location of friends, based on the user's location. The university's robotics institute is experimenting with collecting information by attaching wireless components to robots. “Once you have the infrastructure in place,” Bartel says, “the juices start flowing in terms of how somebody can use it.”

“They're using wireless LANs in classrooms because of the need to move around and just to give students the freedom to move anytime, anywhere,” says Gartner's Dulaney. “They do it for convenience. Plus, they love to play with that stuff.”

Finance
When Time Is Money

Soon after launching its first wireless offering in 1998, Fidelity Investments realized that wireless subscribers were very attractive customers. “They have more assets, they're more financially active and more tech-savvy,” says Joe Ferra, chief wireless officer.

That appealing combination keeps the Boston-based firm listening to its customers' demands for new wireless features and monitoring their use of every new function.

Today the company's wireless offering, Fidelity Anywhere, lets 170,000 customers get real-time stock quotes, make after-hours trades, short-sell and, with phone-integrated BlackBerry handhelds, call a Fidelity rep with the touch of a button. The firm also now lets customers manage their retirement accounts, charitable donations and insurance needs wirelessly.

While wireless capabilities expand, security issues remain an obstacle. “The level of security just isn't high enough yet” for many financial services functions to be deployed wirelessly, says Wai Sing Lee, an analyst at Frost & Sullivan in Toronto. Until Wireless Application Protocol 2.0 or 802.11 standards come out, real innovation will be put on hold, he says.

Some two-thirds of the financial services industry uses wireless technology today, with about 20% of those users in the initial stages of a rollout, according to IDC. What's more, 29% of financial services companies surveyed have or plan to provide online trading capabilities to their clients.

Ferra says security remains a paramount concern, and Fidelity continues to “look at what's out there” in terms of security standards. But right now it relies on encryption and authentication developed using the Handheld Device Markup Language.

The firm even chooses which functions will be offered on each type of device based on security concerns, browser capabilities and latency. “It would be very difficult for me to convince people at Fidelity to offer real-time quotes over a given device if we know the latency is 30 to 40 seconds. It's got to be a lot quicker than that,” Ferra says, adding that those discrepancies are becoming less of an issue.

“I'm convinced this will become a predominant way that people conduct their business with us. These devices are convenient, more reasonably priced and easier to use than ever before.”

Energy & Chemicals
Wireless Powers Sales Force, Productivity of Maintenance Crew

Like most executives in the energy and chemicals industry, the upper echelons of Celanese Chemicals Ltd. are fairly conservative, says Bill Schmitt, the director of e-business at Celanese. “Anything that looks or smells like bleeding-edge technology makes us pretty nervous,” he says.

But the $3 billion chemicals company was comfortable enough with handheld devices and wireless LANs by 2002 to adopt the technology primarily as a productivity tool for sales staff. Now the Dallas-based company is looking at wireless technology to speed maintenance at its chemical plants.

“When you run continuous production units, time is money,” Schmitt says. When a pump goes down, for example, maintenance workers travel through football-field-size plants by foot or bicycle to inspect the problem and then travel back to the control room and storage room to arrange for repairs — which could take up to an hour, he says.

In the future, employees will use Hewlett-Packard Co. Pocket PCs to report problems and arrange for repair equipment to be brought to the site. A pilot test is planned for later in the year.

Schmitt also wants to extend wireless capabilities globally to customers in China and Asia. But he acknowledges that the technology “isn't there yet.”

Europe and Asia were quick to adopt mobile phones and Short Messaging Service messaging, he says, but “in wireless data, the U.S. is still ahead.”

Health Care
Hands-off Technology in a Hands-on Business

As nurses whisk a critically injured patient into the emergency room at St. Vincent's Hospital in Birmingham, Ala., a physician grabs his PDA and with a few stylus strokes accesses the patient's medical history from the hospital's vast clinical data repository.

An admitting clerk scans the patient's insurance card and driver's license using a handheld device at the patient's bedside. After tests and surgery, caregivers will be able to access lab results, medication orders and surgery notes through wireless notebook computers or Pocket PCs that are synchronized with hospital systems for up-to-the-minute accuracy.

These everyday uses of wireless represent just the beginning of St. Vincent's plans for the six-building hospital campus, part of Ascension Health Inc., an $8.9 billion health care provider based in St. Louis. The St. Vincent's wireless network is the largest such network in health care in the Southeast.

“The heart of health care is information,” says CIO Jim Stettheimer. “When you can make information available anytime, anywhere, you're laying the groundwork for huge strides in quality and patient outcomes.”

At least eight out of 10 hospitals regularly use wireless technology today, according to IDC.

Health care workers “are in highly mobile environments where there's a requirement to gain access to information,” says Chris Kozup, an analyst at Meta Group Inc. in Stamford, Conn.

The first phase of St. Vincent's project, which cost $1.6 million, included installing 167 Cisco Aironet 350 Series access points around the campus and a Cisco WLAN. The wireless network went live in July 2002 with 35 users, including physicians and admitting clerks who used Compaq iPaq Pocket PCs, Fujitsu Stylistic 3500 Tablet PCs and some Dell and Compaq notebook computers using Cisco Aironet 350 network interface cards. By March 2003 the number of users had doubled.

As part of a “total leap” into wireless, Stettheimer's team is piloting wireless voice technology from Vocera Communications that allows clinicians to speak into badges worn on their lapels to contact co-workers.

Ultimately, 600 hospital workers, including doctors, nurses, physical therapists, transporters, social workers and pastoral staff, will send and receive information wirelessly using role-based security, which restricts the kinds of information these workers can access.

Return on investment is measured in terms of time saved and patient satisfaction. In the future, administrators will measure the time it takes to get a medical order through the system.

Stettheimer says the technology will succeed because physicians have been closely involved in designing and implementing the system. “That puts them in a position of ownership and investment in making sure that it works well,” he says.

Manufacturing
The Shortest Distance Between Two Points Is Wireless

Automotive and aerospace plants lead the manufacturing pack in wireless device use, with about two-thirds of all companies actively using the technology.

General Motors Corp.'s Cadillac and Buick assembly plants mounted wireless computers from Symbol Technologies Inc. in Holtsville, N.Y., on forklifts so drivers can wirelessly collect and transmit data from the factory or warehouse floor. The forklift operators can also receive work instructions and and updates without leaving their vehicles.

The wireless network is expected to save $1 million at one GM assembly plant, according to a company statement. Forklift traffic has declined by 400 miles each day. After nine months of wireless use, forklift operators now average 60 to 70 deliveries a day, double the number of deliveries they were making before the system went live.

In a few years, manufacturers may be able to catch product defects by sensing out-of-range vibrations in industrial equipment using “smart dust.”

Carnegie Mellon University's MEMS Laboratory is developing the devices, which are tiny wireless microelectromechanical sensors (MEMS) that can detect everything from light to vibrations. Thanks to recent breakthroughs in silicon and fabrication techniques, these “motes” could eventually be the size of a grain of sand, though each would contain sensors, computing circuits, bidirectional wireless communications and a power supply. Motes would gather scads of data, run computations and communicate that data using two-way band radio between motes at distances up to 1,000 ft.

Manufacturers are already experimenting with triangulation, which uses wireless access points strategically placed throughout a plant. The precise location of multimillion-dollar equipment that moves around the plant can be tracked using radio frequency identification (RFID) tags mounted on the equipment. “This allows asset tracking,” says Meta's Kozup. “That's a bit of a future application, but some are experimenting.”

Retail
This Season's Must-Have: An RFID Tag

Retailers are old-time users of wireless technology for communicating between the checkout counter and the back room and mobile point-of-sale terminals. But today's wireless technology can improve inventory accuracy, fight fraud and increase sales.

Forward-thinking retailers are venturing into RFID technology, chip-embedded tags that hold more information than a bar code and don't require direct contact with a reading device.

“A good 25% of all major retailers have dabbled in RFID,” says Bill Allen, eMarketing manager at Texas Instruments Inc.'s RFID Systems. But most are holding off on full-blown implementations because of the poor economy, equipment costs or complicated supply chains.

Readers mounted on display shelves in stores can survey item tags and send inventory data to back-end systems rather than relying on point-of-sale data or manual counts. In the stock room, a tagged box's contents can be identified without opening the box.

At Prada's flagship store in New York, RFID-enabled dressing rooms are equipped with plasma display screens. When a customer brings a garment into the room, the screen reads the tag and displays information on the designer and choices of fabric and color; it even offers accessory ideas.

While retailers such as Wal-Mart Stores Inc. and Target Corp. have piloted RFID tags on boxes and pallets, retailers that manufacture their own clothing lines are experimenting with individual garment tags. “We felt that retailers who have a vertically integrated supply chain like Benetton or J. Crew or The Limited, who are manufacturing their own goods, would be the first to take advantage of item-level RFID,” says Jim Crawford, an analyst at Forrester Research Inc. in Cambridge, Mass. If retailers have control over the manufacturing facility, tags can be applied at the time of manufacture at no extra cost, he adds.

But at 25 to 50 cents apiece, the cost of individual tags is keeping item-level RFID at bay for many retailers.

“I foresee the use of RFID at the item level in five to seven years,” Allen predicts. “I foresee more applications used for RFID for the carton and pallet level. We are not anywhere near being able to provide retailers with a 5-cent or penny tag. The technology is just not there yet.”

Transportation
Cost Is Still a Roadblock For Some Carriers

About one-third of the companies in the transportation industry used wireless technology at the beginning of 2002, according to IDC. The other two-thirds indicated that they planned to evaluate or implement the technology by the end of the year. Many are installing wireless fleet-tracking devices.

Nationwide trucking company TRL Inc. announced plans in February to convert its entire fleet of 600 trucks to Aether Systems Inc.'s MobileMax system for wireless tracking and messaging. The company has used integrated mobile communications in its fleet for nearly 10 years and recently decided to upgrade to a system that automatically switches between land-based and satellite communications without driver or dispatcher intervention.

“It makes it easier to get the information necessary to dispatch and assign loads,” said Mike Brown, vice president of sales and marketing for the transportation and logistics division at Owings Mills, Md.-based Aether.

Pittston, Pa.-based TRL said the new system will help improve the productivity of its fleet and bolster customer service. But when it comes to wireless adoption, some industry executives say cost is one of the biggest roadblocks.

“Customers are demanding that wireless providers take us to a much lower cost,” but instead the industry is moving to expand offerings, says Dave Berry, vice president of Phoenix-based Swift Transportation Co. “We don't want to watch TV from our trucks; we want lower costs.”

Logistics
Getting It There Faster

The logistics industry has embraced wireless technology wholeheartedly for the past three years. Wireless LANs are used to manage large segments of the logistics chain, from container ports that handle bulk shipments of consumer goods to package delivery giants that track and manage worldwide shipments. Competitors in these areas now use wireless innovations to gain business advantage.

Memphis-based FedEx Corp. ratcheted up the competition with Atlanta-based United Parcel Service Inc. in February when it began deploying new handheld devices for its 40,000 FedEx Express couriers as part of a $150 million technology investment. The company selected Motorola Inc. to develop the PowerPad handhelds, which use Microsoft Corp.'s Pocket PC operating system and automated courier dispatch, pickup and delivery operations.

FedEx picks up and delivers about 3.5 million packages a day, and the PowerPad was designed to save 10 seconds at each stop, according to Ken Pasley, the courier's director of wireless systems development. FedEx expects a complete rollout over 18 months.

Unlike its current SuperTracker handhelds, also developed by Motorola, the new PowerPads can exchange data with FedEx's back-end systems, including its Web-based package-tracking applications, over AT&T Wireless Services Inc.'s nationwide mobile data network.

Craig Mathias, an analyst at Farpoint Group in Ashland, Mass., called the rollout a psychological victory over UPS, which is planning a similar rollout for early this year, as well as other undisclosed wireless innovations.

Government
Fighting Terrorism With Wireless

Federal, state and local governments — notorious for staying safely behind the technology curve — are uncharacteristically bullish on wireless technology. For many, the moves are a reaction to terrorism threats and new homeland security requirements.

The Los Angeles Police Department (LAPD) plans to install high-bandwidth WLANs at its 27 police stations by July to send mug shots, maps and graphical data to police officers on the street. The LAPD will deploy 1,500 Pocket PC handheld computers made by Symbol Technologies, which will include 802.11b WLAN cards.

Police departments in Baltimore and Glendale, Calif., have also developed interfaces between the WLAN radios built into the Symbol handhelds and the WAN-based radios used in police cars. Officers can use handhelds as remote units connected to the WAN while outside their vehicles.

The U.S. Department of Health and Human Services in March announced plans to test a wireless network operated by San Mateo, Calif.-based ePocrates Inc. to transmit bioterrorist health alerts to Palm OS-based handheld computers used by doctors across the country. Already, 250,000 doctors nationwide use ePocrates handhelds to determine the correct prescription and dosage for sick patients.

“Government is moving with the [wireless technology] curve,” says Gartner's Dulaney. “The entire Congress has RIM BlackBerries for e-mail. They rely on it.” On the state level, wireless use is fragmented because officials disagree on which departments have critical communications needs that would require it, he says.

Security and business concerns in New York have officials there considering putting wireless access points in subway tunnels so people can talk when they're underground. “New York believes being connected is extremely important for the health of its business, especially since 9/11,” Dulaney says.

Defense & Military
Wireless on the Front Lines

On the battlefields of Iraq, Afghanistan and Southwest Asia, Army troops have replaced the sneakernet used to requisition supplies and maintenance during the 1991 Persian Gulf War with wireless technology that can save time, money and maybe even lives.

Now, instead of loading a floppy disk with logistics information, supply chain reorder forms, mechanical parts orders and requisitions for vehicle maintenance and then carrying it to base camp for processing, troops are using CAISI (pronounced “Casey”), the Army's Combat Service Support Automated Information Systems Interface. The technology went into the field in October 2002 and is now used by four of the Army's 10 divisions.

“It used to take a week or so to get these supplies commissioned and back to the troops,” explains Maj. Salvatore Fiorella, assistant product manager. “CAISI increases the capability to order supplies by getting the wheels turning immediately, as soon as the transmission is made.”

In one instance, CAISI saved a unit in Southwest Asia $40,000 in hardware costs, the two weeks it would have taken to run wire, and hours of negotiations with the host country to get approval for laying down extra wire.

The system can transmit data about three to four miles, which has limited its use once troops venture deeper into enemy territory. But “with satellites linked to CAISI, that just brings it to the battlefield,” Fiorella adds.

The wireless system consists entirely of off-the-shelf hardware and software. Laptop computers in the field are physically connected to wireless modules, which are triple-encrypted using software from Fortress Technologies Inc. in Oldsmar, Fla., even though CAISI's use is restricted to “sensitive but unclassified” information.

CAISI is just one of the Army's efforts to have 802.11b wireless devices deployed in the field between 2008 and 2010, once all security issues have been addressed. “We have to worry about encryption, we have to worry about firewalls, we have to worry about nonworking communication lines,” says George Knizewski, lead engineer and contractor at the U.S. Army Program Executive Office, Enterprise Information Systems (PEO, EIS), at Fort Belvoir, Va. “We don't want to be on the bleeding edge of technology.”

Today, government agencies require wireless technology to meet the Federal Information Processing Standards (FIPS). “Unless it's up to that level of security, government agencies can't deploy them,” says Frost & Sullivan's Lee. CAISI is one of the first Army systems to be FIPS-compliant, which opens the door to many future uses.

“I see wireless bringing better assistance to the [troops] that are deployed, providing rapid information so they can see what's available on the battlefield, which will help leaders to determine what combat units are equipped to go forward,” Fiorella says.

Collett is a freelance writer. Bob Brewin and Tom Hoffman also contributed to this report.

[an error occurred while processing this directive]