[an error occurred while processing this directive]
[an error occurred while processing this directive]

)))  home  )))  news  )))  in the news  )))  2004  )))

[an error occurred while processing this directive]
TI-RFid™ News Sub Menu [an error occurred while processing this directive]
[an error occurred while processing this directive]
[an error occurred while processing this directive]
The Economist

))) The Future Is Still Smart

Contrary to some recent reports, the roll-out of revolutionary smart-tag technology is still going to plan.

June 24, 2004

SO THOROUGHLY have the lessons of the internet bubble been learned that the launch of any new technology is now invariably accompanied by much talk from industry observers about dangerous hype and inevitable disappointment. A case in point is radio frequency identification (RFID), a new, super-cheap version of which may, its backers hope, be destined to transform everything from shopping to warfare. As soon as RFID's boosters alerted the world to their innovations, reports of dire setbacks began to circulate. Yet if anything, the surprise is how well the roll-out of the new technology is meeting early expectations.

RFID systems are made up of readers and "smart tags" — tiny microchips each with an attached antenna. The tags can be stuck on everything from milk cartons to hospital patients. When prompted by a reader, the tag broadcasts the information on its chip. Unlike the traditional bar-code, which smart tags aim to replace, RFID chips give every tagged object a unique identification. (A bar-code describes only a class of objects, such as cans of Coke.) Companies hope to use RFID to track the trillions of objects that circulate the world every year in planes, lorries and ships, through ports and warehouses, on to shop shelves, through tills and into homes and offices. Accurate tracking should eventually save hundreds of billions of dollars a year as it improves distribution, reduces theft, cuts labour costs and shrinks inventory. Governments also want to use RFID to reduce drug counterfeiting and improve military logistics, among other things.

Smarter than the average bar-code

Firms have put smart tags on some goods for quite a while. But due to their cost tags have until recently mostly been stuck on expensive or oft-stolen items, such as designer clothes and compact discs.

In 2002, the Auto-ID centre, a partnership between academic researchers and business based in Cambridge, Massachusetts, came up with a standard for a new, stripped-down RFID chip that stores just 96 bits of information-enough to give every object in the world a unique number. With tag readers plugged into a computer network, this number can be used to look up detailed information about the object, such as its origin, age and expiry date. At the same time, the Auto-ID centre also challenged manufacturers to produce a five-cent tag. Several start-ups, including Alien Technology and Matrics, said they could do so. Suddenly, there was huge interest and talk of a potential mass market.

Last June, Wal-Mart, the world's biggest retailer, said it would require its 100 top suppliers to put tags on pallets and cases of products for shipment to a cluster of its supercentres in northern Texas. (Those press-ganged suppliers were later joined by 37 "volunteers".) Tesco, Britain's biggest retailer, also decided to introduce the technology. This year Metro, a German retailer, and Target and Albertsons, two other American ones, announced tag mandates for their suppliers. On June 17th, Wal-Mart said it would extend its RFID roll-out to its top 300 suppliers and to more shops.

The American government is becoming a big user of the new tags, too. Last October, the Pentagon said it would require its suppliers to put tags on cases and pallets shipped to its warehouses. It expects suppliers to have the technology working by January. The Food and Drug Administration wants drug manufacturers, distributors and retailers to adopt the new RFID technology to combat counterfeiting.

Alien Technology says that its current production line can assemble 2m chips a month. By the end of this year, it will have a second-generation line, able to assemble 2 billion chips a year. By 2006, it plans to introduce two third-generation production lines, each able to assemble ten billion chips a year. For orders of 1m, Alien Technology now sells its tags for 20 cents each. When the third-generation arrives, says Tom Pound of Alien Technology, "we believe that our best customers will be able to order finished tags for prices approaching five cents." Established manufacturers, such as Texas Instruments and Philips, are also entering the market.

So why all the gloom? Much of it stems from suppliers who feel they are being forced to pay for an investment that saves retailers money. Wal-Mart, for instance, is using tags to track goods from when they leave suppliers, through its warehouses, docking doors and supercentre stock rooms, to when they leave the back rooms for the supermarket shelves. Even more gallingly, the only time suppliers are likely to hear from Wal-Mart is when they make mistakes. At least the Pentagon, which last year sent a delegation to Wal-Mart's headquarters in Bentonville, Arkansas, to learn about RFID, plans to pay for its own tags.

Another problem is that the industry does not yet have a single hardware standard. The work of the Auto-ID centre produced two competing tag standards. EPCglobal, one of the successor bodies to the Auto-ID centre, is now working on a single superseding second-generation standard. Within EPCglobal four warring factions of manufacturers recently shrank to two. EPCglobal has promised to deliver the new standard by the end of this month, which should spur investment.

As investment rises, prices should fall further. Meanwhile, many firms hope that item-level tagging will soon make sense, particularly in Europe, where more efficient supply chains mean that there is less scope to reduce costs by other means.

Marks & Spencer, a British retailer, has just extended a trial in which tags are applied to suits, shirts and ties for men. The advantage of such item-level tagging is that it allows retailers to monitor stock levels with far more accuracy, and to order replacement goods at the end of each day to make sure that every size, style and colour remains in stock. Beyond improving efficiencies, retailers hope that smart tags could help to drive sales. James Stafford, head of RFID at Marks & Spencer, gives one example: a customer could take a tagged suit to a kiosk, which could then suggest a matching shirt and tie. Mr Stafford points out that men often lack confidence when shopping for clothes and would welcome advice, but are reluctant to ask for help.

But firms will have to handle privacy issues delicately. Scaremongering by some privacy advocates, who fear that details of everything they buy will be held on a database and potentially used for nefarious purposes, has made some firms quite defensive about their RFID ambitions.

Yet the ambitions mostly remain, and are increasingly becoming reality. Star City, an Australian casino, is already using smart tags to cut the cost of cleaning the 80,000 uniforms worn by its staff. The emergency room at the Shelby County Regional Medical Centre in Memphis, Tennessee, uses them to keep track of patients. Las Vegas airport is using tags to track luggage better, to reduce the number of items that get lost and to improve security.

As prices fall, demand should continue to grow, from tens of billions of tags in 2006, to hundreds of billions by 2009, to perhaps trillions a few years later. As prices fall to a fraction of a cent, most organisations dealing with physical logistical challenges should find valuable uses for the new tags. Some may one day even thank Wal-Mart for introducing them.

[an error occurred while processing this directive]