[an error occurred while processing this directive]
[an error occurred while processing this directive]

)))  home  )))  news  )))  press releases  )))  2000  )))

[an error occurred while processing this directive]
TI-RFid™ News Sub Menu [an error occurred while processing this directive]
[an error occurred while processing this directive]
[an error occurred while processing this directive]

))) Texas Instruments Announces 3D Analog Front End IC for Automotive RFID-Based Vehicle Access

Automotive RFID-Based Vehicle Access

))) DALLAS, TX (December, 2000)

Texas Instruments Radio Frequency Identification (RFID) Systems today announced its new 3D Analog Front End (3D AFE) IC, a
low-frequency RF chip that simplifies vehicle access design while providing cost, time, power and board space savings. The 3D AFE (part # TMS 37122) supports passive entry (including anti-collision), passive go, immobilization and remote keyless entry, all in one system.

Texas Instruments’ 3D AFE is a primary component of a keyless access solution and requires no action from the user to gain entry to their vehicle.  In the case of passive entry, drivers can have the keyfob in their pocket or purse, and when they come within 2 meters (about 6.5 feet) of the vehicle and pull the door handle, the device automatically identifies the driver and unlocks the door.

The 3D AFE interfaces to three different antennas, ensuring that data signals are picked up regardless of the orientation of the identification device.  Current keyfobs require the user to aim the device directly at the vehicle.  Compared with a single antenna, TI’s 3D AFE provides reliable hands-free access for users and is more cost-effective than a discrete solution because it draws less power, uses less PCB space and takes less time to design the vehicle access system.

The 3D AFE’s patented, user-programmable, dual wake pattern detection  distinguishes whether the vehicle access system has been activated from inside or outside  the vehicle. With these two on-chip wake patterns, engineers avoid design alternatives that are more expensive and that may result in delays in bringing products to market.  This provision for position detection is an added safety feature for consumers since accidental car starts are minimized when the person with the device is outside the car.

“We’ve designed a low-power, cost-effective 3D AFE that makes it easier and more convenient for designers to implement low-cost passive entry systems,” says Michael Knebelkamp, automotive strategy manager of Texas Instruments RFID Systems, “Up until now, engineers needed discrete solutions that were costly and consumed a lot of power.”

With a standby current of 5mA and less than 10mV peak-to-peak sensitivity, the 3D AFE provides a long battery life.  The device also features a battery recharge capability and battery-less backup.  The 3D AFE comes in an industry-standard, 16-pin TSSOP package, which is small enough to fit into a keyfob or credit-card device.  It has also been designed with on-chip antenna trimming using EEPROM controlled capacitor arrays to enable easier and more cost-effective production of the keyfob’s PCB.

The 3D AFE is compatible with the DST immobilizer, Texas Instruments’ high security, anti-theft transponder that uses 40-bit challenge/response encryption and RFID to remotely interrogate the driver before starting the vehicle.  Texas Instruments first introduced an RFID-based anti-theft immobilizer security system in 1993.

[an error occurred while processing this directive]
[an error occurred while processing this directive]