))) home ))) news ))) press releases ))) 2001 )))
Fast food is getting even faster for consumers who’ll be using the new Texas Instruments RFID-enabled Nokia wireless phone. In two national quick-serve restaurant chains, Nokia is beginning trials of its Nokia 5100 Series SmartCovers™, which incorporate TI’s radio frequency identification (RFID) technology and use a wireless network from 2Scoot. Consumers can combine the SmartCovers with any Nokia model 5100 Series phone and turn their phone into a mobile cashless payment device they can use inside the restaurant or at the drive-thru to make food purchases quickly and conveniently.
TI's DST tags provide a highly secure wireless transaction using authentication encryption. Using this technology, the RFID reader sends any random number (of predetermined length) to the tag, which is then scrambled based upon a 40 bit hidden encryption key so that the reader can authenticate the response as being only from a valid tag.
Fast, convenient and safe way to pay for fast food without the hassles of fumbling for your wallet. Allows retailers to identify individual purchasers and create powerful customer loyalty programs.
RFID retail applications based on Texas Instruments technology debuted in 1997, with the introduction of ExxonMobil’s Speedpass. There are now more than 4 million Speedpass customers. McDonalds is currently testing Speedpass at nine Chicago-area restaurants. TI's RFID systems are deployed worldwide with more than 100 million tags used in diverse applications including automotive anti-theft, asset management, assess control, supply chain and logistics.
View the Nokia press announcement at http://press.nokia.com/PR/200101/803668_5.html.
[an error occurred while processing this directive]