))) home ))) news ))) press releases ))) 2003 )))
Texas Instruments Radio Frequency Identification (TI-RFid™) Systems, a leading provider of RFID systems used in applications worldwide, today announced that Carrollton, Texas-based Open Options Inc., will resell Texas Instruments' line of 13.56 MHz contactless RFID vicinity cards and readers for access control applications.
Open Options will offer TI-RFid™ cards and readers as part of its line of access control products which includes its NPower DNA™ security management software. The NPower DNA open software system runs on a Microsoft platform and can be scaled to answer specific customer needs such as integrating human resources, IT and contractor databases into one cohesive system. Among its many features, the software can monitor alarms, trace an individual's card usage, and monitor and assign access to specific doors throughout a facility.
“Our agreement with TI allows us to offer our growing array of customers a customizable RFID-based access control solution with many more features at a price that's comparable to traditional proximity solutions ,” said Brent Doherty, product manager, Open Options Inc.
TI-RFid™ access control solutions are compliant with the ISO 15693 standard and incorporate the advanced capabilities of 13.56 MHz technology, including unique and secure identification, two-way, read/write communication, user programmability, and enhanced memory for storing multiple applications on a single card. In addition to vicinity badges, TI manufactures tags in a variety of forms including keyfobs and labels. Several TI-RFid™ readers are available including wall-plate, mullion, long-range and keypad readers.
All of the company's ISO 15693 tags have faster data transfer and a 40 percent longer read range than traditional proximity cards. They contain a unique tamperproof ID code and can be encoded and encrypted to support universal Wiegand formats and RS 232/485 protocols. In addition, the user can define DES encryption keys and control their own card programming.
“Our companies share a similar philosophy when it comes to offering open architecture access control products that the market is seeking,” said Kelly Stark, access control business manager, TI-RFid™ Systems.
[an error occurred while processing this directive]Open Options, based in Carrollton, Texas, is a forward thinking independent security company that distributes an array of quality access control products for customers who embrace the distinct advantages of the open architecture concept. The company offers scalable software solutions and a common hardware platform including intelligent controllers, sub-controllers, UL Listed panel enclosures, system communication devices and solutions to effectively distribute lock and camera power. Complimenting the company's core products is their superior customer support and custom software development. For more information visit, www.openoptionsinc.com or call 1-877-818-7001.