>> Semiconductor Home > Applications
Application Report Abstract

Caller ID on TMS320C2xx
Caller ID is a method of transmitting the telephone number and/or name of the caller to the subscriber via a burst of V23 or BEL202 data during the ringing phase of a telephone call. Various methods of signaling the start of this message are used in different countries and this report attempts to identify a near universal core routine for handling the messages within the DSP environment. ADSI is an extension of Caller-ID used in some countries to deliver menu driven options to feature phones. The basic signaling is the same as Caller-ID except that the messages are sent during the call phase, and there is a full acknowledgement of the request to send data.
This report covers the reception and decoding of either the Caller-ID or ADSI burst; it does not cover the interpretation of the burst or the recognition of non-DSP signaling, such as ringing or line reversal that may occur at the start, nor the need to switch a matching impedance onto the line. These are considered to be a part of the microcontroller function.
This application report is designed to be used with the Texas Instruments Caller-ID software package.
> View the complete PDF document: bpra056.pdf, (177 kb) |