FIFO Mailbox-Bypass Registers: Using Bypass Registers to Initialize DMA Control (Rev. A)
The TI 32- and 36-bit FIFOs contain mailbox-bypass registers that transmit priority from one FIFO port to the other, port A to B or port B to A with out storing the data in the FIFO SRAM buffer. This document describes the FIFO mailbox-bypass registers and shows an example of direct memory access (DMA) control of a digital signal processor (DSP). The components described are the SN74ACT3641 and the 32-bit floating-pointTMS320C31 DSP.
> View the complete PDF document: scaa007a.pdf, (65 kb)