Order Now
| Part Number | Buy from Texas Instruments | Status | Host | OS | Current Version | Version Date | Description |
SPRC069:
|
ACTIVE | PC | Win 95/98/2000/NT | v1.0a | 02/26/2004 | C24x Fast Fourier Transform (FFT) Library |
Description
Fast Fourier Transforms are an efficient class of algorithms for the digital computation of the N-point Fourier transform (DFT). In general, their input sequence are assumed to be complex. In many real applications, the data sequences to be processed are real valued. Even though the data is real, complex-valued DFT algorithm can still be used. One simple approach creates a complex sequence from the real sequence; that is, real data for the real components and zeros for the imaginary components, The complex FFT can then be applied directly.
However, this method is not efficient as it consumes 2N memory locations (Real & Imaginary) for N point sequence. When input is purely real, their symmetric properties compute DFT very efficiently. One such optimized real FFT algorithm for 2N-point real data sequence is packing algorithm. The original 2N-point sequence is packed as N-point complex sequence and N -point complex FFT is performed on the complex sequence. Finally the resulting N -point complex output is unpacked into another N+1 point complex sequence, which corresponds to spectral bin 0 to N of 2N-point real input sequence. Spectral bin 0 to N is sufficient, as the remaining bins N+1 to 2N-1 are complex conjugates of spectral bins N-1 to 1.
The real FFT requires 2N+2 memory locations to compute the FFT for 2N-point real valued sequence, which is highly preferable in contrast to the complex FFT that consumes 4N-locations for 2N-point real valued sequence. Moreover using this strategy, the complex FFT size can be reduced by half, at the FFT cost function of O(N) operations to pack the input and unpack the output. Hence, the real FFT algorithm computes the FFT of a real input sequence almost twice as fast as the general FFT algorithm.
This FFT library contains 128, 256 & 512 point real/complex FFT and they are summarized below:
Note:
- Documentation of Filter Modules is archived in the self-extracting zip file, and the pdf files can be found in c:\tidcs\c24\dsp_tbox\filter\doc directory.
- Software Test Bench (STB) support library must be downloaded to use the STB examples.
Software Test Bench:
To facilitate evaluation and deployment of these modules, they are made available as Software Test Benches (STBs) which run as code composer projects on readily available EVMs or eZdsp hardware platforms.
Each STB focuses on a particular software module and shows the customer how to invoke it, pass variable or data to it, and how to link it into their systems. Where possible, the module under evaluation is made to interact with other modules such as signal generators, which can provide input stimulus and data-logging modules or EVM-DAC drivers to examine a module´s response in a real-time environment. This helps customers to get a more realistic feel of the software module´s capability and applicability.The idea behind the STB strategy to demonstrate the FFT module is indeed simple. A block of N data sample is sampled/acquired using ADC (20Khz Sampling frequency) and then processed by the N-pint Real or Complex FFT module to determine the spectral content. Magnitude-square of all the spectral bins are updated along with input signal on the CCS graph window using Real Time Monitor for observation. User can quickly start evaluating the FFT modules by sweeping the input frequency and observing the spectral response.
Features
- "C" callable assembly interface & Direct ASM interface
- Object oriented, re-entrant, multiple times "instance-able" modules
- Each module has it's own Software Test bench (STB) for a quick and easy "self contained" evaluation
- STB framework is offered as a Code Composer project
- Fully documented (PDF files are included within the self extracting zip file)

Cart