Description
The TRF2443 Lineup Calculation Tool is a graphical user interface (GUI) allowing users to see device performance versus device configuration. The GUI plots end-to-end receiver gain, IP3, and noise figure over the entire analog gain control voltage (VAGC) range for a user defined device configuration. In addition, multiple plots can be overlaid on one another so that tradeoffs in device performance can be more easily understood. The data presented is accurate as the GUI uses measured characterization data eliminating errors that could result from using a mathematical model.