WEBENCH® Medical AFE Designer

Step 1:

The AD1293 Medical AFE WEBENCH Designer is already pre-configured for the 3-lead or 5-lead ECG application

 

 

Step 2:

If you want to configure the ADS1293 yourself and need help getting started, you can click on the step-by-step instruction in the Help Bar tab to see the description of each block and an arrow pointing to that associated block.

 

Step 3:

To configure the ADS1293, click on each block to change its register.

 

Step 4:

Click on the "Register Map" icon to see the complete ADS1293 register map.

 

Step 5:

Click on the "Performance" tab to display the estimated performance for the selected configuration, including power consumption, noise, and effective number of bits (ENOB).

 

Step 6:

Click on the "Disk" icon to save the register configuration file, which can be uploaded to the ADS1293 offline tool that runs with the ADS1293 evaluation board.

 
More WEBENCH help
See our disclaimer


Back to top