WEBENCH® Video Training
Learn how to use WEBENCH with these training videos. Each video walks the user though specific features of WEBENCH. The videos are short and include examples. See all WEBENCH videos.
| Number | Title | Length | Description |
1 |
24:35 min |
This is an overall introduction to WEBENCH Power designer including the following features:
|
|
2 |
11:25 min |
This presentation is a short introduction to the WEBENCH Power Designer tool including an overview of design creation, electrical simulation and thermal simulation. |
|
3 |
WEBENCH® Power Designer - Efficiency Calculation and Design Optimization |
15:10 min |
This presentation shows how efficiency is calculated in WEBENCH Power Designer. It also exhibits how users can easily optimize designs in WEBENCH Power designer for high efficiency, small footprint and low cost. |
4 |
WEBENCH® Power Designer - BOM Management and How to Change Components |
5:55 min |
This presentation shows how WEBENCH Power designer calculates the Bill Of Materials for power supply designs. It also discusses how a user can modify components in the BOM using graphs to visualize tradeoffs between critical component parameters, power dissipation, footprint and cost. |
5 |
10:03 min |
This presentation shows how a user can run Spice simulations in WEBENCH Power Designer. This includes selection of different simulation types such as steady state, load transient, line transient, startup and Bode Plot. Also, it discusses how to change the load current and other sources to use in the simulation including modifying the maximum and minimum current/voltage and the rise and fall times. In addition the presentation shows how to use the WEBENCH waveform viewer to plot different waveforms, zoom in and overlay waveforms from different simulations. |
|
6 |
4:53 min |
This presentation shows how to use the WebTHERM® Thermal Simulator to identify and correct thermal problems on the power supply printed circuit board. In addition it describes how to use WebTHERM to identify co-heating of parts on the board and how to change simulation conditions including the copper thickness, board orientation and airflow. |
|
7 |
6:53 min |
This presentation shows how to use the WEBENCH Visualizer to select between dozens of dynamically calculated design options for a given set of power supply requirements. It also shows how to use the WEBENCH Visualizer to quickly optimize and evaluate multiple power supply solutions for efficiency, footprint, and cost using a graphical approach. |
|
8 |
8:28 min |
This presentation shows how to use WEBENCH Power Architect to quickly optimize and create multiple load power supply systems. It also describes how to use WEBENCH Power Architect to design power supplies for a wide variety of FPGAs and microprocessors in addition to custom user specified loads. |

Cart